Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Is there a way to automate a reset using a USB to UART bridge if it's connected to a Raspberry Pi
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 22 replies
  • Subscribers 332 subscribers
  • Views 4597 views
  • Users 0 members are here
  • usb host
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Is there a way to automate a reset using a USB to UART bridge if it's connected to a Raspberry Pi

BigG
BigG over 2 years ago

I am trying to design a circuit for a new sensor board which essentially uses UART comms but I want to incorporate the option for USB to allow you to use a USB cable from a Raspberry Pi USB host to the sensor board.

But if I'm using USB I don't have access to the Raspberry Pi's reset pin via the USB cable. This is no problem if the Raspberry Pi powers up, but that is no good if the Raspberry Pi reboots. I would like to have it that if the Raspberry Pi reboots, my sensor board will do so too.

To simplify the design and testing process I am using one of these breakout boards: www.adafruit.com/.../5335

This uses a CP2102N and breaks out DTR, RTS, CTS etc etc. So I have options.

image

But I don't have any ideas... hence the question

  • Sign in to reply
  • Cancel

Top Replies

  • BigG
    BigG over 2 years ago in reply to shabaz +2
    Yes, that's my goal. I'm looking for a magical solution that does not involve using any extra GPIO pins. The idea of using UART break is certainly an interesting one. So, thanks for the circuit... I…
  • shabaz
    shabaz over 2 years ago in reply to BigG +2
    Here's a bit more of a sensible circuit! : ) Exactly same concept, but uses a cheap IC (74HC14), and eliminates awkwardness of the previous circuit, which may load the input, and it was pretty crude…
  • shabaz
    shabaz over 2 years ago +1
    Hi Colin, There's this blog post which I think implements what you're requesting, which is a way for a Pi (or any other host) to control GPIO, so that it can remotely reboot a device if the software…
  • shabaz
    0 shabaz over 2 years ago

    Hi Colin,

    There's this blog post which I think implements what you're requesting, which is a way for a Pi (or any other host) to control GPIO, so that it can remotely reboot a device if the software on the Pi restarts.  Simple USB Control of GPIO: Automating Device Resets and Bootloader Mode Buttons 

    I didn't try building for Pi however, so am only 80% sure if that will work. Also, that blog is using a different USB-UART chip (but a really good one).

    If you want to stick to the CP2102N, then control of GPIO is discussed here:

    /products/roadtest/rv/roadtest_reviews/155/silicon_labs_usb-to_1

    However, the CP2102N code doesn't support Linux too well (the Linux SDK code looked pretty ancient back when that review was written, maybe it's improved now), so there may be issues with using it with Raspberry Pi.

    Another trick (which doesn't care about host SDK) is to use any generic simple microcontroller on your sensor board, and get it to detect some special UART sequence. It can piggy-back onto the received data UART line, and control the power to your sensor. It doesn't matter if the sensor doesn't like the special sequence, because it will get reset after that.

    Possible candidate for an ultra-cheap simple microcontroller could be the one described here:  Low-Cost Microcontrollers: Using a CH32V003 RISC-V Device! 

    There is UART example code at that link. But you could use any microcontroller of course. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • BigG
    0 BigG over 2 years ago in reply to shabaz

    Thanks Shabaz.

    This is great. It sounds like there is certainly options out there. I will have a read through your blogs and the road test report.

    For background, what triggered my interest in the CP2102N and the possibility for hardware style reset was this schematic for the Adafruit ESP32 Feather V2 board.

    https://learn.adafruit.com/assets/109518

    The schematic shows this sort of arrangement, but I'm still trying to figure out how this works in conjunction with the CP2102N USB to serial converter shown.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 2 years ago in reply to BigG

    While that works, I think it's dependent on the OS (e.g. might be quite different to control that using say Windows versus Linux or Mac etc) to allow control of those pins. I've never tried it myself, but have seen that on some boards.

    Personally if I really was sure just a single pin of control is needed, then I'd investigate using UART break. since that doesn't require anything special with any OS, and would not require a USB-UART with the extra connections either.

    Something like the below circuit might work (will need tweaking of component values to suit the desired baud rate).

    How it works: Basically, if the RX pin goes low for any long length of time (a normally disallowed thing for UART) then the capacitor slowly charges up, pulling the BJT base low. That then results in the RESET OUT pin going high, asserting reset until the RX pin goes high.

    With normal serial data, the RX pin only goes low for a short amount of time, which isn't enough time to discharge the cap.

    Whenever you wanted to perform a reset, you would deliberately set the baud rate in your host program to a low value, and send a null character (i.e. 0x00). Then you'd change to your normal baud rate.

    The circuit is deliberately low-cost, but could be replaced with something more sophisticated if desired (e.g. logic gates or a microcontroller), but I think the single BJT+two diodes method could be made to work with appropriate component values for the resistors and capacitor.

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • BigG
    0 BigG over 2 years ago in reply to shabaz

    Yes, that's my goal. I'm looking for a magical solution that does not involve using any extra GPIO pins. The idea of using UART break is certainly an interesting one.

    So, thanks for the circuit... I couldn't quite see how it works but now that I've discovered my new best (electronics software) friend, I can visualise how it works.... this is just simulating UART RX pulsing every 100msec and it shows how RESET OUT alternates from high to low etc. Cooool.

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 2 years ago in reply to BigG

    Here's a bit more of a sensible circuit! : ) 

    Exactly same concept, but uses a cheap IC (74HC14), and eliminates awkwardness of the previous circuit, which may load the input, and it was pretty crude. This one is much cleaner. 74HC14 only costs 33p in single qty, so it should be fine for anything except the most price-sensitive products.

    The 100k resistor and 100nF capacitor set the RC time constant, and it should (I think) work with 300 baud 0x00 character for creating the break sequence, and any sensible baud rate (i.e. 9600 or higher) will easily take the target out of reset.

    Another bonus, there is both negative and positive asserted outputs, so it's more flexible. Plus, there are two spare inverters for any other purpose.

    It is probably worth putting a 100k pull-up on the input of this circuit, just to keep things in a known state if the USB side is disconnected.

    It could be worth assembling this on a breadboard, to see if it works. I'd give it a shot, but am a bit tied up for a few days : (

    EDIT: Also it needs a 100nF decoupling capacitor across the IC.

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • BigG
    0 BigG over 2 years ago in reply to shabaz

    Thanks Shabaz. Good to see how this circuit design is evolving. Your contribution is much appreciated.

    I just so happened to stumble across the LM66100 from TI, which is a Single-Input, Single-Output (SISO) integrated ideal diode.

    www.ti.com/.../LM66100

    So, as one often does we look for applications, and I thought that maybe we could apply it here where instead of UART TX data break we use DTR. So, wondering if this would work as the input... it's about 40p

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • BigG
    0 BigG over 2 years ago in reply to BigG

    Doh! If the 74HC14 is an inverter I don't even need to use the LM66100. As you say your circuit has two spare gates, so can we use one for DTR.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 2 years ago in reply to BigG

    I wasn't sure what the DTR is needed for (the UART break works without it), but agree, if you need that DTR inversion, you've got the spare capacity for that with the 74HC14.

    Now I think about it, the RXD-line UART break is actually more 'standard' than the Adafruit DTR/RTS circuit. It just happens that the Adafruit option is cheaper when those connections are available and if there is more control of the host software to implement it. Whereas, the 'break' is standard in lots of serial terminal software. I used to work on serial interfacing hardware that would specifically look out for a break (although it was integrated inside other silicon - FPGA from memory) rather than 74HC logic. 

    Here's what the terminal software I use (I'm using SecureCRT, but other terminal software will have similar features) can be configured for:

    image

    When the user hits the key combination, a break is issued. I just measured it, and SecureCRT sends a 100msec break. 

    With PuTTY, it's right-click on the top bar, to enter the menu:

    image

    PuTTY break length is even longer, 300 msec.

    I'm wondering why USB-UART adapters don't come with a break-detect as standard. It could be a nice feature for the occasional use when prototyping too, where such a signal needs to be sent out-of-band in this way.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • BigG
    0 BigG over 2 years ago in reply to shabaz

    Yes, I like the option of using UART break, although I don't know much about this method. It does give you user control which is good. On the otherhand, DTR is possibly simpler but you have no control over the signal line as its triggered by the host device when it reboots. I think the ability to have both options on a circuit would be very useful.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 2 years ago in reply to BigG

    I see.. DTR will also go high every time the host side software closes the UART connection, you might not always desire a sensor reboot each time that occurs. Might be worth having a jumper on the PCB to temporarily override that, in case (say during testing) it's likely to stop and start the serial connection without a reboot.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>