Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Single Mosfet level shifter does not appear to work
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 31 replies
  • Subscribers 333 subscribers
  • Views 3844 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Single Mosfet level shifter does not appear to work

obones
obones over 1 year ago

Hello,

As a follow-up to my previous question, I have written a little program for the PIC16F628A that I had been lying around for quite a while. It works well, but I have to make sure the "PowerLoss" signal is seen by both the PIC and the OrangePi.
As the PIC works at 5V and the Orange Pi at 3.3V without being 5V tolerant, I have to shift the levels between both sides. After looking around, I found the AN97055 application note from Philips that mentions a single NMOS level shifter and even recommends using a BSS88 that I also had around.

However, after having wired it in a way that I believe is right, I noticed that when PowerLoss "pulls down" the 5V side, the 3.3V side is not event close to zero volts, but rather around 1.3 volts. This is not liked by the H3 inside the OrangePi as it freezes itself after a while and I have to reboot it.

I tried to simulate the circuit with LTSpice and while it does not have the BSS88 by default, I found a library for it in the Blackboard project at github and so was able to create the following simulation:

image

Version 4
SHEET 1 1572 680
WIRE -128 0 -288 0
WIRE 0 0 -128 0
WIRE 528 0 176 0
WIRE -128 32 -128 0
WIRE 176 32 176 0
WIRE -288 112 -288 80
WIRE 0 112 0 0
WIRE 528 112 528 80
WIRE -128 160 -128 112
WIRE -64 160 -128 160
WIRE -16 160 -64 160
WIRE 176 160 176 112
WIRE 176 160 80 160
WIRE 256 160 176 160
WIRE 336 160 256 160
WIRE 336 176 336 160
WIRE 432 224 400 224
WIRE 464 224 432 224
WIRE 608 224 544 224
WIRE 624 224 608 224
WIRE 432 256 432 224
WIRE 336 336 336 272
WIRE 432 336 336 336
WIRE 624 336 624 304
WIRE 336 400 336 336
FLAG 336 400 0
FLAG -288 112 0
FLAG 528 112 0
FLAG 624 336 0
FLAG -64 160 PLoss3v3
FLAG 256 160 PLoss5v
FLAG 608 224 24V
SYMBOL voltage -288 -16 R0
WINDOW 123 0 0 Left 0
WINDOW 39 0 0 Left 0
SYMATTR InstName V1
SYMATTR Value 3.3
SYMBOL voltage 528 -16 R0
WINDOW 123 0 0 Left 0
WINDOW 39 0 0 Left 0
SYMATTR InstName V2
SYMATTR Value 5
SYMBOL voltage 624 208 R0
WINDOW 123 0 0 Left 0
WINDOW 39 0 0 Left 0
SYMATTR InstName V3
SYMATTR Value PULSE(0 24 1 0.0001 0.0001 5 10 2)
SYMBOL npn 400 176 M0
SYMATTR InstName Q1
SYMATTR Value 2N3904
SYMBOL res -144 16 R0
SYMATTR InstName R1
SYMATTR Value 4.7k
SYMBOL res 160 16 R0
SYMATTR InstName R2
SYMATTR Value 1.5k
SYMBOL res 560 208 R90
WINDOW 0 0 56 VBottom 2
WINDOW 3 32 56 VTop 2
SYMATTR InstName R3
SYMATTR Value 100k
SYMBOL res 416 240 R0
SYMATTR InstName R4
SYMATTR Value 6.8k
SYMBOL nmos 80 112 R90
SYMATTR InstName M1
SYMATTR Value BSS88/SIE
SYMATTR Prefix X
TEXT -320 424 Left 2 !.tran 10
TEXT -272 -96 Left 2 !.lib siemens.lib

Tracing the voltages, it's not even giving the 1.3 volts that I measure on the "real thing" :

image

Now, maybe the library that I found is bogus, but maybe I also forgot something here. 

One thing that I noticed is that the LTSpice symbol is not showing the "parasitic" diode on the N channel mosfet, while the application note clearly says that it's integral to the behavior of this arrangement.

Adding a single diode across the S and D makes the levels work properly, but then I figured that I could go with just a Schottky diode as I'm only ever interested in the 5V side pulling down the 3.3V side, not the other way around. A simple 1N5819 being enough, I'm all sorted, but I'm posting here in the hope of learning what I missed both in the simulation and the real life arrangement.

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 1 year ago +3
    I rather think that there may be an error in your model. I re-did from scratch and seen no problem. I used BSS123 which is in the LT Spice library. MK
  • michaelkellett
    michaelkellett over 1 year ago in reply to obones +3
    I tried it like this: MK
  • shabaz
    shabaz over 1 year ago in reply to obones +3
    Hi, SOT-23 are actually quite massive if you've not encountered them before, they are about the length of a small through-hole 1/8W resistor, and the pins are spaced quite far apart, see the photo below…
Parents
  • shabaz
    0 shabaz over 1 year ago

    This is quite tricky to follow because the earlier question links to another earlier question, so it's a chain of three discussions to try to understand the purpose. It maybe needs a diagram of your proposed solution in context of your entire system.

    Anyway, regarding the level conversion, I didn't understand the circuit, however I was more concerned that you mentioned that the Orange Pi crashed. That's worrying, and makes me wonder if some of the electrical signals or levels are not as expected, or if power is reaching devices through (say) GPIO when there is no power applied to the device, causing unexpected behaviour.

    In theory, you could just use some resistors to reduce the voltage levels (i.e. potential divider), e.g. use three resistors chained into a potential divider if you need separate outputs for 3.3V and 5V logic. But I'm not sure I'd do that if it were me. I think (since I don't understand the 24V source signal origin, and if it's really 24V, or has the capability to vary - by the way, make sure to configure the PIC input as a Schmitt trigger input) I'd rather use some additional circuitry, and it may as well be an optocoupler, just to completely isolate things. They are cheap.

    Secondly, I feel uncomfortable with the idea of connecting that signal to both the Pi and the PIC chip, because what's the device that's supposed to be in control and co-ordinate things? I think that device is supposed to be the PIC chip, acting as a sort of power management device, therefore, why not give it control of passing signals to the Pi as required. In other words, only translate the 24V signal to be used by the PIC, and the PIC can use GPIO to send a signal to the Pi as required. That way, the PIC is always in control, and won't pass on any input signal glitches to the Pi. It just seems more structured this way (but I don't know the detail).

    Thirdly, can the PIC run from 3.3V instead? That way, there's no need to worry about level translations between PIC and Pi at least (but if you do need to interwork 5V and 3.3V logic there in the PIC to Pi direction, then you can just use two resistors as a potential divider at that interface between PIC and PI).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dang74
    0 dang74 over 1 year ago in reply to shabaz

    I think he is okay now in terms of a working solution.  He replaced the MOSFET with a diode.  The anode would be directed to the 3.3V side and the cathode to the 5V side.  When the collector is 5V the diode will be off.  When the collector is 0V the diode conducts and roughly 0.7V will be present on the 3.3V side, which can generally be interpreted as logic 0.  The purpose of this post is to try and understand why the original method failed.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 1 year ago in reply to dang74

    I get that, but personally I don't like working like that. I'd rather know the background, in case things are being done unusually and if a different path should be chosen.

    In this case for instance, there's actually no need for this level conversion, if the microcontroller was run at 3.3V; and even if the level conversion is needed if the microcontroller can only run at 5V, there's no need to do a bidirectional implementation here (with all the shortcomings of this type of implementation), so things can be simplified further.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dang74
    0 dang74 over 1 year ago in reply to shabaz

    Fair point.  It's nice to have the full picture sometimes... and some posts (not this one) are so lacking in information it is next to impossible to offer any guidance.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • anniel747
    anniel747 over 1 year ago in reply to dang74
    This reply was deleted.
    • Cancel
    • Cancel
  • obones
    0 obones over 1 year ago in reply to shabaz

    Thing is, I already have a few PICs lying around doing nothing, so I'd rather use them than order yet another microcontroller. This is a hobbyist project, without any intent of replicating it even for a small series, so I'd rather use what I have at hand to reduce the electronic waste that is already in my "lab".

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dang74
    0 dang74 over 1 year ago in reply to anniel747

    LOL, not sure if this is a sincere request or if you are making the case that sometimes it isn't necessary to provide additional details.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • anniel747
    anniel747 over 1 year ago in reply to dang74
    This reply was deleted.
    • Cancel
    • Cancel
  • dang74
    0 dang74 over 1 year ago in reply to anniel747

    I think you already decided to replace the resistor because you know that the power supply won't function without it... but if you weren't sure and made a post asking for advice it would still make sense to provide some extra details... otherwise people won't feel comfortable offering advice.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dang74
    0 dang74 over 1 year ago in reply to anniel747

    Sorry, looks like some of the colour bands are burned off.  I am guessing you couldn't find a schematic.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • anniel747
    anniel747 over 1 year ago in reply to dang74
    This reply was deleted.
    • Cancel
    • Cancel
  • dang74
    0 dang74 over 1 year ago in reply to anniel747

    LOL, your first couple of posts had me thinking you were playing around... Ironically, I went 180 when you asked me to read the value... which seems foolish now... but thanks for letting me off the hook.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • dang74
    0 dang74 over 1 year ago in reply to anniel747

    LOL, your first couple of posts had me thinking you were playing around... Ironically, I went 180 when you asked me to read the value... which seems foolish now... but thanks for letting me off the hook.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • anniel747
    0 anniel747 over 1 year ago in reply to dang74

    I often see this type of questions on other sites. Another one is "help needed identifying a part" with an useless picture.

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dang74
    0 dang74 over 1 year ago in reply to anniel747

    It took me a while to get there... but I see now that you were mimicking some of the worse offenders.  LOL

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 1 year ago in reply to anniel747

    hehe I like how the creator was quite specific which blackness they were referring to, with the encircling and the four arrows because one arrow wasn't enough : )

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • anniel747
    0 anniel747 over 1 year ago in reply to shabaz

    Worst of all this one came from a clueless repair shop technician. On first repair he only replaced one relay and on first turn-on the second relay blew up generating conductive carbon bridges then burning up the ULN2003A.