Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Why is the Schottky diode being used in control circuit?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 26 replies
  • Answers 1 answer
  • Subscribers 336 subscribers
  • Views 2005 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Why is the Schottky diode being used in control circuit?

Humaninsane
Humaninsane 5 months ago

imageWhy is the Schottky diode being used in control circuit? and why is the 470nF cap is added at that voltage divider output? how is the Cap value 470nF calculated?

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett 5 months ago in reply to Humaninsane +3 suggested
    I think I can see what the ciruit is attempting: T103 switches T104 on and T104 connects R108 to the supply rail. R108 and R119 attenuate the signal by a factor of (180 + 10.2)/10.2. C111 makes a…
  • geralds
    geralds 5 months ago in reply to michaelkellett +2
    Hi simulation with Schottky diode: simulation without Schottky diode: The Schottky diode is important during switching off the transistors. Without Schottky it can produce very high…
  • geralds
    geralds 5 months ago in reply to Humaninsane +1
    Hi, I would say that the T103 is a simple switching transistor in a higher voltage-rated circuit. A BC846 would be too small at 60V. The microcontroller's output switches it on to measure the voltage…
Parents
  • dang74
    0 dang74 5 months ago

    Interesting question... this is what I think.  If the input is an AC signal the Schottky could be used as a halfwave rectifier of sorts to only pass the positive portion of the waveform.  The capacitor then is used to reduce the ripple.  It would be calculated using the formula: c=i/(f.vpp) where vpp represents the desired ripple level.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • dang74
    0 dang74 5 months ago

    Interesting question... this is what I think.  If the input is an AC signal the Schottky could be used as a halfwave rectifier of sorts to only pass the positive portion of the waveform.  The capacitor then is used to reduce the ripple.  It would be calculated using the formula: c=i/(f.vpp) where vpp represents the desired ripple level.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Humaninsane
    0 Humaninsane 5 months ago in reply to dang74

     If the input is an AC signal the Schottky could be used as a halfwave rectifier of sorts to only pass the positive portion of the waveform. - application is only DC (max 60V)

    The capacitor then is used to reduce the ripple.  It would be calculated using the formula: c=i/(f.vpp) where vpp represents the desired ripple level. - Vpp=50vpkpk ripple, i = max 5mA (given to ADCpin). what should i consider for F? 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Humaninsane
    0 Humaninsane 5 months ago in reply to Humaninsane

    can i just consider R118? Like this, image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dang74
    0 dang74 5 months ago in reply to Humaninsane

    Yes... but maybe use the 9.6k parallel equivalent like michaelkellett