FPGA
  • Technologies
  • More
FPGA
Blog John Beetem's IceStorm Notes
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: johnbeetem
  • Date Created: 10 Jul 2015 11:11 PM Date Created
  • Views 6571 views
  • Likes 4 likes
  • Comments 10 comments
  • icestorm
  • fpga
  • xxicc
Related
Recommended

John Beetem's IceStorm Notes

johnbeetem
johnbeetem
10 Jul 2015

Project IceStorm, by Clifford Wolf and Mathias Lasser, is an amazing project that has reverse-engineered the Lattice iCE40 FPGA's bitstream so that it's finally possible to write open-source FPGA design tools for a real FPGA.  I've been playing with IceStorm and its companion tool arachne-pnr (place & route) over the last few days and it's been loads of fun with very few problems.  I'm going to add IceStorm as a synthesis target for my XXICC (21st Century Co-design) project.  That will give me a complete open-source FPGA design system, something I've been wanting for decades.

 

This 'blog is for collecting links and notes for IceStorm so that others can find them quickly and easily.  I will be adding to it as I learn more.  This content is licensed under the Creative Commons Attribution-ShareAlike 3.0 Unported License so others can share it.

 

Here is the official Project IceStorm wiki: Project IceStorm

 

Here is my original IceStorm discussion here at element14: Project IceStorm: fully open-source FPGA tools for Lattice iCE40


IceStorm uses a Lattice iCEstick as a development board.  It's available for US$21 in the USA: Lattice Semiconductor: ICE40HX1K-STICK-EVN iCEstick Evaluation Kit.


Here are instructions for installing IceStorm and its companion tools: Projet IceStorm: le FPGA libéré! [the FPGA set free!].  The instructions are a combination of French and GNU/Linux.  The IceStorm steps are out of date, since IceStorm is now at GitHub.  Here are the specific steps for IceStorm:


1.  Install "libftdi-dev" so IceStorm can talk to iCEstick's FT2232H:


$ sudo apt-get install libftdi-dev


2.  You can install IceStorm anywhere, but the standard place is in "/opt".  You'll probably need to change permissions on "/opt" so you can write to it.


$ cd /opt/

 

3.  Clone IceStorm from GitHub:


$ git clone https://github.com/cliffordwolf/icestorm.git icestorm

 

4.  Make the IceStorm software.  Some of it is in C++11, so your GCC will need to support it (GCC 4.8.1 or later).  The "make" step builds textual chip databases using a Python program, which takes a while on a slow computer.


$ cd icestorm

$ make

$ sudo make install


That's it!  IceStorm is ready to go.


Here is a partial list of IceStorm programs.  Like many open-source projects, IceStorm does not have a lot of documentation.  The IceStorm wiki is your best starting point.  However, each program does have a way to print help.


icepack takes a FPGA configuration data in text form (usually from arachne-pnr) and packs it into a binary file for downloading.  Here is a typical icepack command:


$ icepack moebius.txt moebius.bin


To list icepack options, give the command "icepack -h".


iceprog downloads a bitstream to an iCE40 FPGA or to a serial flash.  Here is a typical iceprog command:


$ sudo iceprog moebius.bin


If you don't want to use sudo, you can add a "rules" file to "/etc/udev/rules.d": see udev rules file for FTDI FT2232D/H, FT232H, and Papilio DUO.


To list iceprog options, give the "iceprog" command with no arguments.  For an iCEstick, iceprog programs the serial flash and then resets the FPGA so that it programs itself from the serial flash.  You can't program the FPGA's internal SRAM directly because of the way the SPI interfaces are wired together.  It is possible to modify iCEstick to program SRAM directly, but you lose the serial flash chip.  The "iceprog" command with no arguments tells you how to do this.

  • Sign in to reply

Top Comments

  • johnbeetem
    johnbeetem over 11 years ago in reply to DAB +3
    Thank you for your comments. IceStorm isn't my project -- I'm just using the results. IceStorm's authors Clifford Wolf and Mathias Lasser are the ones who might need to watch their backs. IANAL, but I…
  • e14 Contributor
    e14 Contributor over 10 years ago +3
    Hi johnbeetem . Thank you for taking the time to publish your notes on this. It looks very promising!
  • shabaz
    shabaz over 11 years ago in reply to johnbeetem +2
    Hi John, I believe you're correct, in Europe it is possible to reverse engineer for the purposes of interoperability at interfaces (e.g. say between an industrial machine and its remote control unit).…
  • johnbeetem
    johnbeetem over 11 years ago

    IceStorm now supports the HX8K-CT256.  That's a pretty powerful chip.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • johnbeetem
    johnbeetem over 11 years ago

    I had the opportunity to talk to a Lattice engineer yesterday at the Embedded Systems Conference.  He had of course heard about IceStorm and I wasn't the first to ask about it.  He said that Lattice doesn't seem to have any issues about IceStorm -- everybody's he's talked to has been positive and nobody has said that they need to shut it down.  He sees it as an opportunity for new ideas in FPGA software rather than a threat to the company.

     

    My opinion is that IceStorm has raised the level of interest in Lattice FPGAs and that's got to help them.  Lattice sees huge opportunities ahead for cheap FPGAs.  Xilinx and Altera seem more interested in selling smaller numbers of much more expensive chips.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 11 years ago in reply to johnbeetem

    Hi John,

     

    I believe you're correct, in Europe it is possible to reverse engineer for the purposes of interoperability at interfaces (e.g. say between an industrial machine and its remote control unit). However, there are some caveats.

    If the manufacturer publishes interface specs, then it is not permissible to perform the reverse engineering since the specs are available. I don't think the specs have to be free of charge unfortunately, a fee

    can be charged for them. Perhaps it could be argued in some cases that the charge is too high and therefore prohibitive.

    Sometimes it is in the manufacturer's interest to publish specs, because the manufacturer may be worried that if people attempt to reverse engineer, then in the process they may accidentally unearth and learn more proprietary things than the manufacturer wants others to know. In that case, better to publish specs.

    The above is just a layman interpretation (since I'm not being paid for this advice hehe - otherwise I would study up to be sure), and therefore could be incorrect.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • johnbeetem
    johnbeetem over 11 years ago in reply to DAB

    Thank you for your comments.  IceStorm isn't my project -- I'm just using the results.  IceStorm's authors Clifford Wolf and Mathias Lasser are the ones who might need to watch their backs.  IANAL, but I believe the laws regarding reverse-engineering vary from country to country.  I have heard that in some European countries it's illegal to reverse-engineer a product to make an illegal copy, but it's OK to reverse-engineer a product for interoperability, i.e., to interface it to other hardware and/or software or to understand better how to use it.

     

    When I buy a chip like a microprocessor, I should be able to use anybody's compiler to generate code for it or even write my own compiler if I am so inclined.  IMO it should be the same for FPGAs and GPUs.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 11 years ago

    Be careful about reverse engineering devices.

    Some companies still consider their techniques proprietary even if you figure them out on your own.

     

    So you might want to check with the original maker of the FPGA to see if they have any problems with you making your open source version of their product.

     

    Just a thought,

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<