FPGA
  • Technologies
  • More
FPGA
Blog Learning AMD Zynq: a project to generate a set of PWM signals. 1 - problem statement and possible approach
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 21 Apr 2023 11:42 AM Date Created
  • Views 5770 views
  • Likes 12 likes
  • Comments 36 comments
  • pynq-z2
  • amdzynqultrasoundpulse
  • zynq
  • fpga
  • vivado
  • vhdl
  • pynq
  • spartan
Related
Recommended

Learning AMD Zynq: a project to generate a set of PWM signals. 1 - problem statement and possible approach

Jan Cumps
Jan Cumps
21 Apr 2023
Learning AMD Zynq: a project to generate a set of PWM signals. 1 - problem statement and possible approach

 yepe has to resolve this problem for a project assignment:

Hi Jan Cumps, I hope you don't mind if I ask a question regarding the PYNQ half-bridge PWM driver. I am working on a student project for school and I need to drive a half-bridge for an ultrasound pulser. I was working through your great tutorial and I had the complementary pwm output on my board PYNQ Z1. However, I have to make certain changes to the operation to make it compatible with my needs which I attempted to do, but I could not determine the best approach. First off, I need to simplify that I only need 50% duty cycle and no other duty cycles needed. I have made a timing diagram for the various waveforms:
image

CLK should be a continuous 20 MHz signal, PRF should be a 10 kHz 50% duty cycle signal that synchronizes the rest of the waveforms. PWM&PWMN are the complementary PWM signals with dead-time of programmable N cycles with a timed delay from a falling edge of PRF. PULSE should be equal to the length of the PWM pulse train, and GATE is equal to pulse but with a programmable delay. The PWM pulse-train should be 5 MHz. The first thing I tried to do is to change your example to see if I could get a 5 MHz complementary PWM but I could not see how the frequency is determined so I was playing around with the board clocks and only could get it up to 650 kHz.

I am a biginner at vhdl so I am a bit out of my element. I have developed all the electronics and analogue demodulation circuits but I still lack the control system to tie it together. If I were to implement these signals in the PYNQ, where do you propose to start?

My suggestion is to cut the task in simple(r) chunks:

I think that the easiest way to achieve this, as beginner, is to eat the elephant in pieces. Ignore my code, because it's not the basis for what you need.

  • make a design that can generate the clock. Confirm by probing.
  • make a design that can generate one of the easy signals, based on that clock. PWM maybe? If you can make that clock, you know that you'll be able to generate the slower ones too (edit jc: the max frequency will a function of the resolution of the dead time).
  • add PWMN to the design. That should be easy, because it's NOT PWM
  • try a separate design with the PRF logic. If you have that working, add to the original one (or keep separate, feeding it from the same clock?)
  • same for the remaining ones.

image

The advantage of little steps is that you'll get early success, and that boosts the morale.
Advantage of separate blocks for a beginner is that the code stays separate and graspable. 

The main job for each signal will will be to:

  • find out after how many ticks of the clock the signal should change
  • count the clock ticks and compare it to the figure(s) figured out above
  • set the output(s) to the desired state.

If you'd handle this different, comment below.

Capture of status after post 2:

image

link to all posts.

  • Sign in to reply

Top Comments

  • michaelkellett
    michaelkellett over 3 years ago in reply to Jan Cumps +1
    Looks to me as if it would be much better with maybe 100MHz internal clock - if the 20MHz is a fixed thing from outside then use an FPGA PLL to get up to 100M (or more). You can get really sassy with…
  • michaelkellett
    michaelkellett over 3 years ago in reply to yepe +1
    Much clearer now - thanks I'll leave Jan to get on with helping (mostly ), otherwise it'll get confusing. MK
  • yepe
    yepe over 3 years ago in reply to Jan Cumps +1
    Hi, sorry for the late response. The delay between the falling edge of the PRF and the beginning of the pulse train should be such that the end of the pulse-train is the same as the end of the low…
  • Jan Cumps
    Jan Cumps over 3 years ago

    last questions of the day:

    • the delay between PRF falling edge and the start of the pulse train, do you have an idea of the order of magnitude?
    • how many pulses in a train? Is that always 2, varying, or an other number that can be predefined during the design?
    • the delay between PRF rising edge and GATE rising edge?
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to Jan Cumps

    Results:

    Here's the start of the train. You see PWM on channel A, PULSE on channel B
    image

    end of the train, first one showing PWM and PULS, 2nd one showing PWMN and PULSE (working with a 2 channel scope at the moment)

    image image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to Jan Cumps

    when driven from Pynq, it will not be in sync with the clock, but for testing it's OK.

    Once you get this enabled signal from the VHDL control logic, It will rise right when the PWM gets enabled, and fall when the PWM stops.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to Jan Cumps

    the PULSe signal could be identical to the Enable from the previous comment. 
    I'll try if that works ...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago

    To disable the PWM, you could putand AND gate at output A, and an OR gate at output B.
    Link the other input of A to a enable signal that you can control.
    And the other input of B to the inverted enable signal.
    This would cause that A was always LOW, and B always HIGH, when disabled.

    I've taken another approach: add an enable input to the PWM generator:

    library IEEE;
    use IEEE.std_logic_1164.all;
    
    package PulsePckg is
    
      constant HI   : std_logic := '1';
      constant LO   : std_logic := '0';
      constant ONE  : std_logic := '1';
      
    component Pwm is
      generic (
        resolution : integer := 6; -- bit width of the counter used for duty cycle
        duty_bits : integer := 4   -- bit width of the variable that holds the desired deadband 
      );
      port (
        n_reset_i : in  std_logic;          -- async reset
        enable_i : in  std_logic;           -- enable the outputs
        clk_i  : in  std_logic;             -- Input clock.
        duty_i : in  std_logic_vector (resolution - 1 downto 0);      -- Duty-cycle input.
        band_i : in  std_logic_vector (duty_bits - 1  downto 0);      -- number of clock-ticks to keep both signals low before rising edge
        pwmA_o  : out std_logic;            -- PWM output.
        pwmB_o  : out std_logic             -- PWM output inverse.
        );
    end component;  
    
    end package;
    
    --*********************************************************************
    -- PWM module.
    --*********************************************************************
    
    library IEEE;
    use IEEE.MATH_REAL.all;
    use IEEE.std_logic_1164.all;
    use IEEE.numeric_std.all;
    use WORK.PulsePckg.all;
    
    entity Pwm is
      generic (
        resolution : integer := 6;
        duty_bits : integer := 4
      );
      port (
        n_reset_i : in  std_logic;          -- async reset
        enable_i : in  std_logic;           -- enable the outputs
        clk_i  : in  std_logic;             -- Input clock.
        duty_i : in  std_logic_vector (resolution - 1 downto 0);      -- Duty-cycle input.
        band_i : in  std_logic_vector (duty_bits - 1 downto 0);      -- number of clock-ticks to keep both signals low before rising edge
        pwmA_o  : out std_logic;            -- PWM output.
        pwmB_o  : out std_logic             -- PWM output inverse.
        );
    end entity;
    
    architecture arch of Pwm is
      signal timer_r       : natural range 0 to 2**duty_i'length-1;
    begin
    
      clocked: process(clk_i, n_reset_i)
      begin
        pwmA_o   <= LO;
        pwmB_o   <= LO;
       
        -- async reset
        if n_reset_i = '0' then
            timer_r <= 0;
           
        elsif rising_edge(clk_i) then
          -- timer
          timer_r <= timer_r + 1;
        if enable_i = '0' then
          pwmB_o   <= HI;
        
        else
          -- output a
          if timer_r <= unsigned(duty_i) and timer_r >= unsigned(band_i)  then
            pwmA_o <= HI;
          end if;
          -- output b
          if timer_r > to_integer(unsigned(band_i)) + to_integer(unsigned(duty_i)) then 		
            pwmB_o <= HI;
          end if;
        end if; -- enable
        end if; -- rising_edge
      end process clocked;
      
      
    end architecture;

    I've added a new register that can hold 32 flags. Position 0 reserved for the enabled flag. The rest (currently) unused:

    image

    Helper function:

    image

    The register is only to test it in Pynq. In your design, you would enable it in the VHDL block (not existing yet :) ) that also controls the other signals.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>