FPGA
  • Technologies
  • More
FPGA
Forum Altera EP4CE6 Mini Board I/O?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 584 subscribers
  • Views 908 views
  • Users 0 members are here
Related

Altera EP4CE6 Mini Board I/O?

vwolff
vwolff over 6 years ago

I was discussing the FPGA development board (Altera EP4CE6 Mini Board ) with John Wiltrout. I am able to execute and load the blinking LED demo "My First FPGA Design Tutorial" (see attached file).  I can enter different programs and make them blink in different patterns.  I have not successfully toggled an IO pin. For instance I want to toggle IO pin one, so I enter FPGA pin_87 which, I believe corresponds to Expansion Connector pin number one. I get nothing.   Any suggestions?

 

image

Thanks,

Von

Attachments:
imagett_my_first_fpga.pdf
imageEP4CE6-Mini-Board-Hardware-Users-Guide.pdf
  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 6 years ago +2
    I've not used an Altera chip so apologies if this is stuff you've already checked and ruled out, but I think if you're following that guide, page 1-36 and the surrounding pages are where you map the HDL…
  • michaelkellett
    michaelkellett over 6 years ago in reply to jw0752 +2
    Thanks John, been away a couple of days so missed this ! @Von, I assume you are using Altera Quartus software. Could you please let me know which version - if relatively recent the easiest thing is for…
Parents
  • shabaz
    shabaz over 6 years ago

    I've not used an Altera chip so apologies if this is stuff you've already checked and ruled out, but I think if you're following that guide, page 1-36 and the surrounding pages are where you map the HDL signal names to the physical pins. But I presume you've done that.

    It might be worth double-checking what the 'I/O Standard' setting is for the pins (it is in the screenshot on page 1-36 and 1-38). If there is a 3.3V logic level setting then that should be selected I'm guessing. Are no warnings or errors generated, and is there some summary report the Altera software generates? (It may be a text file it dumps in a folder). If so, that should contain the mappings, and the 'I/O Standard' values too, for double-checking.

    How is the output pin being examined, with an LED, or (say) a logic analyzer?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 6 years ago

    I've not used an Altera chip so apologies if this is stuff you've already checked and ruled out, but I think if you're following that guide, page 1-36 and the surrounding pages are where you map the HDL signal names to the physical pins. But I presume you've done that.

    It might be worth double-checking what the 'I/O Standard' setting is for the pins (it is in the screenshot on page 1-36 and 1-38). If there is a 3.3V logic level setting then that should be selected I'm guessing. Are no warnings or errors generated, and is there some summary report the Altera software generates? (It may be a text file it dumps in a folder). If so, that should contain the mappings, and the 'I/O Standard' values too, for double-checking.

    How is the output pin being examined, with an LED, or (say) a logic analyzer?