FPGA
  • Technologies
  • More
FPGA
Forum Questions about the AVNET Network FMC Module
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 584 subscribers
  • Views 1416 views
  • Users 0 members are here
Related

Questions about the AVNET Network FMC Module

jb-ch
jb-ch over 5 years ago

Hello,

 

I am Jean-Baptiste and I am currently working on ip designs for Ethernet based network. I currently have a setup with a Netpga CML card on which is plugged the Avnet Network FMC module.

https://www.avnet.com/shop/us/products/avnet-engineering-services/aes-fmc-netw1-g-3074457345635205181/

 

The entire design is pure VHDL thus there is no SW part.

The vadj is set to 1.8V and the power led on the network FMC module shows that vadj value on the dedicated leds.

I am able to properly use part of the board but I do have some issues using this setup.

 

1) I am running the same MDC/MDIO configuration on port 1 and port 2 of the Avnet Network FMC. Only Port 1 is up and running (I can see Ethernet traffic with wire-shark). However, the second port remains inactive and the activity leds are not showing anything (doesn't matter the applied speed 10/100/1000 Mbit/s).

2) The users leds on the boards are not very bright, it seems that there is not enough intensity in the applied power signal.

 

Is anyone has experimented some similar issue using this avnet ethernet fmc module?

(Note that I have tried to remove Q1 as described in the Erratum but it doesn't fix my issue with port 2).

 

Many thanks,

Best regards,

Jean-Baptiste

  • Sign in to reply
  • Cancel
Parents
  • jafoste4
    jafoste4 over 5 years ago

    Hi Jean,

     

    Are you trying to use both ports at the same time? If you try to just use port 2 does it work? Or is it an issue with using both at the same time?

     

    -Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • jafoste4
    jafoste4 over 5 years ago

    Hi Jean,

     

    Are you trying to use both ports at the same time? If you try to just use port 2 does it work? Or is it an issue with using both at the same time?

     

    -Josh