FPGA
  • Technologies
  • More
FPGA
Forum AMD and Xilinx
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 583 subscribers
  • Views 1603 views
  • Users 0 members are here
  • fpga
Related

AMD and Xilinx

mp2100
mp2100 over 5 years ago

https://www.amd.com/en/press-releases/2020-10-27-amd-to-acquire-xilinx-creating-the-industry-s-high-performance-computing

  • Sign in to reply
  • Cancel

Top Replies

  • Gough Lui
    Gough Lui over 5 years ago +2
    Intel versus AMD all over again, just in the FPGA space as opposed to the CPU space? - Gough
  • Gough Lui
    Gough Lui over 5 years ago in reply to DAB +2
    Well, when Intel acquired Altera, my hope was that FPGA acceleration would become mainstream and that even regular CPUs may start shipping with FPGA logic units to accelerate specific tasks. Sadly, even…
  • Gough Lui
    Gough Lui over 5 years ago in reply to Gough Lui +2
    As it turns out, just recently, AMD patented a hybrid CPU+FPGA architecture which might be enabled by Xilinx technology ... perhaps AMD following a similar path will really cement the hybrid design as…
Parents
  • Gough Lui
    Gough Lui over 5 years ago

    Intel versus AMD all over again, just in the FPGA space as opposed to the CPU space?

     

    - Gough

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • DAB
    DAB over 5 years ago in reply to Gough Lui

    I think there is a lot more to it.

    AMD is seeking to enter more areas of chip design and FPGA technology allows them to bundle their current chipsets with specific targeted capability for more applications.

     

    It will be very interesting to see what they do with there added technology and IP.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • DAB
    DAB over 5 years ago in reply to Gough Lui

    I think there is a lot more to it.

    AMD is seeking to enter more areas of chip design and FPGA technology allows them to bundle their current chipsets with specific targeted capability for more applications.

     

    It will be very interesting to see what they do with there added technology and IP.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Gough Lui
    Gough Lui over 5 years ago in reply to DAB

    Well, when Intel acquired Altera, my hope was that FPGA acceleration would become mainstream and that even regular CPUs may start shipping with FPGA logic units to accelerate specific tasks. Sadly, even after all these years, it seems only some very high-end chips from Intel have such FPGA and CPU hybrid designs (limited to a few Xeons as far as I've seen).

     

    Another hope of mine was that it would be the first step towards abstracting FPGA acceleration into something more modular, easy to use and scalable in a similar way to how the x86/x86-64 instruction set has made CPUs from Intel and AMD virtually interchangeable (at least on a superficial level), and how OpenCV had "cured" the ill that was CUDA which was Nvidia's proprietary GPU compute architecture, bringing GPU compute capabilities to cross between vendors. I personally haven't seen such efforts with FPGAs - perhaps the hardware-specific connection makes it a little difficult and we are still in the infancy of potential CPU + FPGA hybrid processing.

     

    I've heard for years that many large-scale cloud operations have always had interest in virtually anything that can accelerate processing. I just hope that AMD pushes it harder than Intel does, since Intel's not had the best track record as of late with all the speculative execution issues, but also with their retreat from mobile and IoT to some degree ... AMD is definitely in a formidable position when it comes to CPUs at the moment. I'm just so happy that they managed to survive Intel's anti-competitive behaviour for so long and come up with a line of CPUs that really pull their weight whether you're looking for performance, value for money or energy efficiency. Their GPU division is perhaps not quite as successful ... perhaps it is next to see a revival. How the FPGAs will slot into their portfolio is definitely going to be interesting to observe.

     

    - Gough

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Gough Lui
    Gough Lui over 5 years ago in reply to Gough Lui

    As it turns out, just recently, AMD patented a hybrid CPU+FPGA architecture which might be enabled by Xilinx technology ... perhaps AMD following a similar path will really cement the hybrid design as a new frontier perhaps to be standardised and leveraged for complex tasks.

     

    - Gough