Products
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
FPGA
  • Technologies
  • More
FPGA
Forum 四种常用FPGA/CPLD设计思想与技巧(2)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 0 replies
  • Subscribers 582 subscribers
  • Views 165 views
  • Users 0 members are here
Related

四种常用FPGA/CPLD设计思想与技巧(2)

vhe1981
vhe1981 over 15 years ago

当向一块RAM写数据的时候,从另一块RAM读数据,然后送到处理单元处理,此时每块RAM的容量仅需2560位即可,2块RAM加起来也只有5120位的容量。

image

另外,巧妙运用乒乓操作还可以达到用低速模块处理高速数据流的效果。如图2所示,数据缓冲模块采用了双口RAM,并在DPRAM后引入了一级数据预处理模块,这个数据预处理可以根据需要的各种数据运算,比如在WCDMA设计中,对输入数据流的解扩、解扰、去旋转等。假设端口A的输入数据流的速率为100Mbps,乒乓操作的缓冲周期是10ms。以下分析各个节点端口的数据速率。

 

A端口处输入数据流速率为100Mbps,在第1个缓冲周期10ms内,通过“输入数据选择单元”,从B1到达DPRAM1。B1的数据速率也是100Mbps,DPRAM1要在10ms内写入1Mb数据。同理,在第2个10ms,数据流被切换到DPRAM2,端口B2的数据速率也是100Mbps,DPRAM2在第2个10ms被写入1Mb数据。在第3个10ms,数据流又切换到DPRAM1,DPRAM1被写入1Mb数据。

 

仔细分析就会发现到第3个缓冲周期时,留给DPRAM1读取数据并送到“数据预处理模块1”的时间一共是20ms。有的工程师困惑于DPRAM1的读数时间为什么是20ms,这个时间是这样得来的:首先,在在第2个缓冲周期向DPRAM2写数据的10ms内,DPRAM1可以进行读操作;另外,在第1个缓冲周期的第5ms起(绝对时间为5ms时刻),DPRAM1就可以一边向500K以后的地址写数据,一边从地址0读数,到达10ms时,DPRAM1刚好写完了1Mb数据,并且读了500K数据,这个缓冲时间内DPRAM1读了5ms;在第3个缓冲周期的第5ms起(绝对时间为35ms时刻),同理可以一边向500K以后的地址写数据一边从地址0读数,又读取了5个ms,所以截止DPRAM1第一个周期存入的数据被完全覆盖以前,DPRAM1最多可以读取20ms时间,而所需读取的数据为1Mb,所以端口C1的数据速率为:1Mb/20ms=50Mbps。因此,“数据预处理模块1”的最低数据吞吐能力也仅仅要求为50Mbps。同理,“数据预处理模块2”的最低数据吞吐能力也仅仅要求为50Mbps。换言之,通过乒乓操作,“数据预处理模块”的时序压力减轻了,所要求的数据处理速率仅仅为输入数据速率的1/2。

 

通过乒乓操作实现低速模块处理高速数据的实质是:通过DPRAM这种缓存单元实现了数据流的串并转换,并行用“数据预处理模块1”和“数据预处理模块2”处理分流的数据,是面积与速度互换原则的体现!

 

串并转换设计技巧

 

串并转换是FPGA设计的一个重要技巧,它是数据流处理的常用手段,也是面积与速度互换思想的直接体现。