FPGA
  • Technologies
  • More
FPGA
Forum Interfacing a circuit in an FPGA to a PC.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 583 subscribers
  • Views 970 views
  • Users 0 members are here
  • tutorial
  • electronic
  • firmware
  • gate
  • experimental
  • apl
  • fpga
  • usb
  • vhdl
  • Technology
  • instrumentation
  • usb2
  • altera
  • array
  • field
  • software
  • programmable
  • instrument
Related

Interfacing a circuit in an FPGA to a PC.

e14 Contributor
e14 Contributor over 14 years ago

If you have an interest in exchanging data between circuitry in an FPGA and a PC, I have written a simple GUI that demonstrates transfers at full USB2 rates to and from an FPGA interfaced with an FTDI FT2232H USB2 interface chip (i.e. the  FTDI Morph-IC-II) :

image

There is a free (binary only) download :

   http://www.lab-tools.com/instrumentation/download/FPGA_PC_Release_TF.zip ,

or source code is available for both personal and commercial uses : i.e. (Altera Quartus II v11.1sp2 archive) plus Apl script source plus APl GUI binary or source.


There is a help page at :

   http://www.lab-tools.com/instrumentation/soft-firm-hard-ware/FPGA_interface_to_PC/help.html

and a YouTube video putting this code through its paces at :

   http://youtu.be/EqLJBdtOvYY

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

These demonstrate a fast way of getting PC access to firmware circuitry in a Field Programmable Gate Array (FPGA).

Pre-written VHDL firmware and array-based software facilitate interfacing a PC to the FPGA over the USB, and gives transparent access to multiple banks of sub-modules and instrument functions in the FPGA at full USB2 rates of 480 Mbit/s (60 MBytes/s).

 

The heart of this code is the Lab-Tools FPGA Modular Firmware Skeleton for multiple instruments.


Each sub-module has an independent block of up to 256 USB interface registers, to configure the sub-instrument and for bi-directional data transfer. This Lab-Tools code forms the skeleton into which the sub-modules / instruments may be slotted, in a consistent manner.

Attachments:
FPGA_PC_Release_TF.zip
  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    I have slightly updated the GUI to Version 0.95 - it should now have some slight functionality even if you do not have a Morph-IC-II FPGA module plugged in.

     

    Note you will first need to download and install the APLX Support Library from MicroApl : http://www.microapl.co.uk/apl/player/index.html .

    Also, if you run Norton, it will probably complain that the .exe file is infected - the file is not infected, but it is a powerful piece of code, as it has to access a number of .dlls to program and interface to the FPGA.