FPGA
  • Technologies
  • More
FPGA
Forum Project IceStorm: fully open-source FPGA tools for Lattice iCE40
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 36 replies
  • Subscribers 583 subscribers
  • Views 26258 views
  • Users 0 members are here
  • floss
  • icestorm
  • fpga
  • ice40
  • yosys
Related

Project IceStorm: fully open-source FPGA tools for Lattice iCE40

johnbeetem
johnbeetem over 11 years ago

As some of you may have noticed, I've been obsessed for many decades with having open FPGA bitstream documentation so that people can write their own FPGA designs tools, especially FLOSS (Free-as-in-Liberty Open Source Software).

 

I recently found out about IceStorm, a project that has somehow reverse-engineered and documented the Lattice iCE40 FPGA.  They've actually put together a fully-open-source tool chain with Yosys for Verilog synthesis and Arachne_pnr for placement and routing.  I don't know how usable or robust the tools are.  I'm planning on taking a close look starting next month.

 

If you're interested, here's the IceStorm link, which has links to the other tools: Project IceStorm

Discussion of Yosys and the tools is at reddit: Yosys Open SYnthesis Suite

 

Update: Here are a couple of nice Hackaday items about IceStorm:

 

From 29 March 2015: Reverse Engineering Lattice’s iCE40 FPGA Bitstream | Hackaday

From 29 May 2015: An Open Source Toolchain For iCE40 FPGAs | Hackaday

 

Update 2: Here are some good IceStorm installation instructions: Projet IceStorm : le FPGA libéré ! | Front de Libération des FPGA.  They're in a combination of French and GNU/Linux.

 

Here's the Lattice IceStick directly supported by IceStorm: Lattice Semiconductor: ICE40HX1K-STICK-EVN iCEstick Evaluation Kit.  It's US$20.89 in the USA.

  • Sign in to reply
  • Cancel

Top Replies

  • johnbeetem
    johnbeetem over 10 years ago +2
    I found out from a friend about another iCE40 board: Olimex iCE40HX1K-EVB It's a tiny board (5x5 cm or 2"x2") with an iCE40HX1K-VQ100, 256K x 16 SRAM, 16 Mb serial flash, 2 buttons, 2 LEDs, oscillator…
  • diablero
    diablero over 10 years ago in reply to johnbeetem +2
    A new board. Does the World Need an FPGA Arduino? | Hackaday
  • michaelkellett
    michaelkellett over 10 years ago in reply to johnbeetem +2
    My thinking was that if you are going to buy a board you could expect it to be made on a production line and almost any would be able to place BGAs. You can use one of Lattice's sparsely pinned BGAs on…
Parents
  • johnbeetem
    johnbeetem over 11 years ago

    iCEstick is now US$30.02 and out of stock at Newark (USA).  I don't know why it went up so much.  It's still US$21.86 at Lattice Semiconductor site.

     

    IceStorm now supports the iCE40-HX8K with 7680 logic cells, which is 6 times the capacity of the HX1K with 1280 logic cells.  You can get an HX8K breakout board for US$42.88 at Lattice Semiconductor site.  It's not listed at Newark.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • johnbeetem
    johnbeetem over 11 years ago

    iCEstick is now US$30.02 and out of stock at Newark (USA).  I don't know why it went up so much.  It's still US$21.86 at Lattice Semiconductor site.

     

    IceStorm now supports the iCE40-HX8K with 7680 logic cells, which is 6 times the capacity of the HX1K with 1280 logic cells.  You can get an HX8K breakout board for US$42.88 at Lattice Semiconductor site.  It's not listed at Newark.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • michaelkellett
    michaelkellett over 11 years ago in reply to johnbeetem

    The HX8K is big enough to do useful work although its lack of multipliers is a pain. It comes in BGA only -  the 132 ball 0.5mm pitch part is quite cheap but requires the use of exotic design rules to use all the pins. I think the OSHPark multi layer design rules will allow you to get one running and use most of the IO.

    The part is also available in 0.8mm pitch 256 ball BGA which might allow easier design rules but I haven't tried.

     

    I do wish Lattice would make ALL the ICE40xxxx parts available in TQFP - I'm sure it would increase the number of design ins quite a lot.

     

    MK