FPGA
  • Technologies
  • More
FPGA
Forum Lattice XP2 Brevia Dev Kit - How to Connect an parallel ADC?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 12 replies
  • Answers 2 answers
  • Subscribers 582 subscribers
  • Views 3055 views
  • Users 0 members are here
Related

Lattice XP2 Brevia Dev Kit - How to Connect an parallel ADC?

msliva
msliva over 10 years ago

Have some of you an example "How to Connect an parallel ADC to the Lattice XP2 Brevia Dev Kit"?

 

It could be parallel ADC 10-16 bit, 20 MSPS or higher.

 

Thanks in advance!

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 10 years ago in reply to msliva +2 suggested
    Here is a schematic of how to connect the AD9200 to the Brevia - I don't think this will work on prototype boards because you need a physical layout good at 100MHz or more (because of the bandwidth of…
  • michaelkellett
    michaelkellett over 10 years ago +1 suggested
    For the benefit of others I've suggested that Mira bring his problem here so that he can benefit from the wisdom of the E14 collective ! I've already suggested the Analog Devices AD9200 Farnell sell the…
Parents
  • michaelkellett
    0 michaelkellett over 10 years ago

    For the benefit of others I've suggested that Mira bring his problem here so that he can benefit from the wisdom of the E14 collective !

     

    I've already suggested the Analog Devices AD9200 Farnell sell the  AD9200JRSZAD9200JRSZ for£3.02 for one This is the 0-70C version in 28 pin SOP package It's quite an old design(pre 1999 but has some interesting spec features

    • 10 bit
    • 20 MHz max sampling rate
    • 300 MHz sample and  hold (which means it can be use din undersampling mode to look at signals with frequencies above 20MHz)
    • Parallel interface
    • Cheap

    As is usual with parts from Analog Devices there is a lot of useful background information in the data sheet and it is well worth studying it carefully.

    AD recommend using an AD8041 op amp to drive the ADC input and this is also available from Farnell in DIP or SO packages. We can use the same 3.3V supply for the ADC and the Op Amp and we'll go for a +/- 5V full scale input range.

    In order to use these parts you can use surface mount adapter boards Farnell do the Roth range so we could use  RE931-05RE931-05 at£5.14 and  RE932-01RE932-01 for the op amp at£3.52

    It would be much nicer to design a pcb but then you would need to get some made which will cost some money and take a little time. Because the parts need to work at high frequencies  I would go for a pcb - fast delivery double sided boards 50mm square would cost me £37.80 for 1 board, 24 hour production. The Roth prototype board construction will save about £30 but is much harder to get right (lots of messy wires and little components hanging in the air).

     

    I don't have time do any more on this right now so please reply and let me know if you would rather a design based on a proper pcb and if the +/- 5V range is good.

     

    Once we have a physical design it's possible to work on the FPGA logic - actually you have to think a bit about that as you do the circuit so you don't end up using pins on the FPGA that will never work for your application.

     

    Do you want to write the logic for the FPGA in VHDL or Verilog (hint - I only use VHDL !!)

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • msliva
    0 msliva over 10 years ago in reply to michaelkellett

    Hello Michael,

     

    Thank you very much for your time and analysis.

    I would like to try it with surface mount adapter boards. For me is +/- 5V range good.

    I want to write the logic for the FPGA in VHDL.

     

    Thanks in advance!

     

    MS

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 10 years ago in reply to msliva

    OK - I've ordered some bits - they should arrive on 5th by which time I will have drawn a circuit diagram.

     

    How do you want to get the data out of the FPGA and what will you do with it ?

    (The Brevia board has an FTDI USB chip which supports COM port emulation.)

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • msliva
    0 msliva over 10 years ago in reply to michaelkellett

    In the first step I want to use only COM port emulation.

     

    MS

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 10 years ago in reply to msliva

    Here is a schematic of how to connect the AD9200 to the Brevia - I don't think this will work on prototype boards because you need a physical layout good at 100MHz or more (because of the bandwidth of the amplifier) . The AD9200 really needs an additional buffer amp for biasing which I have shown here. All the capacitors are 0603 surface mount except the two 10uF which are 0805. If you are still interested let me know and I'll lay out a pcb. To build it you'll need to get some pcbs made but from OSHPARK or similar they won't be very expensive.

     

    R2 loops an FPGA pin back to one of its PLL inputs so we can generate an FPGA clock at a suitable frequency.

    image

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • msliva
    0 msliva over 10 years ago in reply to michaelkellett

    Thank you very much. Can you post VHDL code here?

    I personally don't need PCB layout yet. I want to use example with low frequency signals.

     

    MS

     

    P.S. U2 should be AD8041?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • msliva
    0 msliva over 10 years ago in reply to michaelkellett

    Thank you very much. Can you post VHDL code here?

    I personally don't need PCB layout yet. I want to use example with low frequency signals.

     

    MS

     

    P.S. U2 should be AD8041?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • michaelkellett
    0 michaelkellett over 10 years ago in reply to msliva

    Hello,

     

    It should be AD8041.

     

    If you only want to use low frequencies the AD9200 is completely the wrong part to use.

    Please tell me what you are trying to measure, what sample rate you need and how many bits resolution. At lower frequencies there are much cheaper and easier to use parts than the AD9200.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • msliva
    0 msliva over 10 years ago in reply to michaelkellett

    Hello,

     

    I need only functional example HW+VHDL yet. I am willing to spend £3.02 (AD9200) for learning purposes. It is no problem. I wrote about low frequences for which is possible to use "surface mount adapter boards" such as RE931-05.

     

    MS

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 10 years ago in reply to msliva

    Real life doesn't work like that - the ADU8041 and the AD9200 are high frequency parts and they need to be treated as such even if you wok them at low frequencies. The AD9200 is a pipelined synchronous ADC and it doesn't work the same way as lower speed ADCs.

    If you just want to learn how to get his kind of stuff to work I think we would do much better starting with a nice slow ADC like MCP3008 or MCP3001 - that way we can keep the hardware nice and simple can concentrate on the other stuff.

     

    MK