FPGA
  • Technologies
  • More
FPGA
Forum Altera/Terasic DE1 Output Voltage
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 5 replies
  • Answers 3 answers
  • Subscribers 583 subscribers
  • Views 1191 views
  • Users 0 members are here
Related

Altera/Terasic DE1 Output Voltage

djfraz
djfraz over 8 years ago

I am working on a project for university using Altera/Terasic DE1 Cyclone ii Starter Board. I am trying to test a servo module, the output waveform is as expected, but the output voltage is only about 5mV. Can someone give me a simple answer as to how i can change the output voltage which the board is supplying?

  • Sign in to reply
  • Cancel

Top Replies

  • djfraz
    djfraz over 8 years ago in reply to johnbeetem +1
    It was first connected to a servo, but when i wasn't seeing any movement (i had the pulse width controlled by onboard switches) i connected it directly to my oscilloscope. I was seeing the correct pulse…
Parents
  • johnbeetem
    0 johnbeetem over 8 years ago

    Rachel is correct about driving coils.  You usually can't drive a coil (or motor or speaker) directly from an FPGA output because you usually need more current than a typical FPGA can source or sink.  You also must make sure you have a flyback diode.  The current through an inductor cannot be shut off instantaneously, and if you try to do this you get a large voltage spike.  The flyback diode provides an alternate path for this current so the voltage spike doesn't destroy the transistor you're using to switch current on and off.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • johnbeetem
    0 johnbeetem over 8 years ago

    Rachel is correct about driving coils.  You usually can't drive a coil (or motor or speaker) directly from an FPGA output because you usually need more current than a typical FPGA can source or sink.  You also must make sure you have a flyback diode.  The current through an inductor cannot be shut off instantaneously, and if you try to do this you get a large voltage spike.  The flyback diode provides an alternate path for this current so the voltage spike doesn't destroy the transistor you're using to switch current on and off.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer