FPGA
  • Technologies
  • More
FPGA
Forum Looking for the right FPGA
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 3 replies
  • Answers 2 answers
  • Subscribers 582 subscribers
  • Views 755 views
  • Users 0 members are here
  • mos
  • commodore
  • fpga
  • 6526
  • vhdl
  • commodore_64
  • fpga developement
Related

Looking for the right FPGA

ajkatz83
ajkatz83 over 8 years ago

 

Hey all!

 

Been working a bit in the 8-bit world, especially with the Commodore machines, the 64 and SX-64 and I have noticed there have been some folks out there who have replaced some of the chips with FGPAs. I know I am crazy for thinking this, however, I am curious to see if that can be done. I have never used an FPGA nor VHDL, which seems to be the machine language necessary to make this all work. I was using my one machine the other day and the CIA (complex Interface Adapter) basically blew up and stripped me of the two I had for "just in case." I saw one fellow trying to do such a project more than a year ago, and I feel rather inspired.

 

For the specs below (off the datasheet) What kind of FPGA would be necessary?

 

FEATURES · 16 Individually programmable I/O lines · 8 or 16-Bit handshaking on read or write · 2 independent, linkable 16-bit interval timers · 24-hour (AM/PM) time of day clock with programmable alarm · 8-Bit shift register for serial I/O · 2TTL Load capability · CMOS compatible I/O lines · 1 MHz operation

 

ANd if there is a specific FPGA that meets all this, is there a VHDL development software that's free or do you buy it with said FPGA?

 

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 8 years ago +4 suggested
    You could fairly easily use an FPGA to make a plug compatible 6526 part except for the 5V working. Modern FPGAs don't support 5V IO and the CMOS type parts in small packages don't. There are a few 5V working…
  • johnbeetem
    johnbeetem over 8 years ago +3 suggested
    You might look into the original Xilinx Spartan II (not the IIE). The Spartan II is a 2.5 V internal device with 5V tolerant I/Os if you use 3.3V LVTTL standard. It's an old family but some parts are still…
Parents
  • johnbeetem
    0 johnbeetem over 8 years ago

    You might look into the original Xilinx Spartan II (not the IIE).  The Spartan II is a 2.5 V internal device with 5V tolerant I/Os if you use 3.3V LVTTL standard.  It's an old family but some parts are still available.  You'll need to use an older version of the Xilinx tools, but those are available for free at the Xilinx site.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • johnbeetem
    0 johnbeetem over 8 years ago

    You might look into the original Xilinx Spartan II (not the IIE).  The Spartan II is a 2.5 V internal device with 5V tolerant I/Os if you use 3.3V LVTTL standard.  It's an old family but some parts are still available.  You'll need to use an older version of the Xilinx tools, but those are available for free at the Xilinx site.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer