FPGA
  • Technologies
  • More
FPGA
Forum Avnet Petalinux 2020.1 Picozed+FMC2 build script problem
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Answers 1 answer
  • Subscribers 583 subscribers
  • Views 2556 views
  • Users 0 members are here
Related

Avnet Petalinux 2020.1 Picozed+FMC2 build script problem

mesamike
mesamike over 5 years ago

I could swore this was working just a couple days ago, but now when I run 'make_pz7020_fmc2.sh'

it ends with an error:

ERROR: avnet-image-minimal-1.0-r0 do_rootfs: Could not invoke dnf. Command '/opt/avnet/petalinux/projects/pz7020_fmc2_2020_1/build/tmp/work/pz7020_fmc2-xilinx-linux-gnueabi/avnet-image-minimal/1.0-r0/recipe-sysroot-native/usr/bin/dnf -v --rpmverbosity=info -y -c /opt/avnet/petalinux/projects/pz7020_fmc2_2020_1/build/tmp/work/pz7020_fmc2-xilinx-linux-gnueabi/avnet-image-minimal/1.0-r0/rootfs/etc/dnf/dnf.conf --setopt=reposdir=/opt/avnet/petalinux/projects/pz7020_fmc2_2020_1/build/tmp/work/pz7020_fmc2-xilinx-linux-gnueabi/avnet-image-minimal/1.0-r0/rootfs/etc/yum.repos.d --installroot=/opt/avnet/petalinux/projects/pz7020_fmc2_2020_1/build/tmp/work/pz7020_fmc2-xilinx-linux-gnueabi/avnet-image-minimal/1.0-r0/rootfs --setopt=logdir=/opt/avnet/petalinux/projects/pz7020_fmc2_2020_1/build/tmp/work/pz7020_fmc2-xilinx-linux-gnueabi/avnet-image-minimal/1.0-r0/temp --repofrompath=oe-repo,/opt/avnet/petalinux/projects/pz7020_fmc2_2020_1/build/tmp/work/pz7020_fmc2-xilinx-linux-gnueabi/avnet-image-minimal/1.0-r0/oe-rootfs-repo --nogpgcheck install base-passwd bonnie++ bridge-utils can-utils e2fsprogs e2fsprogs-e2fsck e2fsprogs-mke2fs e2fsprogs-resize2fs fpga-manager-script haveged iperf3 kernel-modules mtd-utils openssh openssh-scp openssh-sftp-server openssh-sshd packagegroup-core-boot packagegroup-core-ssh-dropbear parted pciutils run-postinsts shadow tcf-agent udev-extraconf util-linux-mkfs' returned 1:

DNF version: 4.2.2

cachedir: /opt/avnet/petalinux/projects/pz7020_fmc2_2020_1/build/tmp/work/pz7020_fmc2-xilinx-linux-gnueabi/avnet-image-minimal/1.0-r0/rootfs/var/cache/dnf

Added oe-repo repo from /opt/avnet/petalinux/projects/pz7020_fmc2_2020_1/build/tmp/work/pz7020_fmc2-xilinx-linux-gnueabi/avnet-image-minimal/1.0-r0/oe-rootfs-repo

repo: using cache for: oe-repo

not found other for:

not found modules for:

not found deltainfo for:

not found updateinfo for:

oe-repo: using metadata from Sun 25 Oct 2020 05:53:56 AM UTC.

No module defaults found

--> Starting dependency resolution

--> Finished dependency resolution

Error:

Problem: package packagegroup-core-ssh-dropbear-1.0-r1.noarch requires dropbear, but none of the providers can be installed

  - package dropbear-2019.78-r0.cortexa9t2hf_neon conflicts with openssh provided by openssh-8.0p1-r0.cortexa9t2hf_neon

  - package openssh-8.0p1-r0.cortexa9t2hf_neon conflicts with dropbear provided by dropbear-2019.78-r0.cortexa9t2hf_neon

  - conflicting requests

(try to add '--allowerasing' to command line to replace conflicting packages or '--skip-broken' to skip uninstallable packages or '--nobest' to use not only best candidate packages)

 

ERROR: Logfile of failure stored in: /opt/avnet/petalinux/projects/pz7020_fmc2_2020_1/build/tmp/work/pz7020_fmc2-xilinx-linux-gnueabi/avnet-image-minimal/1.0-r0/temp/log.do_rootfs.683

ERROR: Task (/opt/avnet/petalinux/projects/pz7020_fmc2_2020_1/project-spec/meta-avnet/recipes-core/images/avnet-image-minimal.bb:do_rootfs) failed with exit code '1'

NOTE: Tasks Summary: Attempted 3570 tasks of which 2862 didn't need to be rerun and 1 failed.

 

Summary: 1 task failed:

  /opt/avnet/petalinux/projects/pz7020_fmc2_2020_1/project-spec/meta-avnet/recipes-core/images/avnet-image-minimal.bb:do_rootfs

Summary: There was 1 ERROR message shown, returning a non-zero exit code.

ERROR: Failed to build avnet-image-full

 

What happened? It seems like something that the script needs to download isn't available any more.

  • Sign in to reply
  • Cancel
Parents
  • narrucmot
    0 narrucmot over 5 years ago

    We recently had to make a change for theUltraZed and Ultra96-V2 BSPs to replace dropbear with openssh (openssh provides better throughput that dropbear, and this is important for some applications), and for consistency we decided to make the same change for the MicroZed, PicoZed, and MiniZed BSPs.  Something about the PicoZed configuration is still dependent on dropbear, and this is causing the build failure you mention.  Thank you for bringing this to our attention.  I am working on fixing this now.

     

    --Tom

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • mesamike
    0 mesamike over 5 years ago in reply to narrucmot

    Thanks....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • mesamike
    0 mesamike over 5 years ago in reply to narrucmot

    Thanks....