FPGA
  • Technologies
  • More
FPGA
Forum Avnet Petalinux 2020.1 Picozed+FMC2 build script problem
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Answers 1 answer
  • Subscribers 583 subscribers
  • Views 2554 views
  • Users 0 members are here
Related

Avnet Petalinux 2020.1 Picozed+FMC2 build script problem

mesamike
mesamike over 5 years ago

I could swore this was working just a couple days ago, but now when I run 'make_pz7020_fmc2.sh'

it ends with an error:

ERROR: avnet-image-minimal-1.0-r0 do_rootfs: Could not invoke dnf. Command '/opt/avnet/petalinux/projects/pz7020_fmc2_2020_1/build/tmp/work/pz7020_fmc2-xilinx-linux-gnueabi/avnet-image-minimal/1.0-r0/recipe-sysroot-native/usr/bin/dnf -v --rpmverbosity=info -y -c /opt/avnet/petalinux/projects/pz7020_fmc2_2020_1/build/tmp/work/pz7020_fmc2-xilinx-linux-gnueabi/avnet-image-minimal/1.0-r0/rootfs/etc/dnf/dnf.conf --setopt=reposdir=/opt/avnet/petalinux/projects/pz7020_fmc2_2020_1/build/tmp/work/pz7020_fmc2-xilinx-linux-gnueabi/avnet-image-minimal/1.0-r0/rootfs/etc/yum.repos.d --installroot=/opt/avnet/petalinux/projects/pz7020_fmc2_2020_1/build/tmp/work/pz7020_fmc2-xilinx-linux-gnueabi/avnet-image-minimal/1.0-r0/rootfs --setopt=logdir=/opt/avnet/petalinux/projects/pz7020_fmc2_2020_1/build/tmp/work/pz7020_fmc2-xilinx-linux-gnueabi/avnet-image-minimal/1.0-r0/temp --repofrompath=oe-repo,/opt/avnet/petalinux/projects/pz7020_fmc2_2020_1/build/tmp/work/pz7020_fmc2-xilinx-linux-gnueabi/avnet-image-minimal/1.0-r0/oe-rootfs-repo --nogpgcheck install base-passwd bonnie++ bridge-utils can-utils e2fsprogs e2fsprogs-e2fsck e2fsprogs-mke2fs e2fsprogs-resize2fs fpga-manager-script haveged iperf3 kernel-modules mtd-utils openssh openssh-scp openssh-sftp-server openssh-sshd packagegroup-core-boot packagegroup-core-ssh-dropbear parted pciutils run-postinsts shadow tcf-agent udev-extraconf util-linux-mkfs' returned 1:

DNF version: 4.2.2

cachedir: /opt/avnet/petalinux/projects/pz7020_fmc2_2020_1/build/tmp/work/pz7020_fmc2-xilinx-linux-gnueabi/avnet-image-minimal/1.0-r0/rootfs/var/cache/dnf

Added oe-repo repo from /opt/avnet/petalinux/projects/pz7020_fmc2_2020_1/build/tmp/work/pz7020_fmc2-xilinx-linux-gnueabi/avnet-image-minimal/1.0-r0/oe-rootfs-repo

repo: using cache for: oe-repo

not found other for:

not found modules for:

not found deltainfo for:

not found updateinfo for:

oe-repo: using metadata from Sun 25 Oct 2020 05:53:56 AM UTC.

No module defaults found

--> Starting dependency resolution

--> Finished dependency resolution

Error:

Problem: package packagegroup-core-ssh-dropbear-1.0-r1.noarch requires dropbear, but none of the providers can be installed

  - package dropbear-2019.78-r0.cortexa9t2hf_neon conflicts with openssh provided by openssh-8.0p1-r0.cortexa9t2hf_neon

  - package openssh-8.0p1-r0.cortexa9t2hf_neon conflicts with dropbear provided by dropbear-2019.78-r0.cortexa9t2hf_neon

  - conflicting requests

(try to add '--allowerasing' to command line to replace conflicting packages or '--skip-broken' to skip uninstallable packages or '--nobest' to use not only best candidate packages)

 

ERROR: Logfile of failure stored in: /opt/avnet/petalinux/projects/pz7020_fmc2_2020_1/build/tmp/work/pz7020_fmc2-xilinx-linux-gnueabi/avnet-image-minimal/1.0-r0/temp/log.do_rootfs.683

ERROR: Task (/opt/avnet/petalinux/projects/pz7020_fmc2_2020_1/project-spec/meta-avnet/recipes-core/images/avnet-image-minimal.bb:do_rootfs) failed with exit code '1'

NOTE: Tasks Summary: Attempted 3570 tasks of which 2862 didn't need to be rerun and 1 failed.

 

Summary: 1 task failed:

  /opt/avnet/petalinux/projects/pz7020_fmc2_2020_1/project-spec/meta-avnet/recipes-core/images/avnet-image-minimal.bb:do_rootfs

Summary: There was 1 ERROR message shown, returning a non-zero exit code.

ERROR: Failed to build avnet-image-full

 

What happened? It seems like something that the script needs to download isn't available any more.

  • Sign in to reply
  • Cancel
Parents
  • narrucmot
    0 narrucmot over 5 years ago

    This is fixed now.  There was a packagegroup in the rootfs configuration for MicroZed and PicoZed that had a dropbear dependency.  That packageroup wasn't needed so it was removed.  Try re-running the script now and you should be all set.

     

    --Tom

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • mesamike
    0 mesamike over 5 years ago in reply to narrucmot

    I deleted my project and cache directories and ran the script again.

    It built successfully this time.

    Thanks for your quick attention to this!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • mesamike
    0 mesamike over 5 years ago in reply to narrucmot

    I deleted my project and cache directories and ran the script again.

    It built successfully this time.

    Thanks for your quick attention to this!