FPGA
  • Technologies
  • More
FPGA
Forum What are you using FPGAs for?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 27 replies
  • Subscribers 586 subscribers
  • Views 3417 views
  • Users 0 members are here
  • fpga
Related

What are you using FPGAs for?

Catwell
Catwell over 16 years ago

I rarely use FPGAs. I mostly have stuck in other embedded development environments during my career. But, how are you using FPGAs these days?

 

Cabe

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago

    I'm currently integrating an FPGA into a space insturmentation design. For low power, realtime applications they can't be beat. There great for robustness also, you don't have to worry about things changing or crashing. BTW the FPGA is an Actel 600 gate nano.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to e14 Contributor

    How do you like the Nano?  The density and package size is interesting to me.  I've been thinking about trying them out, but I'm reluctant to purchase yet another programming cable.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to e14 Contributor

    High-radiation areas are great for FPGAs due to their ability to add TMR. Polling between the cores with a trigger to scrub the one that is off in the weeds.

     

    @Jeri write your own programmer utilizing an FPGA you currently have a JTAG programmer for. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mindthomas
    0 mindthomas over 15 years ago

    Hi.

    I use FPGAs and CPLDs a lot in the work I do. CPLDs are especially handy when it comes to voltage translation, as they are pretty inexpensive, and can easily be reprogrammed, so pin definitions can be moved around. An example of this would be the BusBlaster, where a CPLD is used as voltage translator.

    I use FPGAs because you have total control of what is happening in real time. You are not limited to an "instruction" set, where a single instruction can take a couple of clock cycles.

    Most of the times though, I implement some kind of microcontroller inside the FPGA, which makes it a great device. I'm in total control of the microcontrollers periphirals, and I can make my own if needed.

     

    Visit my blog to see some of the FPGA board reviews and starter projects I did: http://blog.tkjelectronics.dk

     

    Best Regards

    Thomas Jespersen

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to e14 Contributor

    They are good for connecting logic, but not for DSP applications... they are good for low power applications, ours only draws ~15mA @12mHz and were  using 300k gates (half)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • maiatec
    0 maiatec over 15 years ago in reply to e14 Contributor

    I agree. We can not compare a microprocessor specifically designed as a DSP with a FPGA. FPGA has many advantages in relation to a DSP and also has disadvantages. Depending on application we can use  a FPGA and get the best it can offer. All of it depends on good sense. We can not forget one great advantage: miniaturization !

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago

    I used to work at a company that makes NMR/MRI equipment (super conducting magnets, etc.). I was the Linux kernel guy, and we built this awesome platform based on the Xilinx Virtex II Pro (essentially a custom SoC). I still keep my hand in a little, but I'm mostly working on "Enterprise Linux" for a living these days. Still, I've currently a pipe dream of implementing a fake IDE/PATA controller in a cheapo CPLD or maybe FPGA that will allow me to expose some GPIO lines via a fake "disk" in my old empeg (Linux car mp3 player device - they stopped making them ten years ago) and thereby, with a lot of driver hacking allow me to do USB over "IDE", adding a USB interface to the player.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 15 years ago in reply to maiatec

    I think you are  a little out of touch - FPGAs can offer truly amazing DSP performance - outclassing DSP chips by a huge margin. eg "The Virtex-6 FPGA family provides up to 2,016 DSP48 slices that deliver over 1000 GMACS of DSP processing performance",

     

    There are no single chip DSPs that can come close.

     

    Obviously such performance comes at a cost in money and in power and is certainly not suitable for a great many applications.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • maiatec
    0 maiatec over 15 years ago in reply to michaelkellett

    you started disagreeing and it ended up agreeing that there are advantages and disadvantages. Very good ! Finally, at the end you gave some advantages and disadvantages.

    It depends on the application and the cost involved. If you had read item 5 ("there are some applications where the use of microcontrollers/microprocessors is useless. When we need to process various signals in a short time (few nanoseconds) in parallel. The best choice: FPGA"), would understand exactly what I was trying to explain. Undoubtedly, FPGA is more powerful than any microprocessor / microcontroller but there is a cost to pay. The cost benefit depends on your application.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 15 years ago in reply to maiatec

    I think my comment was accidently (by me) linked to yours - it was actually in response to "They are good for connecting logic, but not for DSP applications" from someone else.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<>