FPGA
  • Technologies
  • More
FPGA
Forum What are you using FPGAs for?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 27 replies
  • Subscribers 586 subscribers
  • Views 3505 views
  • Users 0 members are here
  • fpga
Related

What are you using FPGAs for?

Catwell
Catwell over 16 years ago

I rarely use FPGAs. I mostly have stuck in other embedded development environments during my career. But, how are you using FPGAs these days?

 

Cabe

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 16 years ago
    I plan on interfacing it with a fast ADC and memory to implement a software-defined radio.
    At school we have a dev kit that is capable of generating a VGA signal using one. Other uses could be cracking a cypher, etc. Infinite possibilities image
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 16 years ago

    I am working on a design implementing a computationally-intensive image processing algorithm, which has to run real-time at up to 60 frames per second.  Such computation requires a large array of CPU cores, which is more costly and power-intensive than a custom FPGA solution.  They tend to excel at tasks where there is a fixed set of computations to be performed, and are able to achieve a high throughput because the operations can be performed in parallel across the logic fabric in the chip.  Image processing, telecommunications, and aerospace are areas which are using the larger FPGA devices these days.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mmtsuchi
    0 mmtsuchi over 16 years ago

    I mainly use FPGA for a whole project : commands for (very) high power machines.

    FPGA is infinetly configurable and I say "upgradable".

     

    FPGA with Nios II as a data logger with multiple communication (rs232, ethernet, profibus, memory card)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 16 years ago
    I'm accustomed to using FPGAs for signal cleaning applications, when a precision output is important.   The simple programmable logic allows for only a specific set ot signals to be allowed passage, with all others removed, even if they're unknown.  It takes the guesswork out of building a hard-wired circuit solution, gives way more parallelization of the operations, and allows for refactoring later.  Of course, that also makes it an excellent prototyping platform for optimization prior to developing custom implementations.  On the other hand, the FPGA is simpler than higher-level (software-based) solutions in that signals don't need to be transformed in order to filter them, eliminating quite a few computational steps, and removing the need for more complicated circuitry to run the software.
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • maiatec
    0 maiatec over 15 years ago

    For example, there are some applications where the use of microcontrollers/microprocessors is useless. When we need to process various signals in a short time (few nanoseconds) in parallel. The best choice: FPGA

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago

    I use FPGA's and CPLD's often.

     

    In the last month or so:

    Frame buffer and ADC for 10ghz imaging system. http://www.youtube.com/watch?v=vDyo_OQFdAc

    Pinball controller board. http://www.youtube.com/watch?v=RG2DkjPieX8

     

    In th next two weeks I'll be demonstrating another project with with video edge detection.

     

    -Jer

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • maiatec
    0 maiatec over 15 years ago in reply to e14 Contributor

    Jeri,

     

    Congratulations !!!

    I enjoyed very much the video about imaging system.

    The way you present is very nice !

    I use FPGA's and CPLD's also and I like to see differents and very creatives applications using them.

    Maia.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago

    I am using FPGAs as an interfacing/clock domain crossing device. Typically has a PCI target block in it for communication with a master device.

     

    I am also working on using an FPGA as a memory controller, that I am also developing a custom softcore processor on (just getting my feet wet with that). I am finding that developing my own custom features are much easier than buying a uC or uP and reading a 2000+ page User's Manual to figure out how to use the device. With the FPGA, I just develop my own functionality as I need it. Not saying that the FPGA trumps the uC or uP, it's just a preference of mine. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • maiatec
    0 maiatec over 15 years ago in reply to e14 Contributor

    I agree. Every time we choose a different uC or uP, thousands of pages are needed to get knowledge.

    I use Altera's FPGA and the microprocessor used is always the same: NIOS.

    So, I don't lose my time to get new information.

    The focus is only in my application.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to maiatec

    Nice, yes the learning curve for that particular softcore is sometimes "taxing" to say the least. However, Id rather avoid the uC "manual": the Renesas RX62N literally has a User's Manual that is 2014 pages long....ouch.

    I haven't used NIOS yet, but I work with people that are using it and have great things to say about it. Apparently the softcore Microblaze (I am more familiar with Xilinx) was developed by some college students in California (silicon valley, I am sure) which blows my mind. But I guess I am trying the same thing. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>