FPGA
  • Technologies
  • More
FPGA
Forum Install Vivado, Vitis and PetaLinux on Windows Sublayer for Linux
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 13 replies
  • Subscribers 580 subscribers
  • Views 14006 views
  • Users 0 members are here
  • zynq
  • vivado
  • wsl2
  • pynq
Related

Install Vivado, Vitis and PetaLinux on Windows Sublayer for Linux

Jan Cumps
Jan Cumps over 4 years ago

I'm installing the Vitis and Vivado tools on a WSL instance.
Most of tutorials on scripting and build automated are for Linux. I want to test this out.
My WSL runs Ubuntu 20.04.3 LTS.

I was surprised that WSL actually shows the install GUI. I thought it was only capable of terminal activity by default.

image

If the install succeeds, I'll also install PetaLinux.
The end goal is to build a Non-PYNQ, home made custom Linux image, and generate an SD card for it.
I want to see if I can make a FPGA design, write drivers for the custom hardware, and have the FPGA bitstream automatically loaded when the board starts from that image.
Big goals. I expect it 'll take months.

  • Sign in to reply
  • Cancel

Top Replies

  • Jan Cumps
    Jan Cumps over 2 years ago +3
    For 2024.1, some extra steps are needed. Before running the installer, to avoid that it hangs during the post-processing steps: sudo apt install libncurses5 Vitis uses VSCode now, I had to install…
  • Fred27
    Fred27 over 4 years ago +2
    WSL2 is a different beast to v1 which couldn't display a GUI. I remember trying to install Vivado and petalinux on WSL quite a while ago. I think it was 2019.1 and perhaps in the early days of WSL2.…
  • Jan Cumps
    Jan Cumps over 4 years ago +1
    Fun fact: Windows draws a little Tux in the taskbar icon for this Linux GUI program, and appends (Ubuntu) on the tooltip text:
Parents
  • misaz
    misaz over 2 years ago

    I never used WSL because I think it do not add much more comparing to running VM yourself manually, except it adds lot of communication channels mallware can use for infecting your host from VM. But it is just my own opinion. I used Vivado on Linux (running on Windows) in Hyper-V VM and used X over SSH for "transfering" GUI. It is basically exactly the same WSL do for you out of box, but you are much more flexible which hypervisor you use, you can even run VM on different host (but high bandwidth network is required. X over SSH behave much worse comparing to RDP, I recommend local network only). Finally, It worked well.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • misaz
    misaz over 2 years ago

    I never used WSL because I think it do not add much more comparing to running VM yourself manually, except it adds lot of communication channels mallware can use for infecting your host from VM. But it is just my own opinion. I used Vivado on Linux (running on Windows) in Hyper-V VM and used X over SSH for "transfering" GUI. It is basically exactly the same WSL do for you out of box, but you are much more flexible which hypervisor you use, you can even run VM on different host (but high bandwidth network is required. X over SSH behave much worse comparing to RDP, I recommend local network only). Finally, It worked well.