FPGA
  • Technologies
  • More
FPGA
Forum Install Vivado, Vitis and PetaLinux on Windows Sublayer for Linux
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 13 replies
  • Subscribers 580 subscribers
  • Views 14019 views
  • Users 0 members are here
  • zynq
  • vivado
  • wsl2
  • pynq
Related

Install Vivado, Vitis and PetaLinux on Windows Sublayer for Linux

Jan Cumps
Jan Cumps over 4 years ago

I'm installing the Vitis and Vivado tools on a WSL instance.
Most of tutorials on scripting and build automated are for Linux. I want to test this out.
My WSL runs Ubuntu 20.04.3 LTS.

I was surprised that WSL actually shows the install GUI. I thought it was only capable of terminal activity by default.

image

If the install succeeds, I'll also install PetaLinux.
The end goal is to build a Non-PYNQ, home made custom Linux image, and generate an SD card for it.
I want to see if I can make a FPGA design, write drivers for the custom hardware, and have the FPGA bitstream automatically loaded when the board starts from that image.
Big goals. I expect it 'll take months.

  • Sign in to reply
  • Cancel

Top Replies

  • Jan Cumps
    Jan Cumps over 2 years ago +3
    For 2024.1, some extra steps are needed. Before running the installer, to avoid that it hangs during the post-processing steps: sudo apt install libncurses5 Vitis uses VSCode now, I had to install…
  • Fred27
    Fred27 over 4 years ago +2
    WSL2 is a different beast to v1 which couldn't display a GUI. I remember trying to install Vivado and petalinux on WSL quite a while ago. I think it was 2019.1 and perhaps in the early days of WSL2.…
  • Jan Cumps
    Jan Cumps over 4 years ago +1
    Fun fact: Windows draws a little Tux in the taskbar icon for this Linux GUI program, and appends (Ubuntu) on the tooltip text:
  • Jan Cumps
    Jan Cumps over 4 years ago

    Fun fact:

    Windows draws a little Tux in the taskbar icon for this Linux GUI program, and appends (Ubuntu) on the tooltip text:

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Fred27
    Fred27 over 4 years ago

    WSL2 is a different beast to v1 which couldn't display a GUI.

    I remember trying to install Vivado and petalinux on WSL quite a while ago. I think it was 2019.1 and perhaps in the early days of WSL2. I never got it to work properly, but things may have moved on since then.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to Jan Cumps

    During the install you get a warning that the Digilent JTAG driver will not be installed. It has to be done separately on Linux.
    The reason is that all the rest of the installation can be done without elevated rights.
    The installer points to application note UG973 for instructions.
    The process is easy:

    sudo /tools/Xilinx/Vivado/2020.2/data/xicom/cable_drivers/lin64/install_script/install_drivers/install_drivers

    image

    That's it.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to Jan Cumps

    Todo after install:
    cd /tools/Xilinx/Vitis/2020.2/scripts
    sudo ./installLibs.sh

    Then:

    source /tools/Xilinx/Vivado/2020.2/settings64.sh
    vivado

    Success:

    image

    For Vitis to work, I had to manually install a missing dependency:

    sudo apt-get install libswt-gtk-4-java

    Then, run Vitis:

    source /tools/Xilinx/Vitis/2020.2/settings64.sh
    vitis

    I have issues with the start up dialog's size, trying to work around that ...

    image

    ... I unexpectedly fixed it by checking the "Use this as default." box, then pressing tab and enter.
    It was a bogus key sequence, but it rendered the dialog big enough for the Launch button:

    image

    Vitis HLS works too:

    source /tools/Xilinx/Vitis_HLS/2020.2/settings64.sh
    vitis_hls

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to Fred27

    Things have moved. Vivado, Vitis and Vitis HLS work.
    I installed version 2020.2, because the current version of Pynq uses those versions.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to Jan Cumps

    If you want to use the JTAG in Linux, you need to pass the USB device from Windows to WSL.
    Here are the instructions.

    It works, but the hw manager only finds the board if I start Vivado with sudo.

    image

    I'm checking how I can get access to /dev/ttyUSB1 as normal user.
    I'm already in the dialout group, but that doesn't seem to help.
    chmod 666 doesn't help either. Investigating ...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to Jan Cumps

    The solution is documented here: https://boxlambda.readthedocs.io/en/latest/installation/#on-wsl

    add the following lines to /etc/wsl.conf:

    [boot]
    command="service udev start"
    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • misaz
    misaz over 2 years ago

    I never used WSL because I think it do not add much more comparing to running VM yourself manually, except it adds lot of communication channels mallware can use for infecting your host from VM. But it is just my own opinion. I used Vivado on Linux (running on Windows) in Hyper-V VM and used X over SSH for "transfering" GUI. It is basically exactly the same WSL do for you out of box, but you are much more flexible which hypervisor you use, you can even run VM on different host (but high bandwidth network is required. X over SSH behave much worse comparing to RDP, I recommend local network only). Finally, It worked well.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 2 years ago

    For 2024.1, some extra steps are needed.

    Before running the installer, to avoid that it hangs during the post-processing steps:

    sudo apt install libncurses5

    Vitis uses VSCode now, I had to install this lib. Else it would silently close.

    sudo apt-get install libnotify4

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to Jan Cumps

    this is an easier to follow instruction: https://hackmd.io/@aeefs2Y8TMms-cjTDX4cfw/r1fqAa_Da

    Follow the instruction for OpenOCD. The FTDI driver on the Pynq Z2 is covered by that.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
>