FPGA
  • Technologies
  • More
FPGA
Forum GIC vs AXI Interrupt Controller
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 10 replies
  • Subscribers 578 subscribers
  • Views 14715 views
  • Users 0 members are here
Related

GIC vs AXI Interrupt Controller

psd0
psd0 over 4 years ago

I ran sample code from the "Using GPIO, Timers and Interrupts" on my Utra96v2 board.  It worked ok, with the timer pulsing at 1 Hz connected to the IRQ input of the Zynq US+ Processing System block triggering an interrupt.  My understanding is that this is using the GIC, which is the interrupt hardware present on the ARM processor (I was running it bare metal on the R5).  I also know that there's an AXI Interrupt Controller IP and was wondering when I would use one approach - connect to the Zynq processor system directly - versus connecting to the AXI Intc and then to the PS.  This is more of a design question than problem.

  • Sign in to reply
  • Cancel

Top Replies

  • _david_
    _david_ over 4 years ago +2
    Good question. I've thought about this before as well, but this is the first time I've really taken a look into this so I'm not really an expert. Before reading this, I would suggest skimming through the…
  • psd0
    psd0 over 4 years ago in reply to psd0 +2
    Called Xil_In32(0x80000008) (AXI Interrupt Controller starts at 0x8000_0000, if I'm reading the Address Editor in Vivado correctly), and per pg099, 0x8 is the offset to the IER. The Xil_In32() returns…
  • psd0
    psd0 over 4 years ago in reply to _david_ +1
    Thanks for taking the time to write a detailed response. I asked because I got GIC version of the UG1209 demo application working fine, but it seems like the AXI Interrupt Controller version doesn't run…
Parents
  • valeteBro
    0 valeteBro over 2 years ago

    Hi brother,

    I am having exactly the same problem, did you find the cause?

    thank you

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • valeteBro
    0 valeteBro over 2 years ago

    Hi brother,

    I am having exactly the same problem, did you find the cause?

    thank you