FPGA
  • Technologies
  • More
FPGA
Forum petalinux 2021.1 BSP builds but core dumps when booting
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 580 subscribers
  • Views 2184 views
  • Users 0 members are here
Related

petalinux 2021.1 BSP builds but core dumps when booting

e14 Contributor
e14 Contributor over 4 years ago

I was able to build the bsp for minized 2021.1 project without issue. I then load a USB stick and copy the image.ub to it along with my local wpa_supplicant.conf file and then plug it into the minized board. I then run the "update_from_usb.sh" script. It fails of course since the minized board mounts the USB stick as "/dev/sda" and not (as is hard coded in all of the scripts) as "/dev/sda1". So I change them (but of course only for this instance since this will fail again) and re-run the script. It works this time and the image has been copied. I then reboot the board. It does start to load the image but I get the following kernel dump during boot:

8<--- cut here ---
Unhandled fault: imprecise external abort (0xc06) at 0x00000000
pgd = (ptrval)
[00000000] *pgd=00000000
Internal error: Oops - BUG: c06 [#1] PREEMPT SMP ARM
Modules linked in:
CPU: 0 PID: 0 Comm: swapper/0 Not tainted 5.10.0-xilinx-v2021.1 #1
Hardware name: Xilinx Zynq Platform
PC is at xintc_write+0x6c/0x80
LR is at xil_intc_initial_setup+0x24/0xbc
pc : [<c03a1384>] lr : [<c03a15ac>] psr: 600000d3
sp : c0c01eb0 ip : 00000000 fp : c0c01f74
r10: 1e008000 r9 : 00000000 r8 : 00000000
r7 : 00000000 r6 : e081000c r5 : ffffffff r4 : deb4a14c
r3 : 00000000 r2 : ffffffff r1 : e0810000 r0 : deb4a14c
Flags: nZCv IRQs off FIQs off Mode SVC_32 ISA ARM Segment none
Control: 18c5387d Table: 0000404a DAC: 00000051
Process swapper/0 (pid: 0, stack limit = 0x(ptrval))
Stack: (0xc0c01eb0 to 0xc0c02000)
1ea0: deb4a14c 00000001 00000064 c03a15ac
1ec0: deb4429c 00000001 00000064 00000000 00000000 c03a165c deb4429c c011bd2c
1ee0: 00000000 00000064 00000064 00000000 00000000 c03a1310 c0b3c29c 00000000
1f00: c0c03f14 c011c82c 00000064 c0933c4a 00000001 c03a1644 c0c00000 00000100
1f20: 00000122 c011c8d4 c03a1310 00000000 00000001 deb4a14c c100e000 deb6d250
1f40: 00000000 c0b1b1c0 c03a1310 00000000 00000000 00000000 c1001fc0 00000000
1f60: c0c01f74 c0c01f7c c0c00000 c0b268b8 00000000 c0c01f74 c0c01f74 c1001f80
1f80: c1001f80 00000000 00000000 c0b31a28 c0c00000 c0c54e94 c0c03ec0 00000000
1fa0: c0b31a38 18c5387d 00000000 c0b03310 c0c45000 c0b00b90 ffffffff ffffffff
1fc0: 00000000 c0b00580 00000000 c0b31a38 00000000 00000000 c0b00330 00000051
1fe0: 10c0387d 00000000 07ff6000 413fc090 18c5387d 00000000 00000000 00000000
[<c03a1384>] (xintc_write) from [<c03a15ac>] (xil_intc_initial_setup+0x24/0xbc)
[<c03a15ac>] (xil_intc_initial_setup) from [<c03a165c>] (xil_intc_start+0x18/0x28)
[<c03a165c>] (xil_intc_start) from [<c011bd2c>] (cpuhp_issue_call+0xa0/0x13c)
[<c011bd2c>] (cpuhp_issue_call) from [<c011c82c>] (__cpuhp_setup_state_cpuslocked+0x190/0x1fc)
[<c011c82c>] (__cpuhp_setup_state_cpuslocked) from [<c011c8d4>] (__cpuhp_setup_state+0x3c/0x50)
[<c011c8d4>] (__cpuhp_setup_state) from [<c0b1b1c0>] (xilinx_intc_of_init+0x268/0x2f0)
[<c0b1b1c0>] (xilinx_intc_of_init) from [<c0b268b8>] (of_irq_init+0x1e0/0x280)
[<c0b268b8>] (of_irq_init) from [<c0b03310>] (init_IRQ+0x64/0x74)
[<c0b03310>] (init_IRQ) from [<c0b00b90>] (start_kernel+0x284/0x4a4)
[<c0b00b90>] (start_kernel) from [<00000000>] (0x0)
Code: e8bd8070 e5941000 e0816006 f57ff04e (ebf5c26d)
random: get_random_bytes called from init_oops_id+0x24/0x48 with crng_init=0
---[ end trace 0000000000000000 ]---
Kernel panic - not syncing: Attempted to kill the idle task!
---[ end Kernel panic - not syncing: Attempted to kill the idle task! ]---

Can anyone tell me what I've done wrong before I do a deep dive into the kernel to see what's going on here?

Cheers!!

  • Sign in to reply
  • Cancel

Top Replies

  • danzima
    danzima over 4 years ago in reply to e14 Contributor +1
    Hi there! Since this is your own post, if you're on a desktop browser you can navigate near where the comments begin and there is are options above that listed as "reply, like, more," and within "More…
  • e14 Contributor
    e14 Contributor over 4 years ago

    Could someone delete this entry, I've no idea how this ended up here.

    Sorry!!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • danzima
    danzima over 4 years ago in reply to e14 Contributor

    Hi there! Since this is your own post, if you're on a desktop browser you can navigate near where the comments begin and there is are options above that listed as "reply, like, more," and within "More" you can choose to delete this post, assuming it is yours. On a mobile browser this option is also in roughly the same place.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 4 years ago in reply to danzima

    There is no option to delete or remove, only move, mute and report as abusive. I'm closing my account down so I'm sorry to leave this to someone who has the ability to do this.

    Cheers!!