FPGA
  • Technologies
  • More
FPGA
Forum Vivado installing on Windows without admin
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 11 replies
  • Answers 1 answer
  • Subscribers 583 subscribers
  • Views 10317 views
  • Users 0 members are here
  • 7 Ways to Leave Your Spartan-6
  • vivado
  • Spartan_Migration
Related

Vivado installing on Windows without admin

computerton
computerton over 4 years ago

Hello guys,

While I'm anxiously waiting for my Arty S7 board, I wonder if anyone knows of a portable install of Vivado.

I'm going to use it on my work PC, because it's much faster than mine, and I don't have admin rights on it...

  • Sign in to reply
  • Cancel

Top Replies

  • dramoz
    dramoz over 4 years ago +2 verified
    Xilinx Tools (2021.2) (Ubuntu) (Main OS, as VM guest, or as WSL2/Windows) NOTE : DON’T forget to replace .x or <#> for the proper version of the tools when running the commands <#> is used so an error…
  • dramoz
    dramoz over 4 years ago in reply to javagoza +2
    If you upgrade to Windows 11 (or on Windows 10 using MobaXterm ) you will only need one installation on WSL2 (Ubuntu 20.04) as both will give you GUI/X11 access - the only issue I had when running WSL2…
  • misaz
    misaz over 4 years ago +1
    I think you can download full offline installer: It is .tar.gz, but if I remember correctly, SFD (single file download) always contained both Linux and Windows installers). In fact, I recommend use…
  • Jan Cumps
    0 Jan Cumps over 4 years ago in reply to dramoz
    dramoz said:
    both will give you GUI/X11 access

    Yes, the look, feel and integration is virtually seamless. I'm on W11.
    Two (and a half) reasons why I have a windows native install too: 

    • I installed it on Win first. WSL2 as afterthought, when I needed to compile github projects from source
    • Overall smoothness,  reactiveness and interactions on Windows native are a bit better, on my device. Not a lot though.
    • It allows me to make my own projects OS independent. If I script them, I try  them on both OSes.
    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<