FPGA
  • Technologies
  • More
FPGA
Forum How To set up Vivado on MacOS
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 582 subscribers
  • Views 12636 views
  • Users 0 members are here
Related

How To set up Vivado on MacOS

rscasny
rscasny over 4 years ago

I had someone contact me about the need to set up Vivado on a Mac. I don't get this question very often. I don't think it's directly supported.

If you have set it up on a Mac, I'd be interested in getting your comments/experiences to pass onto him.

Thanks.

  • Sign in to reply
  • Cancel

Top Replies

  • Metaforest
    Metaforest over 4 years ago +2
    Set up a VMWare Fusion VM running Ubuntu 16 or 18. This will only work well if the host Mac has 4 or more cores, more than 16 GB of RAM and more than 100GB storage available to the VM. If the Mac cannot…
  • bradfordmiller
    bradfordmiller over 4 years ago in reply to dimiterk +1
    It also needs to be on an Intel Mac; I'm not aware of M1 Macs that can (easily) run Intel VMs.
  • bradfordmiller
    bradfordmiller over 4 years ago in reply to Metaforest +1
    An M1 VMWare Fusion *does* run on an M1, but it will only run OS's compiled for ARM. And I'm not aware of a version of Linux that has Rosetta capabilities to run x86 under ARM (yet), but as you say even…
Parents
  • shabaz
    shabaz over 4 years ago

    A separate laptop as mentioned above or even a separate small server (e.g. Intel NUC) can be really handy. I run anything that I cannot run on my laptop (or don't want to run on my laptop) on the separate Intel NUC and remotely connect to it (e.g. SSH for command line, or Remote Desktop for graphical apps). It is possible to use a free copy of VMware ESXi to have many virtual machines on the Intel NUC, and switch them on/off remotely, saving resources/energy/space, great for home use. Info on that is on the VMware website, and performance impact of ESXi is low. The Intel NUC is a very tiny box (just a few times the size of a Pi), but there are other small PC options too.

    I've not tried it, but another option is Vivado on Amazon Web Services (AWS), since Xilinx offers that. The cost is $0.55 per hour currently (just need to remember to shut it down afterwards : )

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 4 years ago

    A separate laptop as mentioned above or even a separate small server (e.g. Intel NUC) can be really handy. I run anything that I cannot run on my laptop (or don't want to run on my laptop) on the separate Intel NUC and remotely connect to it (e.g. SSH for command line, or Remote Desktop for graphical apps). It is possible to use a free copy of VMware ESXi to have many virtual machines on the Intel NUC, and switch them on/off remotely, saving resources/energy/space, great for home use. Info on that is on the VMware website, and performance impact of ESXi is low. The Intel NUC is a very tiny box (just a few times the size of a Pi), but there are other small PC options too.

    I've not tried it, but another option is Vivado on Amazon Web Services (AWS), since Xilinx offers that. The cost is $0.55 per hour currently (just need to remember to shut it down afterwards : )