FPGA
  • Technologies
  • More
FPGA
Forum Simple FPGA/PCIe based SDR (Software Defined Radio)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 582 subscribers
  • Views 6831 views
  • Users 0 members are here
Related

Simple FPGA/PCIe based SDR (Software Defined Radio)

ad0es
ad0es over 3 years ago

Hi,

I am attempting to make an SDR receiver using an Artix-7 FPGA reading multiple ADCs and sending the raw 16 bit samples over PCIe.

I'm a strong c/c++ programmer, and have extensive hardware knowledge. But I have no FPGA programming experience.

I have installed the Vivado suite to a linux box, along with the Cable drivers. I have an Alinx AX7103 development board, along with all the sample code they provide. Vivado claims to include a PCIe IP core. I'm guessing the other blocks I need to build include a 122.88MHz clock for the ADCs, sample buffers, read calls attached to a kernel driver, INTerrupts on buffer available and ???

All of the FFT, FIR, etc. programming is done on the main computer using Cuda, keeping the FPGA relatively simple. I already have a proof of concept running on an ANAN-200D SDR which has had its FPGA lobotomized to do nothing but send samples over the 1Gb Ethernet interface. But the 1Gb channel limits me to 1/2 an ADC sample rate, so not acceptable.

The first task I need to tackle is figuring out how to hookup the included JTAG device and configure Vivado to see it and the Artix-7 behind it...

Any and all suggestions/comments/warnings welcome!

tia,

Steve

  • Sign in to reply
  • Cancel

Top Replies

  • flyingbean
    flyingbean over 3 years ago +4
    You plan looked quite practical since you already moved FFT/FIR out off Artix 7 FPGA because the limited number of DSP slices might be a bottleneck for SDR applications. Please use latest Vitis tool from…
  • flyingbean
    flyingbean over 3 years ago in reply to ad0es +3
    Short answer for JTAG debugging: JTAG need internal RAM on FPGA to keep the snapshot of data. If the implementation is short of the LUT/RAM on FPGA, you might not get enough data for your trouble-shooting…
  • flyingbean
    flyingbean over 3 years ago in reply to ad0es +2
    Hi Steve: Please read this TRD on Artix 7 from Xilinx : https://docs.xilinx.com/v/u/1.0-English/ug964-ac701-trd-ug, ug964, Artix®-7 AC701 Base Targeted Reference Design (TRD) demonstrates, which should…
Parents
  • flyingbean
    flyingbean over 3 years ago

    You plan looked quite practical since you already moved FFT/FIR out off Artix 7 FPGA because the limited number of DSP slices might be a bottleneck for SDR applications. Please use latest Vitis tool from Xilinx since you might get more free IPs on FPGA building blocks. The website will give you a lift for PCIE implementation on Artix 7:https://numato.com/kb/getting-started-with-pci-express-on-aller-artix-7-fpga-board-with-m-2-interface/

    https://www.linkedin.com/pulse/xilinx-dma-pcie-tutorial-part-2-roy-messinger

    For FPGA implementation, bandwidth/clock speed is easier to figure out for specification, but the resource estimation on the FPGA could be uncertain at this point. Rule of the thumb, keep the LUT/FF uasage under 75~85% for easier routing and timing closure.

     Please get a solid reference design on PCIE IP block configuration. Otherwise you might sink into massive data/protocol debug with/without Xilinx JTAG chain.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • ad0es
    ad0es over 3 years ago in reply to flyingbean

    Thanx, those sites look very helpful.Thumbsup I have Vivado 2022.2 installed on Ubuntu 22.10 linux.

    flyingbean said:
    Please get a solid reference design on PCIE IP block configuration. Otherwise you might sink into massive data/protocol debug with/without Xilinx JTAG chain.

    By this do you mean that without a solid design debugging would be  difficult even with a JTAG to monitor it?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • flyingbean
    flyingbean over 3 years ago in reply to ad0es

    Short answer for JTAG debugging: JTAG need internal RAM on FPGA to keep the snapshot of data. If the implementation is short of the LUT/RAM on FPGA, you might not get enough data for your trouble-shooting. A solid design would be Xilinx Wiki/reference design on PCIE and google other people's blogs on this topic. Sometime, I found Xilinx documentation or reference design might have bugs too. PCIE IP block configuration properly is a key for your success.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • flyingbean
    flyingbean over 3 years ago in reply to ad0es

    Short answer for JTAG debugging: JTAG need internal RAM on FPGA to keep the snapshot of data. If the implementation is short of the LUT/RAM on FPGA, you might not get enough data for your trouble-shooting. A solid design would be Xilinx Wiki/reference design on PCIE and google other people's blogs on this topic. Sometime, I found Xilinx documentation or reference design might have bugs too. PCIE IP block configuration properly is a key for your success.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Children
  • ad0es
    ad0es over 3 years ago in reply to flyingbean

    flyingbean,

    Is this the wiki you refer to?

    https://xilinx-wiki.atlassian.net/wiki/spaces/A/overview

    or some other site.  I also found a Xilinx github page.

    tia,

    Steve AD0ES

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • flyingbean
    flyingbean over 3 years ago in reply to ad0es

    Hi Steve: Please read this TRD on Artix 7 from Xilinx : https://docs.xilinx.com/v/u/1.0-English/ug964-ac701-trd-ug, ug964, Artix®-7 AC701 Base Targeted Reference Design (TRD) demonstrates, which should be a solid reference design for your FPGA side work. You might have to migrate TRD design from Vivado 2014 into Vivado 2022.2.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • ad0es
    ad0es over 3 years ago in reply to flyingbean

    Bean,

    It has been moved, found it here for anyone else interested:

    https://docs.xilinx.com/v/u/en-US/ug964-ac701-trd-ug

    Steve AD0ES