FPGA
  • Technologies
  • More
FPGA
Forum Arty A7- 35T DDR3 implementation in Vivado 2020.2
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 581 subscribers
  • Views 3951 views
  • Users 0 members are here
Related

Arty A7- 35T DDR3 implementation in Vivado 2020.2

Jonathan101
Jonathan101 over 3 years ago

Hi!

I built a design in Vivado which consists of microblaze [Arty-A7 35T] .

Due to the fact that I have very large workspace [.cpp, .h files], i also use ddr [ MIG] to the design [With configurations as default].

However, after exporting .xsa to Vitis and build my workspace, I got weird errors:

  • getchar() isn't working
  • variables that suddenly change their value without meaning
  • after main() ends, it start from the beginning

i suspect all of this is related to memory.

i configure in lscript.ld file on Vitis heap and stack to be 0x2000

Is there some microblaze or ddr configuration that need to be done in Vivado in order to make Vitis code to work smoothly?

Thanks in advance.

 My design is based on this webpage:  https://medium.com/@caglayandokme/extending-the-memory-limits-of-microblaze-with-an-external-ddr-6c896e75c218

  • Sign in to reply
  • Cancel

Top Replies

  • javagoza
    javagoza over 3 years ago +3
    A few months ago I did a tutorial using the Arty S7 50 following the advice of the Digilent tutorials. I think it can help you: Arty S7 50 First Baremetal Software Project
  • javagoza
    javagoza over 3 years ago in reply to javagoza +2
    This is one of the configurations that worked for me with the linker script generator for this other project that required large arrays Arty S7 50 VGA Thermal Imaging Camera
  • flyingbean
    flyingbean over 3 years ago +1
    You might need to optimize getchar() with Xilinx's APIs. Please check this forum from Xilinx: support.xilinx.com/.../how-to-input-characters-from-console-why-getchar-works-not-properly
Parents
  • flyingbean
    flyingbean over 3 years ago

    You might need to optimize getchar() with Xilinx's APIs. Please check this forum from Xilinx:

    support.xilinx.com/.../how-to-input-characters-from-console-why-getchar-works-not-properly

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • flyingbean
    flyingbean over 3 years ago

    You might need to optimize getchar() with Xilinx's APIs. Please check this forum from Xilinx:

    support.xilinx.com/.../how-to-input-characters-from-console-why-getchar-works-not-properly

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Jonathan101
    Jonathan101 over 3 years ago in reply to flyingbean

    My friend, i ask for application note which explain how to connect microblaze and DDR. I think wrong hw connection is causing me memory problems in the code.