FPGA
  • Technologies
  • More
FPGA
Forum FPGA's for everyone
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 583 subscribers
  • Views 749 views
  • Users 0 members are here
Related

FPGA's for everyone

e14 Contributor
e14 Contributor over 11 years ago

I have watched many projects to make FPGA's easy to program. This includes custom languages, conversion of languages to HDL, and none have gone mainstream. The really neat thing about FPGA's is that they make interfacing easy. Rather than trying to make everyone an FPGA programmer, why can't we just make FPGA easy to put in a design. We could setup an environment where the interface to computer or microcontroller is standard thru USB, SPI, Ethernet, etc. Then the user can just select from a menu of interfaces they want to use and assign the pins. This would be parallel I/O ports, I2C, serial, PWM, 2x16 display drivers, etc. I have used this at my real work over the last couple of years, and having the interface done shortens the project time, and all we have to do is write the new interface modules.

 

My two cents.

Ron

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 11 years ago +2
    The approach you describe wouldn't address most of the complexity in the kind of FPGA design work I do. For example I've recently spent quite a lot of time on a signal generation package which can do sweeps…
Parents
  • e14 Contributor
    e14 Contributor over 10 years ago

    Ron, I think what you're looking for is pretty much exactly this: https://www.crowdsupply.com/krtkl/snickerdoodle

     

    (full disclosure, I'm one of the creators)


    ARM+FPGA in the same physical package/chip and we've actually made it possible to pick your hardware "personality" (I/O configuration) from a mobile app using pre-build bit streams. We've spent years dealing with the exact problems you mentioned above and snickerdoodle was the solution we came up with to address them.

     

    If you want to check it out, I'd be very interested to hear your thoughts.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 10 years ago

    Ron, I think what you're looking for is pretty much exactly this: https://www.crowdsupply.com/krtkl/snickerdoodle

     

    (full disclosure, I'm one of the creators)


    ARM+FPGA in the same physical package/chip and we've actually made it possible to pick your hardware "personality" (I/O configuration) from a mobile app using pre-build bit streams. We've spent years dealing with the exact problems you mentioned above and snickerdoodle was the solution we came up with to address them.

     

    If you want to check it out, I'd be very interested to hear your thoughts.