FPGA
  • Technologies
  • More
FPGA
Forum How to Create Adder, LPF and HPF, Amplifier Circuits in FPGA LabVIEW
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 9 replies
  • Subscribers 579 subscribers
  • Views 2489 views
  • Users 0 members are here
  • labview fpga
  • digital signal processing
  • fpga
  • digital filters
  • labview
  • cRio9024
Related

How to Create Adder, LPF and HPF, Amplifier Circuits in FPGA LabVIEW

umair1998
umair1998 over 2 years ago

Hello, I have NI cRIO 9024 with NI 9215 and NI 9263.

 

I want to design a digital signal processing circuit with the following sequence 

 

From Sensor 04 Voltages will be Received at AI0-3 Module > I want to Add These 04 Signals > Amplified Them > Pass Them Through Low Pass Filter >> Normalize My Final Output 

 

Currently, all the above operations are being performed by Analog Circuit which contains opamps, resistors, and capacitors. How can I replace all these using LabVIEW? 

 

 

I don't know if my Question is posted on the right platform or not but I am not sure how to ask for help. Please someone should suggest me how to start with my task.

 

Thank you all

 

Best Regards

 

Umair

  • Sign in to reply
  • Cancel

Top Replies

  • jc2048
    jc2048 over 2 years ago +2
    If you have technical questions about the modules or the design software, I think you'd do much better to ask on the NI forums. They look quite active and the engineers participating there will have experience…
  • javagoza
    javagoza over 2 years ago in reply to shabaz +1
    I have taken all of these courses, they are very easy to follow but they will not give you an idea of how to use the LabView FPGA module. If the OP is new to FPGAs I think he/she will have a big learning…
  • michaelkellett
    michaelkellett over 2 years ago in reply to umair1998 +1
    I don't think that the NI modules you mention as being available to you include an FPGA. I don't use NI parts so I may have misread their documents but I suggest that you check that you can access an…
Parents
  • jc2048
    0 jc2048 over 2 years ago

    If you have technical questions about the modules or the design software, I think you'd do much better to ask on the NI forums. They look quite active and the engineers participating there will have experience of the kit and software and will be able to quickly point you at help for the problems that everyone new to this finds.

    Remember, too, that the money paid for FPGA LabVIEW includes technical support.

    But, in general terms, here are a few thoughts...

    First question you need to think about is: do we even need the FPGA to do the processing? Presumably, the chassis comes in a form where initially there is just a pass-through between the processor and the modules. If it's fast enough to do what you want (it's an 800MHz processor, so no slouch), it might be that programming the processor module (assuming you can do that with standard LabVIEW) is simpler than grappling with the FPGA.

    You may need to consider how quantities are represented in the FPGA. FPGA LabVIEW may give you various options, such as integer, fixed point, or some kind of floating point, with options as to resolution (I'm guessing here). There are trade-offs (speed and area in the FPGA) here that would affect your design.

    Next you need a high-level design. You've done that already with your word description of the data flow. FPGA LabVIEW will have some kind of math block, so addition will be easy. Amplification is simply multiplication by a constant (the gain). There will be a filter block you can use. That will probably give you a selection of different characteristics. There's a good probability that will even include digital analogues of the analogue ones you're familiar with (Butterworth, Cheby., etc), as well as digital filters that can't be realized with analogue circuitry. Normalization is multiplication, again. You ought to be able to piece that together quite quickly, try it out, and then start refining it.

    Some things you may need to keep an eye on with a digital system are: latency (delay through the system); clipping, as intermediate values exceed the representation; the numerical 'noise-floor', from rounding errors etc, eating away your resolution; and numerical instability (with recursive filters).

    If you want your digital system to behave more like your analogue one with large signals, you may want to model the op amps better by including integrators to model the slew limitation you get with a compensated op amp.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jc2048
    0 jc2048 over 2 years ago

    If you have technical questions about the modules or the design software, I think you'd do much better to ask on the NI forums. They look quite active and the engineers participating there will have experience of the kit and software and will be able to quickly point you at help for the problems that everyone new to this finds.

    Remember, too, that the money paid for FPGA LabVIEW includes technical support.

    But, in general terms, here are a few thoughts...

    First question you need to think about is: do we even need the FPGA to do the processing? Presumably, the chassis comes in a form where initially there is just a pass-through between the processor and the modules. If it's fast enough to do what you want (it's an 800MHz processor, so no slouch), it might be that programming the processor module (assuming you can do that with standard LabVIEW) is simpler than grappling with the FPGA.

    You may need to consider how quantities are represented in the FPGA. FPGA LabVIEW may give you various options, such as integer, fixed point, or some kind of floating point, with options as to resolution (I'm guessing here). There are trade-offs (speed and area in the FPGA) here that would affect your design.

    Next you need a high-level design. You've done that already with your word description of the data flow. FPGA LabVIEW will have some kind of math block, so addition will be easy. Amplification is simply multiplication by a constant (the gain). There will be a filter block you can use. That will probably give you a selection of different characteristics. There's a good probability that will even include digital analogues of the analogue ones you're familiar with (Butterworth, Cheby., etc), as well as digital filters that can't be realized with analogue circuitry. Normalization is multiplication, again. You ought to be able to piece that together quite quickly, try it out, and then start refining it.

    Some things you may need to keep an eye on with a digital system are: latency (delay through the system); clipping, as intermediate values exceed the representation; the numerical 'noise-floor', from rounding errors etc, eating away your resolution; and numerical instability (with recursive filters).

    If you want your digital system to behave more like your analogue one with large signals, you may want to model the op amps better by including integrators to model the slew limitation you get with a compensated op amp.