FPGA
  • Technologies
  • More
FPGA
Forum Development board to test my ASIC
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 581 subscribers
  • Views 628 views
  • Users 0 members are here
  • terasic
  • embedded
  • fpga developement
Related

Development board to test my ASIC

AMIR.KHAN
AMIR.KHAN over 2 years ago

Can anyone suggest me a development board that supports GPIOs with 1.2V and 3.3V or atleast 1.2V.

  • Sign in to reply
  • Cancel

Top Replies

  • vmate
    vmate over 2 years ago +1
    The Digilent Genesys 2 has adjustable IO voltage from 1.2 to 3.3V https://digilent.com/reference/programmable-logic/genesys-2/reference-manual The VADJ power rail requires special attention. It is…
  • vmate
    vmate over 2 years ago

    The Digilent Genesys 2 has adjustable IO voltage from 1.2 to 3.3V
    https://digilent.com/reference/programmable-logic/genesys-2/reference-manual


    The VADJ power rail requires special attention. It is an adjustable rail that powers the FMC mezzanine connector, user push-buttons, switches, XADC Pmod connector and the FPGA banks connected to these peripherals (banks 15, 16, 17). The feedback pin of the VADJ regulator is connected to a resistor network modifiable by jumper JP6. Changing its position changes the resistor divider in the feedback loop, thereby changing the voltage on the regulator’s output. The possible voltages are listed in Figure 2. If JP6 is not set, the VADJ voltage defaults to 1.2 V. This feature enables setting the VADJ voltage to suit a certain FMC mezzanine card or application.