FPGA
  • Technologies
  • More
FPGA
Forum Seeking Feedback on Your Preference for an AMD Kria Workshop
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 14 replies
  • Subscribers 582 subscribers
  • Views 2819 views
  • Users 0 members are here
  • AMD workshop
  • member survey
Related

Seeking Feedback on Your Preference for an AMD Kria Workshop

rscasny
rscasny over 2 years ago

I am planning for offering an AMD Kria workshop in early 2025. (Note: it takes awhile to put a workshop together!) I wanted to get your interest. Please vote in the polls below so I can gauge your interest level. Thanks.

Let me give some background first:

What is Kria?

  • Kria SOMs were designed with SW engineers in mind, providing familiar design environments without requiring FPGA programming experience.

Kria SOMs

  • Kria K24 SOM features a cost-optimized, custom-built ZynqTm UltraScale+Tm MPSoC device targeting power efficient DSP-intensive applications such as motor control.
  • Kria K26 SOM features a mid-range custom-built Zynq UltraScale+ MPSoC device in a small form factor targeting vision AI, robotics and industrial applications.

AMD Kria Starter kits

  • KV260 Vision AI Starter Kit: Designed for vision AI applications, the KV260 is the fastest way to develop unique vision solutions for production volume deployment with the K26 SOM.
  • KR260 Robotics Starter Kit: Designed for robotics and industrial applications, the KR260 is the fastest way to develop intelligent factory solutions for production volume deployment with the K26 SOM.
  • KD240 Drives Starter Kit: An out-of-the-box ready development platform for motor control and DSP applications. Embedded SW developers without FPGA expertise can easily get started by running accelerated applications and leverage multiple development flows, including Python, the MATLAB® Simulink® environment, and more.

The Polls

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 2 years ago +4
    This is new technology for me. Although there is some canned starter software, given the underlying complexity, I would need to start with some introductory work. Eventually I would be interested to see…
  • phoenixcomm
    phoenixcomm over 2 years ago in reply to dougw +2
    I really don't get it. Everything, everybody wants to talk to the "Cloud"?? What is the driving force for the Cloud? This means you have to pay somebody else to do the work, and how SECURE is it? This…
  • dyessgg
    dyessgg over 2 years ago +2
    I would suggest to NOT buy the "Vision" kit. It's a crippled version of the SoM with one of the interconnects missing and very little real documentation. Unfortunately, it was the first kit on the market…
Parents
  • dougw
    dougw over 2 years ago

    This is new technology for me. Although there is some canned starter software, given the underlying complexity, I would need to start with some introductory work. Eventually I would be interested to see how this integrates with ROS2.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • phoenixcomm
    phoenixcomm over 2 years ago in reply to dougw

    I really don't get it. Everything, everybody wants to talk to the "Cloud"??  What is the driving force for the Cloud?  This means you have to pay somebody else to do the work, and how SECURE is it? This is like what we used to call shared hosting. One of my large DB was on the Cloud I had 250K of data plus static pages which we generated via a program we would run called publish. Now to put this in context, it was written in PERL which is heavily dependent on where Perl lived and where CPAN lived. (this was not my choice as the system was "pre-configured" there were over 100 modules and each had references to Perl and CPAN. I have my data I downloaded the MySQL tables but they had erased the Tree of Static web pages! I also had a copy of the source I was using. 

    My intentions were to track down every instance and fix it to my standards. I never relaunched the site, as it was going to need a rewrite. I  started from scratch, This project I later abandoned. I will explain this later. I do all of my hosting on a Linux box that is less than 20 feet from this chair. I am content to just pay AT&T for my 1Gbyte fiber service, and I have several projects that I am working on concurrently, well sort of. New upgraded web server which requires a software upgrade from Debian 10 to 12. The new OpenBSD uses pf, in the transparent mode of course, to both work as my firewall and my switch,. A Pi-hole with Astrix my voice-over IP phone system.  While all this mess is going on I put up Jetty (a lightweight version of Tomcat on my desktop, so I can use Java applications for the websites, so I can for once put a nail into Perl. 

    I will end this diatribe. ~~ Cris. 

    PS Please remember this: If you use WiFi of any sort you now have a back door into you data. Stay wired!!!  BTW this also includes a tunnel between to WiFi points as well. 

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • dyessgg
    dyessgg over 2 years ago in reply to phoenixcomm

    The "cloud" is just someone else's computer that they control and manage and tell you how you're going to use it, or not.  They can kick you off their servers and you're just out of luck.  (Research the Social Media site Parler that went through just that.)

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dyessgg
    dyessgg over 2 years ago in reply to phoenixcomm

    The "cloud" is just someone else's computer that they control and manage and tell you how you're going to use it, or not.  They can kick you off their servers and you're just out of luck.  (Research the Social Media site Parler that went through just that.)