FPGA
  • Technologies
  • More
FPGA
Forum (solved) Did you manage to debug a Microblaze RISC-V with Vitis Unified IDE (2024.1) ?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 581 subscribers
  • Views 4744 views
  • Users 0 members are here
Related

(solved) Did you manage to debug a Microblaze RISC-V with Vitis Unified IDE (2024.1) ?

Jan Cumps
Jan Cumps over 1 year ago

I've made a Vivado 2024.1 design with a Microblaze RISC-V. With debug functionality. I have done similar activities in the past, With Vivado 2022.1.
I exported the hardware design, started a Vitis project, and created a simple microblaze Hello application.

Vitis knows the Microblaze is there. The application builds in Vitis without issues. I also can load the bitstream file to the FPGA, over JTAG.

But when I want to program the MicroBlaze, or debug it, the debugger doesn't find the core. It finds the two ARM cores inside the Zinq, but not the MB I designed in fabric.

I have this working in Viado / Vitis 2022.1, where they aren't using the Unified IDE yet.

Vitis can load the bitfile without issues, over JTAG:

image

But when starting the programmer or debugger, it doesn't find the MicroBlaze in the JTAG chain.

Error:

no targets found with "name =~ "Hart*"". available targets: 1* APU 2 ARM Cortex-A9 MPCore #0 (Running) 3 ARM Cortex-A9 MPCore #1 (Running) 4 xc7z020

I found same errors on google, but no solutions that worked ...

  • Sign in to reply
  • Cancel

Top Replies

  • bidrohini
    bidrohini over 1 year ago +1
    The debug functionality for MicroBlaze should be correctly set up in your Vivado block design. Verify that the MicroBlaze core has the necessary debug configuration enabled (like JTAG interface) in the…
  • Jan Cumps
    Jan Cumps over 1 year ago +1
    I was able to get it working: What did I do different: Initially, I loaded the bitfile to the FPGA via Vitis menu Vitis -> Program device. And then, when debugging, I got the behaviour as described…
  • bidrohini
    bidrohini over 1 year ago

    The debug functionality for MicroBlaze should be correctly set up in your Vivado block design. Verify that the MicroBlaze core has the necessary debug configuration enabled (like JTAG interface) in the hardware design.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 1 year ago

    I was able to get it working:

    image

    What did I do different:

    Initially, I loaded the bitfile to the FPGA via Vitis menu Vitis -> Program device. And then, when debugging, I got the behaviour as described in my original post.

    I have now changed the debug setup (click on the cog wheel next to the debug command), and added loading of the bit file to the launch setup:

    image

    That did the trick. I don't know yet if this is a workaround because something in my VHDL design is missing (did I implement the reset logic wrong?). Or if this is how it's supposed to be done.

    Anyways, I'm ready for debugging the MicroBlaze Slight smile

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 1 year ago in reply to bidrohini

    Thank you. It had the setup - but uncertain if I did all correctly.
    See comment Arrow down: how I got it working).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 1 year ago

    turns out that I don't have to load the bitfile, when the FPGA is already programmed. With the settings below, I can program and debug the microblaze, without reloading the bit file or resetting the ARM processor.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 1 year ago

    Debug example:

    I'm toggling Y11 (arduino A0). 

    image

    Debugger in action:

    image

    And the is driven high when executing this command:

    XGpio_DiscreteWrite(&Gpio, LED_CHANNEL, LED);

    image

    And when connected to the LED array instead of the Arduino A0-A5: