FPGA
  • Technologies
  • More
FPGA
Forum Turing my M5stack core2 to a flipper
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 581 subscribers
  • Views 5474 views
  • Users 0 members are here
  • Keyfob
  • core2
  • m5stack
  • flipper
  • github
  • fpga
  • usb
  • uart
  • programmable
Related

Turing my M5stack core2 to a flipper

Kobe
Kobe over 1 year ago

Hey guys, Im new to coding, but have general knowledge of hardware. Im about to take on task which is out my scrope but wit chatgpt i will try it. this what i will be doing, i bought all the parts , the hard part is the coding. if anyone is willing to jump on board this project let me know.  here is what im doing : 

Flipper-Like Project with M5Stack Core2

Welcome to the **Flipper-Like Project using M5Stack Core2**! This project aims to transform the M5Stack Core2 into a versatile, Flipper Zero-like device. By leveraging the Core2's hardware capabilities and expanding its functionality with additional modules and custom software, we hope to build a powerful tool for RF communication, signal analysis, and more.

---

## **Project Overview**

The goal of this project is to create a device inspired by the **Flipper Zero**, but based on the open-source-friendly **M5Stack Core2** hardware. This project will focus on:

- **RF communication**: Support for common protocols like Sub-1GHz, Bluetooth, Wi-Fi, and LoRa.
- **Modularity**: Integration with M5Stack modules (e.g., LoRa, RS485, Proto Boards).
- **User Interface**: A touchscreen interface powered by the Core2's built-in display.
- **Expandability**: Allow for additional custom hardware, such as CC1101, NRF24L01, and FPGA modules.
- **Open Development**: Create a community-driven project where developers can contribute new features and improve existing ones.

---

## **Current Features**

- **Hardware Integration**:
- M5Stack Core2 touchscreen and processing power.
- RF modules: CC1101, LoRa (433MHz and 900MHz), and NRF24L01.
- Support for additional modules: FPGA (iCESugar-nano), ESP32, and external antennas.

- **Planned Functionalities**:
- Sub-1GHz scanning and transmission.
- Signal replay and analysis.
- Wi-Fi and Bluetooth communication.
- Infrared (IR) support.
- GPIO-based hacking tools.

---

## **Hardware Requirements**

### **Required Components**
1. **M5Stack Core2**: The central controller with a touchscreen interface.
2. **RF Modules**:
- CC1101 RF Module.
- NRF24L01 Wireless Module.
- LoRa Modules (e.g., Ra-08 and Ra-08H).
3. **Expansion Modules**:
- M5Stack Proto Boards.
- iCESugar-nano FPGA Development Board.
4. **Antennas**:
- Sub-1GHz antennas.
- External directional antennas for extended range.
5. **Power Supply**:
- M5Stack Battery Modules (13.2).
6. **Miscellaneous**:
- SMA connectors, jumper wires, headers, etc.

---

## **Software Requirements**

1. **Firmware Development**:
- PlatformIO with Visual Studio Code for development.
- ESP-IDF for Core2 programming.

2. **Features Under Development**:
- A user-friendly interface for scanning and replaying RF signals.
- Drivers for CC1101, NRF24L01, and LoRa modules.
- Wi-Fi and Bluetooth utilities for hacking and testing.

3. **Libraries and Dependencies**:
- **M5Stack Core2 Libraries**: Touchscreen, display, and GPIO handling.
- **RF Driver Libraries**: For Sub-1GHz communication (e.g., ELECHOUSE CC1101 library).
- **Signal Processing Libraries**: FFT and RF signal encoding/decoding.

---

## **How to Contribute**

1. **Fork and Clone**
- Fork this repository and clone it to your local machine.

2. **Set Up Development Environment**
- Install PlatformIO and required libraries.
- Flash the initial firmware onto the Core2 to verify setup.

3. **Choose a Task**
- Check the [Issues](#issues) tab for open tasks.
- Suggest new features or improvements in Discussions.

4. **Submit Pull Requests**
- Develop your feature or fix and submit a pull request.
- Include detailed descriptions of changes made.

---

## **Getting Started**

1. **Prepare the Core2**:
- Flash the provided base firmware.
- Connect required modules (e.g., CC1101, NRF24L01).

2. **Install Software**:
- Clone this repository.
- Set up the development environment with PlatformIO.

3. **Test Basic Functionality**:
- Verify touchscreen and RF module communication.
- Test signal scanning and basic transmissions.

---

## **Future Plans**

1. **Expand RF Protocol Support**:
- Add support for Zigbee, Z-Wave, and other protocols.
2. **Develop Community Plugins**:
- Enable developers to create custom tools and utilities.
3. **Improve Usability**:
- Add graphical tools for signal analysis and automation.

---

## **Contact and Support**

If you have any questions or need support:
- Open a discussion or issue on this GitHub repository.
- Contact the project maintainer via email or the community chat.

---

Together, we can create an open-source alternative to Flipper Zero that empowers users and supports innovation. Let's build something amazing!

  • Sign in to reply
  • Cancel

Top Replies

  • JWx
    JWx over 1 year ago +1
    Something like this one? https://github.com/pr3y/bruce Bruce stems from a keen observation within the community focused on devices like Flipper Zero. While these devices offered a glimpse into the…
Parents
  • JWx
    JWx over 1 year ago

    Something like this one?

    https://github.com/pr3y/bruce

    Bruce stems from a keen observation within the community focused on devices like Flipper Zero. While these devices offered a glimpse into the world of offensive security, there was a palpable sense that something more could be achieved without being that overpriced, particularly with the robust and modular hardware ecosystem provided by ESP32 Devices, Lilygo and M5Stack products.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • JWx
    JWx over 1 year ago

    Something like this one?

    https://github.com/pr3y/bruce

    Bruce stems from a keen observation within the community focused on devices like Flipper Zero. While these devices offered a glimpse into the world of offensive security, there was a palpable sense that something more could be achieved without being that overpriced, particularly with the robust and modular hardware ecosystem provided by ESP32 Devices, Lilygo and M5Stack products.