FPGA
  • Technologies
  • More
FPGA
Forum Hardware Manager unconnected. Autoconnect crashes
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 580 subscribers
  • Views 2433 views
  • Users 0 members are here
  • jtag
  • usb
  • som
  • k24
Related

Hardware Manager unconnected. Autoconnect crashes

sam_jones
sam_jones over 1 year ago

Hi all,

i am able to run linux images on the K24 SoM board via SD card image.

However i cant access the board via JTAG. Open Hardware doesnt detect it.

I have run "install" scripts in /xicom. Other Xilinx FPGAs (e.g. Zybo) are immediately detectable.

Do i have to install any special drivers ?

Thanks

  • Sign in to reply
  • Cancel

Top Replies

  • iksevas
    iksevas over 1 year ago +2
    The JTAG interface uses an FTDI chip. Have you that driver installed?
  • kmikemoo
    kmikemoo over 1 year ago in reply to sam_jones +1
    sam_jones If your cable is communicating enough to run the install scripts, you don't need a different cable. If the cable communicates on a different system, you don't need a different cable. If you're…
  • sam_jones
    sam_jones over 1 year ago in reply to iksevas +1
    This did the trick for me . I thought that was only meant for Windows platforms. Btw. while running ftdi_program , i encountered some missing *.so error. Find more details on the link below on how to resolve…
Parents
  • manihatn
    manihatn over 1 year ago

    I have only used KV260 boards and those didn't require any special driver. So I would expect the same here. It doesn't appear like a cable problem.

    A couple of questions:

    1. It might be good to check the default boot mode for the board. Have you tried setting the boot mode to JTAG? I remember we can do it using some tcl scripts.

    2. Which version of Vivado and Petalinux tools are you using to build your custom image ? What are the version of the tools with which the SD card image was built?

    3. The reason for the above is to check if the K24 SOM  is compatible with your version of Vivado tools  

    Hardware manager can behave strange some times when you swapping between a K24 (Zynq US+) and Zybo (Zynq). I have had instances where it holds the state of the device even after disconnecting it and connecting it to a new device. So the hardware manager task needs to be removed cleanly from from the task list or a restarted. A cold restart might make a difference. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • manihatn
    manihatn over 1 year ago

    I have only used KV260 boards and those didn't require any special driver. So I would expect the same here. It doesn't appear like a cable problem.

    A couple of questions:

    1. It might be good to check the default boot mode for the board. Have you tried setting the boot mode to JTAG? I remember we can do it using some tcl scripts.

    2. Which version of Vivado and Petalinux tools are you using to build your custom image ? What are the version of the tools with which the SD card image was built?

    3. The reason for the above is to check if the K24 SOM  is compatible with your version of Vivado tools  

    Hardware manager can behave strange some times when you swapping between a K24 (Zynq US+) and Zybo (Zynq). I have had instances where it holds the state of the device even after disconnecting it and connecting it to a new device. So the hardware manager task needs to be removed cleanly from from the task list or a restarted. A cold restart might make a difference.