FPGA
  • Technologies
  • More
FPGA
Forum The Cray 1A Supercomputer
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 584 subscribers
  • Views 2964 views
  • Users 0 members are here
  • fpga
  • cray 1a
Related

The Cray 1A Supercomputer

clem57
clem57 over 10 years ago

     Browsing the web, a saw this great picture of a famous CRAY 1A built in 1975 by Seymour Cray after four years of design work. It was revolutionary because it used ICs for the first time in a supercomputer even though they were around since the 1960's. Here is a picture of one in the computer museum.

 

900px-Cray-1_%281%29.jpg

                         Courtesy of https://en.wikipedia.org/wiki/Cray-1



image

     What was interesting was someone decided to implement this machine on a FPGA. So in the matter of 40 years give or take a few, we have a quantum leap in technology

and an impressive reduction in cost.

spartan3_1600.jpg

 

 

The Hardware

The actual design was implemented in a Xilinx Spartan-3E 1600 development board.

This is basically the biggest FPGA you can buy that doesn’t cost thousands of dollars for a devkit.

The Cray occupies about 75% of the logic resources, and all of the block RAM.

 

From the website: Homebrew Cray-1A

 

Message was edited by: e14 Community moderator for HTML error reasons.

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 7 years ago +3
    This Cray implementation is quite old and some of the information re. FPGAs is very out of date. The Spartan 3E 1600 is no longer supported by current Xilinx tools and is certainly way below the curve…
  • jw0752
    jw0752 over 10 years ago +2
    It is great to have lived in a time period where this much progress has been made in only 40 short years. Thanks for illustrating the extent to which computer technology has eclipsed the landmark accomplishments…
  • ralphjy
    ralphjy over 7 years ago in reply to ntewinkel +2
    I'm amazed that he got his wife to help
Parents
  • DAB
    DAB over 7 years ago

    Yes, I remember when the Cray was the gold standard for processing speed.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • DAB
    DAB over 7 years ago

    Yes, I remember when the Cray was the gold standard for processing speed.

     

    DAB