FPGA
  • Technologies
  • More
FPGA
Forum FPGA SoC for ASIC/RTL portfolio projects: Arty Z7-20 vs Kria KR260, plus STM32?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 581 subscribers
  • Views 115 views
  • Users 0 members are here
Related

FPGA SoC for ASIC/RTL portfolio projects: Arty Z7-20 vs Kria KR260, plus STM32?

Khalil_11
Khalil_11 1 day ago

I’m looking for advice on building strong independent skills and a portfolio for entry-level ASIC/RTL design roles. My main interests are digital logic, RTL, and computer architecture, but I also want enough embedded knowledge to work comfortably with hardware/software interfaces.

I’ve used Verilog, Libero, and ModelSim during an FPGA internship, plus some ESP32, but I need to become more independent at designing, verifying, and debugging projects.

I’m interested in an FPGA SoC with a built-in processor so I can write my own RTL and learn memory-mapped interfaces, interrupts, and DMA. ChatGPT suggested the Digilent Arty Z7-20 and AMD Kria KR260, but I’d appreciate an independent opinion on whether either fits my goals. I’m open to other recommendations.

I’m also considering an STM32 board alongside the FPGA SoC. Would that add useful experience, or would it spread my attention too thin? My hardware budget is up to $1,000, but I’d prefer to spend less and avoid expensive software or IP licenses.

My main questions are:

• How should I prioritize SystemVerilog, verification, timing constraints, computer architecture, and embedded C?
• What projects would demonstrate useful engineering ability beyond following tutorials?
• What hardware would you buy for those projects, and what would you build first?

Please connect any board recommendation to concrete projects and mention relevant tool or licensing limitations.

  • Sign in to reply
  • Cancel
  • veluv01
    0 veluv01 1 day ago
    Khalil_11 said:
    I’m interested in an FPGA SoC with a built-in processor so I can write my own RTL and learn memory-mapped interfaces, interrupts, and DMA.

    You can also use an {Programmable Logic}PL fabric only FPGA Dev board like the Arty A7-100 or even the Nexys A7 too. It's just that you'll be using the softcore processor like the Microblaze-V, which is available for free in the Vivado IP catalog and you can try all of the stuff you listed out, and additionally you can also try to build your own RISC-V soft core processor too. If you're gonna need a SoC FPGA i.e FPGA with a ARM processor go with the Arty Z7-20 [Zynq  7020], Digilent has some really good documentation for getting started. KR260 isn't beginner friendly as it's an MPSoC and does require a lot of resources (to work with it, in this ongoing RAM crisis) when compared to the Zynq 7020 and Artix A100.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • fpgaguru
    0 fpgaguru 1 day ago

    For serious work I recommend the Kria KR260 board, it is well within your budget and it has a Zynq UltraScale+ FPGA as opposed to the much older 7-Series alternatives. It is targeted for robotic and industrial applications, if that's your cup of tea. It comes with a Vivado/Vitis license for this board included so you are not limited by the free version of the tools. 

    I also suggest you take a look at Ross AI, AMD's free and AI agnostic AI agent, it should be able to help with learning and using the tools. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett 1 day ago

    You are obviously close to the start of your FPGA journey. I strongly urge you not splash your budget out on an expensive board - the Digilent Arty is plenty to get on with. You could start cheaper but the support will be worse.

    Maybe re-consider getting into a system on a chip approach - if you look at the questions that arise about FPGAs on E14 you'll see that a lot of them are people getting bogged down in fighting the Linux OS on the FPGA - you can do that cheaper elsewhere.

    If you get an entry level job it is very unlikely that you will be let loose to do everything from RTL to computer architecture - there are lots of Linux experts - few RTL experts so I suggest you start off trying to do useful stuff with non SOC type FPGA board. One based on AMD Artix 7 or Spartan 7 would be suitable.

    It's always hard to think of good learning projects that will impress employers -  so do stuff that is interesting to you.

    At the beginning concentrate on Verilog (if you must  - I prefer VHDL but you will need to be capable in both - I think learning  VHDL first teaches better habits but it's not important  to you yet)

    RTL, Timing, constraints (not just timing)

    Using AMD/Xilinx is probably the best bet - the free tools will be adequate.

    Do the usual traffic lights, pong, video controller

    A good challenge project is to make an Ethernet controller which can send and receive UDPs without using a ready written MAC or on chip processor or processor IP.

    Learn embedded C on a processor  - almost anything will do.

    MK