FPGA
  • Technologies
  • More
FPGA
Forum snickerdoodle/snickerdoodle black (really needs a better name)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 13 replies
  • Subscribers 585 subscribers
  • Views 2419 views
  • Users 0 members are here
Related

snickerdoodle/snickerdoodle black (really needs a better name)

gdstew
gdstew over 10 years ago

Since this is kind of a crossover I'm not sure it belongs in the FPGA group, however:

 

Has anyone else seen this https://www.crowdsupply.com/krtkl/snickerdoodle ? For a Zynq 7Z010 based board, $60 including shipping is a good price. An extra $10 gets 1 GB SDRAM (512 MB for base unit).

A $149 black version uses the 7Z020 and includes 1 GB SDRAM.

 

I'm not familiar with Crowd Supply so I'm a little hesitant to buy in.

 

Edit: fixed link, thanks Paul.

  • Sign in to reply
  • Cancel

Top Replies

  • fustini
    fustini over 10 years ago +1
    RE: Crowd Supply, I bought my Open Source Hardware Novena laptop through them last year and was pleased with their service ( Novena: Open Source Hardware laptop launches! ) One of the founders was recently…
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to johnbeetem +1
    Thanks, John. Maybe you can get one on order just in case your schedule frees up in a couples months... Can't go wrong with $55 The open-course Lattice stuff is certainly interesting and they have some…
  • johnbeetem
    johnbeetem over 10 years ago in reply to clem57 +1
    Clem Martins wrote: Ryan Cousins I am confused about the Pi smasher. Why would I need/use it? Snickerdoodle by itself is a small module with high-density connectors. To do anything useful with…
Parents
  • johnbeetem
    johnbeetem over 10 years ago

    $60 including shipping is attractive until you realize that to do useful things with the board you probably need one of the base boards (e.g., the $55 piSmasher), which means you need to add $10 to put the high-density connectors on the bottom of the board.  This configuration is now $55 + $10 + $55 = $120 plus $10 if you want as much DRAM as RasPi 2 plus shipping.  That's still a competitive price for a Zynq, but not an amazing deal.

     

    I haven't delved into Zynq for several reasons.  First is the high cost of development boards in past years.  Second, I've read too many comments on what a pain it is to get software running on Zynq.  This is all second-hand, so I don't know what the answer is.  Xilinx makes outstanding silicon, but their tools have a very steep learning curve and their previous foray into integrated Power PC cores didn't go so well.  I'm also leery of an FPGA family that's still so expensive (single-chip pricing from distributors) even though it's been out for several years now.  The original Zynq article in Xilinx's Xcell Journal 2Q2011 suggested "a starting price below $15".

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • johnbeetem
    johnbeetem over 10 years ago

    $60 including shipping is attractive until you realize that to do useful things with the board you probably need one of the base boards (e.g., the $55 piSmasher), which means you need to add $10 to put the high-density connectors on the bottom of the board.  This configuration is now $55 + $10 + $55 = $120 plus $10 if you want as much DRAM as RasPi 2 plus shipping.  That's still a competitive price for a Zynq, but not an amazing deal.

     

    I haven't delved into Zynq for several reasons.  First is the high cost of development boards in past years.  Second, I've read too many comments on what a pain it is to get software running on Zynq.  This is all second-hand, so I don't know what the answer is.  Xilinx makes outstanding silicon, but their tools have a very steep learning curve and their previous foray into integrated Power PC cores didn't go so well.  I'm also leery of an FPGA family that's still so expensive (single-chip pricing from distributors) even though it's been out for several years now.  The original Zynq article in Xilinx's Xcell Journal 2Q2011 suggested "a starting price below $15".

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • gdstew
    gdstew over 10 years ago in reply to johnbeetem

    Actually no, I do not need/want/see much use for the PiSmasher (-$55), although I would probably put the connectors on the bottom (+$10), and go for the 1 GB SDRAM ($+10, total $80).

    Somehow you also forgot to mention the "other" expansion board that is $25 but I don't need it either. And to do what I want this board for  you would also need to add a FPGA board to the

    Pi (+$70+ dollars) so now we are talking about apples/apples.

     

    Development board costs in the past are irrelevant here, I am talking about this board. Since this is a dual-core ARM part I don't see past PowerPC products as a problem either. FPGA tools

    for complicated FPGAs are going to have a steep learning curve. I think it has something with complicated but I might be wrong. I don't really care about retail prices for chips as I usually am

    not developing products (there are exceptions, this is not one).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to johnbeetem

    Just depends on what you're looking for, John. If all you need is a couple USB ports and an HDMI jack, you're probably set with R Pi. But if you need I/O, want Gigabit Ethernet or HDMI in, Wi-Fi & Bluetooth, you're much better off with snickerdoodle + piSmasher (or just getting snickerdoodle alone if you don't need the bulkier connectors).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 10 years ago in reply to e14 Contributor

    Ryan Cousins wrote:

     

    Just depends on what you're looking for, John. If all you need is a couple USB ports and an HDMI jack, you're probably set with R Pi. But if you need I/O, want Gigabit Ethernet or HDMI in, Wi-Fi & Bluetooth, you're much better off with snickerdoodle + piSmasher (or just getting snickerdoodle alone if you don't need the bulkier connectors).

    US$55 ($65 with down connectors) is a great price for a Zynq module, so if you want something to plug into your own custom baseboard it's a nice way to go.

     

    I'd probably be interested in getting one for myself if I weren't already swamped with FPGA projects, mostly creating open-source tools for FPGA design.  So for me the Lattice iCE40 is particularly interesting.  It has a tiny fraction of the capabilities of a Zynq, but has a documented bitstream and an open-source toolchain, which isn't available for Xilinx FPGAs (yet).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to johnbeetem

    Thanks, John. Maybe you can get one on order just in case your schedule frees up in a couples months... Can't go wrong with $55 image

     

    The open-course Lattice stuff is certainly interesting and they have some great parts (we've even used a few of them on various snickerdoodle baseboard designs). There's some tricky stuff when it comes to open FPGA tools but a cool concept nonetheless.