FPGA
  • Technologies
  • More
FPGA
Forum ICE40UP5k in stock
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 21 replies
  • Subscribers 584 subscribers
  • Views 4863 views
  • Users 0 members are here
Related

ICE40UP5k in stock

michaelkellett
michaelkellett over 8 years ago

For anyone interested in a cheap DIY pcb assembly kind of FPGA:

 

Mouser have the Lattice ICE40UP5K-SG48ITR in stock at £4.98 each (25 off).

 

These are in a 48 pad QFP package with 0.5mm pitch but readily hand solderable (to a suitable pcb of course).

 

This part has 128k of RAM on chip as well as some other fun stuff.

 

iCE40 Ultra / UltraLite / UltraPlus - Lattice Semiconductor

 

MK

  • Sign in to reply
  • Cancel

Top Replies

  • rachaelp
    rachaelp over 8 years ago in reply to johnbeetem +7
    I just looked at the other thread you linked to and then saw the schematic linked by shabaz for the board. OMG... I'd have not bothered even looking at the PCB based on the schematic design alone. It looks…
  • shabaz
    shabaz over 8 years ago in reply to rachaelp +7
    I think it is a bit mean he is blaming a 'high school kid from Sri Lanka'. The product is from his firm with his name on his website, he should take responsibility. The buck stops with him. He should have…
  • shabaz
    shabaz over 8 years ago in reply to johnbeetem +5
    Hi John! I think it is possible the price-point is low because it could be reusing old components, maybe.. There was some comment on the other thread that the serial flash had strings in it from some other…
Parents
  • rachaelp
    rachaelp over 8 years ago

    Oh that looks like a cool little device. There is probably scope for creating a carrier board which gives access to all the IO but deals with any power and clocking in a breadboard friendly format maybe with a microUSB for connecting to the PC for programming. Hmmm, I can see an additional project coming up image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 8 years ago in reply to rachaelp

    rachaelp  wrote:

     

    Oh that looks like a cool little device. There is probably scope for creating a carrier board which gives access to all the IO but deals with any power and clocking in a breadboard friendly format maybe with a microUSB for connecting to the PC for programming. Hmmm, I can see an additional project coming up

    The iCE40UP5K is the FPGA on the US$8 Gnarly Grey UPduino.  The board has some electrical issues, so check the last link.  It doesn't have a built-in programmer.

     

    Edit: it still seems to be in stock at gnarlygrey.atspace.cc.  I first learned of the UPduino from andrea venturi's comment in Not-as-expensive FPGA Boards

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • rachaelp
    rachaelp over 8 years ago in reply to johnbeetem

    I just looked at the other thread you linked to and then saw the schematic linked by shabaz for the board. OMG... I'd have not bothered even looking at the PCB based on the schematic design alone. It looks like a dogs dinner and almost no thought was put into it other than wiring up to every pin. Such a poor design for something which should have been really quick and easy to do right for anybody with even basic hardware design experience. Shocking....

     

    So I wonder if there is any desire for a well designed board for this part in a similar form factor to that UPduino? Or any suggestions for a preferred form factor, feature requests, etc? I'm probably going to start putting something together for a test board as it's not going to take long and I can probably get the boards done on a panel with some other things I am planning to get PCB's made for.

     

    Best Regards,


    Rachael

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 8 years ago in reply to rachaelp

    rachaelp  wrote:

     

    Such a poor design for something which should have been really quick and easy to do right for anybody with even basic hardware design experience. Shocking....

    The designer said he paid a "High School/College kid in Sri Lanka" to do the layout.  Obviously a learning experience for him.

    rachaelp  also wrote:

     

    So I wonder if there is any desire for a well designed board for this part in a similar form factor to that UPduino? Or any suggestions for a preferred form factor, feature requests, etc? I'm probably going to start putting something together for a test board as it's not going to take long and I can probably get the boards done on a panel with some other things I am planning to get PCB's made for.

    I would be interested in one or two to start with if the price is good.  There's still no "standard" FPGA hobbyist/educational/prototyping board.  There are lots of boards from lots of vendors and none has hit the critical mass to be "the one" like Raspberry Pi.

     

    I have several iCE40 HX1K boards: an original iCEblink40 that's so old... [how old is it?]... it's so old that the chip is labeled Silicon Blue, the company that created iCE40 and was bought by Lattice.  I also have a Lattice iCEstick and a Nandland GoBoard.  My pet peeve with all of them is that they're hard-wired to boot from Serial Flash, so if you want to program the iCE40 FPGA configuration RAM directly (which is a lot faster) you have to do some PCB surgery.

     

    My preferences would be:

     

    1.  DIP form factor with 0.1" spacing on header holes.  Don't populate the headers, since users may want to do something custom with them.

     

    2.  FTDI programmer, e.g., an FT2232H or FT232H.  These are nice chips and software is easy, but unfortunately they are rather expensive... almost as much as the FPGA itself.  The dual-channel FT2232H is nice since you can use the second channel for a UART, but the single-channel FT232H is cheaper.  It could be depopulated for a low-cost version that's programmable through an optional header.

     

    3.  Make provision for programming the FPGA configuration RAM, e.g., some zero-Ohm jumpers to change from default Serial Flash programming to direct RAM programming.  I think Lattice has an HX8K board that has jumpers for this.

     

    4.  At least one user-programmable LED.

     

    The important thing is to keep it really cheap, which is very hard to do in small quantities.  The UPduino US$8 is pretty much impossible without vendor subsidy, and even iCEstick's US$25 with FT2232H is hard to meet without subsidy.  You'd be competing with those, so if you can't do it for US$25 you probably won't get much interest.  Kickstarter is a good way to get the initial volume up and to gauge level of interest.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 8 years ago in reply to rachaelp

    I think it is a bit mean he is blaming a 'high school kid from Sri Lanka'. The product is from his firm with his name on his website, he should take responsibility. The buck stops with him. He should have checked the design, if it really did come from a 'high school kid'. I'm sceptical (but then, I always am : ) And also tired of seeing poor quality products.

    I'm glad you're considering doing this : ) It is in capable hands : )

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 8 years ago in reply to rachaelp

    I think it is a bit mean he is blaming a 'high school kid from Sri Lanka'. The product is from his firm with his name on his website, he should take responsibility. The buck stops with him. He should have checked the design, if it really did come from a 'high school kid'. I'm sceptical (but then, I always am : ) And also tired of seeing poor quality products.

    I'm glad you're considering doing this : ) It is in capable hands : )

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • Cancel
Children
  • ntewinkel
    ntewinkel over 8 years ago in reply to shabaz

    >I think it is a bit mean he is blaming a 'high school kid from Sri Lanka'.

     

    I agree - if the designer chose to hire out the work to an intern, he's ultimately still responsible for the final product. To blame the intern for a product the company made shows the company is not trustworthy.

    Interesting way to develop a cheap product though.

     

    I wonder if he used Fiver.

    • Cancel
    • Vote Up +5 Vote Down