FPGA
  • Technologies
  • More
FPGA
Forum What resistor value do I need?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 20 replies
  • Subscribers 585 subscribers
  • Views 3742 views
  • Users 0 members are here
Related

What resistor value do I need?

andywest
andywest over 8 years ago

I have an 8 ohm, 0.5 watt speaker that I want to drive directly from an IO pin of an FPGA. I just want to generate simple square wave beeps, so I think I can connect like this:

 

FPGA IO pin -> resistor -> speaker -> ground

 

The IO pin is set to 3.3V LVTTL, and I can choose between 4mA and 8mA.

 

My question is what resistor values would I need for 4mA and 8mA to get the loudest volume without drawing too much current?

 

Thanks!

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 8 years ago +6
    Hi Andy, You can try a 470 ohm which will limit the current to the speaker to 8 mA. The problem is that most of the power will be across the resistor and the speaker may not be loud enough to hear. You…
  • dougw
    dougw over 8 years ago +5
    3.3v / 8mA = 412.5 ohms total 412.5 - 8 = 404.5 ohms for the extra resistor You might get double the effective voltage across your speaker by using a bridge tied load configuration. (use 2 output pins…
  • dougw
    dougw over 8 years ago in reply to andywest +4
    You still need the resistor on one pin but no ground.
Parents
  • jw0752
    jw0752 over 8 years ago

    Hi Andy,

     

    You can try a 470 ohm which will limit the current to the speaker to 8 mA. The problem is that most of the power will be across the resistor and the speaker may not be loud enough to hear. You could also try a small audio output transformer with a 500 ohm input and an 8 ohm output. This at least would put more of the power through to the speaker. Probably a good idea to put a flyback diode across the transformer primary so the spikes don't kill your FPGA's output. Another option would be to use a logic level MOSFET to drive the speaker and use the FPGA to drive the MOSFET.

     

    John

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • jw0752
    jw0752 over 8 years ago

    Hi Andy,

     

    You can try a 470 ohm which will limit the current to the speaker to 8 mA. The problem is that most of the power will be across the resistor and the speaker may not be loud enough to hear. You could also try a small audio output transformer with a 500 ohm input and an 8 ohm output. This at least would put more of the power through to the speaker. Probably a good idea to put a flyback diode across the transformer primary so the spikes don't kill your FPGA's output. Another option would be to use a logic level MOSFET to drive the speaker and use the FPGA to drive the MOSFET.

     

    John

    • Cancel
    • Vote Up +6 Vote Down