FPGA
  • Technologies
  • More
FPGA
Forum Arduino Gets into FPGAs with MKR Vidor 4000
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 584 subscribers
  • Views 1709 views
  • Users 0 members are here
Related

Arduino Gets into FPGAs with MKR Vidor 4000

rscasny
rscasny over 8 years ago

I've had on my desktop a little note that simply said "Arduino FPGA." Cryptic as the note sounds, it was an electronic sticky note reminding me to look up the specs of Arduino's new FPGA maker board, the MKR Vidor 4000.image

 

The board features an Intel (used to be Altera) Cyclone 10 FPGA that it expects to be used for high-speed DSP operations for audio and video processing.  Arduino will come out a visual editor that translates the design into Verilog, complies it on Arduino servers before downloading it all onto the FPGA. Sounds pretty easy. (Perhaps too easy?)

 

The FPGA contains 16K Logic Elements, 504Kbit of embedded RAM and 56 18x18 bit HW multipliers for high-speed DSP; Each pin can toggle at over 150 MHz and can be configured for functions such as UARTs, (Q)SPI, high res/ high freq PWM, quadrature encoder, I2C, I2S, Sigma Delta DAC, etc.

 

The MKR VIDOR 4000 features also a Microchip SAMD21, onboard 8 Mbyte SDRAM, 2 Mbyte QSPI Flash (1MB for user applications), Micro HDMI connector, MIPI camera connector, Wifi & BLE powered by U-BLOX NINA W10 Series, the classic MKR interface on which all pins are driven both by SAMD21 and FPGA and a MiniPCI Express connector with up to 25 user programmable pins.

 

Will this advance the adoption of FPGAs. I'm sure Arduino thinks so. What do you think?

  • Sign in to reply
  • Cancel

Top Replies

  • DAB
    DAB over 8 years ago +2
    It would be interesting to see how well the Arduino FPGA stacks up against a PSOC for ease of use and circuit complexity. DAB
  • gsgill112
    gsgill112 over 8 years ago +2
    Well, I think As Arduino is designed for pretty much everyone , They might have pre configured Logic Blocks/ IP to choose from. Nonetheless, FPGAs in an Arduino , It's just Awesome. Regards, GS Gill
  • Gough Lui
    Gough Lui over 8 years ago +2
    I'm hopeful. If anything, having open designs, good documentation, community support, potential for low-cost alternatives will only encourage adoption. However, I think users will need to better understand…
Parents
  • jc2048
    jc2048 over 8 years ago

    This forum on their website is worth a read-through as some of the (official) replies give an idea of what they're trying to do with it. It sounds like it's very early days on the programming side but there's potential there if they can get people using it and get the tools to a point where they're easy to use.

     

    http://forum.arduino.cc/index.php?board=125.0

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • jc2048
    jc2048 over 8 years ago

    This forum on their website is worth a read-through as some of the (official) replies give an idea of what they're trying to do with it. It sounds like it's very early days on the programming side but there's potential there if they can get people using it and get the tools to a point where they're easy to use.

     

    http://forum.arduino.cc/index.php?board=125.0