FPGA
  • Technologies
  • More
FPGA
Forum Get a Free Board -- Seeking 2 People to Build a Project with Digilent CMOD S7 featuring Spartan-7 FPGA
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 28 replies
  • Subscribers 587 subscribers
  • Views 6364 views
  • Users 0 members are here
  • scasny
  • xilinx
  • embedded
  • digilent
Related

Get a Free Board -- Seeking 2 People to Build a Project with Digilent CMOD S7 featuring Spartan-7 FPGA

rscasny
rscasny over 7 years ago

I often get members who want learn "the secret" of how to get picked as an official roadtester. Well, successful (and frequent) roadtesters usually start with something small: writing a blog, starting a discussion, or doing a small project -- all these things I look at when I make roadter selections.

 

I also get members who apply for roadtests for FPGA products yet have little or no background in programmable device technology nor any experience in the often-complex design tools for these devices. when you have 60 days to do a roadtest, I feel it would be a big burden on the roadtester if he/she had no experience in these things to begin with.

 

I have thought about both of these types of members and was looking for something simple that (a) would-be roadtester could do to build up their portfolio of things they have done on the community, and (b) something simple where they could learn about FPGAs and get some time to hone their skills with the associated design tool.

 

I hunted around and came up with the Digilent CMODS7 dev board featuring the Xilinx Spartan-7 FPGA. I have two of them I would like to giveaway to any member who feels he or she is in the above two groups and wants to take a step forward.

 

Let me tell you a little about the Digilent CMOD S7Digilent CMOD S7. It's a great little board that will help you increase your skills and help you demonstrate your ability to carry out a project to completion -- the key skill to be a super roadtester.image

 

The Digilent CMOD S-7 is a breadboardable Spartan-7 FPGA board.

 

It come in a small, 48‐pin DIP form factor board, featuring 32 FPGA digital I/O signals, 2 FPGA analog input signals, an external power input rail, and ground are routed to 100‐mil‐spaced through‐hole pins, making the Cmod S7 well suited for use with solderless breadboards. At just 0.7” by 3.05” inches, it can be loaded in a standard socket and used in embedded systems. The board also includes a programming ROM, clock source, USB programming and data transfer circuit, power supplies, LEDs, and buttons.

 

Here are some more features:

 

Xilinx Spartan‐7 FPGA (XC7S25‐1CSGA225C)

o 3,650 slices containing four 6‐input LUTs and 8 flip‐flops

o 1,620 Kbits of fast block RAM

o 3 clock management tiles, each with a phase‐locked loop and mixed‐mode clock manager

o 80 DSP slices

o Internal clock speeds exceeding 450 MHz

o On‐chip analog‐to‐digital converter (XADC)

o Programmable over JTAG and Quad‐SPI Flash

 

Memory

o 4 MB Quad‐SPI Flash

 

Power

o Powered from USB or 5V external supply connected to DIP pin 24

 

USB

o USB‐JTAG programming circuitry

o USB‐UART bridge

 

Push‐buttons and LEDs

o 2 Buttons

o 4 LEDs

o 1 RGB LED

 

Expansion Connectors

o 1 Pmod connector

 

Software Supportimage

The Cmod S7 is fully compatible with the high‐performance Vivado Registered Design Suite versions 2018.1 and newer. It is supported under the free WebPACKTm installation option, which does not require a license, so designs can be implemented at no additional cost. This free installation includes the ability to create MicroBlazeTm soft‐core processor designs. Design resources, example projects, and tutorials are available for download at the Cmod S7 Resource Center.

 

How To Get this Free Board

Leave a comment and tell me about yourself as an element14 member. Tell me about your electronics knowledge as well. What you have done on the community, and what you would like to do to get this board. I'l take a week or so and then review the comments. I'll end up picking two people. I'll send you the board and I you have to post a blog on the CMOD S& including pictures or videos of what you have done.

 

Sincerely,

 

Randall Scasny

RoadTest Program Manager

  • Sign in to reply
  • Cancel

Top Replies

  • rscasny
    rscasny over 7 years ago in reply to alphanu +3
    Hi Ben. I will be launching another free FPGA board project/giveaway next week. So, stay tuned. Thanks for your email. Randall
  • michaelkellett
    michaelkellett over 7 years ago in reply to mike-0rc +3
    There is a free (as in beer) version of Vivado with no time limits. https://www.xilinx.com/products/design-tools/vivado/vivado-webpack.html MK
  • zamaliphe
    zamaliphe over 7 years ago +2
    so about me well i'm computer programer i come across fpga world throw spartan 3E500 i learned the VHDL / verilog as start and i have done some small projects using it now i normally use HLS and c / c…
Parents
  • Fred27
    Fred27 over 7 years ago

    Have fun with it, guys. The Spartan 7 is a very impressive piece of hardware.

     

    neuromodulator If you're new to FPGAs then be prepared for quite a journey into the strange and unknown! A good journey, but a strange one.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Fred27
    Fred27 over 7 years ago

    Have fun with it, guys. The Spartan 7 is a very impressive piece of hardware.

     

    neuromodulator If you're new to FPGAs then be prepared for quite a journey into the strange and unknown! A good journey, but a strange one.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • zamaliphe
    zamaliphe over 7 years ago in reply to Fred27

    thanks

    Fred27

    i do agree FPGAs is a  quite  journey its dificult one as well .

    and spartan 7 would be great board for it

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • neuromodulator
    neuromodulator over 7 years ago in reply to Fred27

    Yeah I'm new... and FPGAs have always looked a bit scary to me. The most that I've done has been to download Vivado and play a bit with it (without any real FPGA of course). How was your FPGA learning journey?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mike-0rc
    mike-0rc over 7 years ago in reply to neuromodulator

    I have yet to learn any.....Although My place of work uses FPGA's in a wide range of products and they are willing to teach me, so it shouldn't take too long before I find my feet. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rscasny
    rscasny over 7 years ago in reply to neuromodulator

    Hi Miguel.

     

    I want to respond to you and your concerns.

     

    Let me step back a quick moment.

     

    One of the reasons I got these boards (element14 paid for them) was I wanted a little more flexibility in choosing people and timelines. I also wanted to get people who may not feel like they have the background to compete in a full FPGA board roadtest. I want to give opportunities to members who are interested in FPGAs and perhaps need something to learn from. (I have another board that I will be looking for people to blog for.)

     

    So, you say: "Yeah I'm new... and FPGAs have always looked a bit scary to me. The most that I've done has been to download Vivado and play a bit with it (without any real FPGA of course). How was your FPGA learning journey?"

     

    I think you said you have downloaded Vivado and played around with it a bit.

     

    I hope we can make FPGAs less scary to you as well as other members.

     

    It appears your concern was over the requirements I spelled out: 1-month to test and experiment and then write a blog,

     

    I realize everyone is different; we learn at different rates. One month was my ball park time, but this is a blog, not a roadtest, so there is some flexibility.

     

    If you were very experienced, I guess I would expect the blog to be more along the lines of a project. But you have less experience.

     

    So, perhaps the goal of your blog would be to work with the board with open eyes and go through it and write about the obstacles you are experiencing as someone new to programmable logic technology. Tell us about the board. Tell us about your experiences with Vivado. Tell us what other obstacles you are confronting. Tell us about your successes as well.

     

    Now, where can you get help?

     

    Well, a fantastic resource would be by an element14 member, Adam Taylor. Adam is now making himself available to answer questions. You can ask theme here: Get Your Xilinx FPGA/Programmable SoC Questions Answered here

     

    This resource should help you as well: https://reference.digilentinc.com/reference/programmable-logic/cmod-s7/reference-manual

     

    So, I've described how you can write the blog. What about the timeline? How about an extra two weeks? This will give you a bit more time to get yourself situated in working with this board.

     

    I'd like to give this to you because you responded first. Please email me privately with your mailing information: rscasny

     

    If you choose not to, please tell me, and I'll have to select someone else.

     

    Thanks.

     

    Randall