FPGA
  • Technologies
  • More
FPGA
Files Installing and Running XXICC rev 0.0p
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Next
  • Previous
  • Share
  • More
  • Cancel
Related
Recommended

Installing and Running XXICC rev 0.0p

This document describes how to install and run XXICC on your computer, either by compiling XXICC source code or installing binaries.  install00p.zip contains two files: install00p.pdf is the readable document and install.xoe is its source code which you can edit using the XXICC Object Editor (XOE).

 

This is revision 0.0p, which updates GNU/Linux FTDI permissions in section 5.3 to support the Gadget Factory Papilio DUO FPGA board.

 

For more information on XXICC and GalaxC, see the ’blog post XXICC (21st Century Co-design) release 0.0p and XXICC's home page: xxicc.org


install00p.pdf has instructions for installing XXICC for all versions (GNU/Linux and Windows) and for all purposes.  This means finding all the steps you need for a particular platform such as Raspberry Pi 2 can be a little involved.  As a supplement to Raspberry Pi 2 meets Papilio DUO, here are the specific steps for installing XXICC including Flavia on RasPi 2.  They have been tested on Raspbian “Wheezy” 2015-02-16.  For more detail on any of the steps, see install00p.pdf.

 

  1. Create a directory for XXICC.  You can call it anything you want, but the instructions assume you have called it XXICC and it’s in your home directory.

    cd ~
    mkdir XXICC

  2. Change to your XXICC directory: cd ~/XXICC
  3. Download the XXICC source code code00p.zip into your XXICC directory and unzip it:

    unzip code00p.zip

  4. Before compiling XXICC, you need to install the libxft developer’s libraries:

    sudo apt-get update
    sudo apt-get install libxft-dev

  5. Make a subdirectory for XXICC object code: mkdir xxicc.od
  6. Compile XXICC’s C files: make T=XGL

    This should create the XXICC executable xxicc in about 26 seconds.

  7. Install libftdi.so, which XXICC needs to talk to Papilio DUO’s FT2232H USB serial chip.

    sudo apt-get install libftdi1

    This installs libftdi.so.1.  However, XXICC needs it to be named libftdi.so, so you must add a symbolic link in /usr/lib/arm-linux-gnueabihf:

    cd /usr/lib/arm-linux-gnueabihf
    sudo ln -s libftdi.so.1 libftdi.so
    cd ~/XXICC

  8. Compile XXICC’s GalaxC files, including the ones needed for Flavia: ./xxicc fla

    When XXICC finishes compiling (about 36 seconds), it should bring up a file selection dialog.  For now, close the dialog and xxicc terminates.  The next time you run xxicc it will load object code and come up in less than a second.

  9. Before you use Papilio DUO, download 85-ftdi.rules (udev rules file for FTDI FT2232D/H, FT232H, and Papilio DUO) and copy it (using
    sudo) to /etc/udev/rules.d.  85-ftdi.rules sets permissions so that XXICC can talk to FTDI serial devices without having to run as superuser.  85-ftdi.rules takes effect when you reboot or you can reload udev rules with the command:

    sudo udevadm control --reload

    85-ftdi.rules requires that you are a member of the dialout group.  User pi is already in dialout.  Otherwise see if you’re in dialout by giving the groups command.  If you’re not in dialout, give the command:

    sudo adduser <userid> dialout

 

That should do it!  Please comment if you have any questions or helpful suggestions.

  • papilio-duo
  • raspberry-pi-2
  • flavia
  • xxicc
johnbeetem
johnbeetem
  • 16 May 2015
  • 1 Download