This is a compiled and linked XXICC executable binary "xxicw.exe" for Microsoft Windows on x86 PCs for users who do not want to build it from source code. "xxicw.exe" was built as described in Installing and Running XXICC rev 0.0q
…This is a compiled and linked XXICC executable binary "xxicw.exe" for Microsoft Windows on x86 PCs for users who do not want to build it from source code. "xxicw.exe" was built as described in Installing and Running XXICC rev 0.0q
…FlaviaLB60-00q.zip contains data files for the FlaviaLB60 implementation of the Free Logic Array, described in Flavia: the Free Logic Array and Chapter 12 of The XXICC Anthology rev 0.0q. FlaviaLB60 is for the ValentF(x) LOGI-Bone FPGA board, rev R1.0…
FlaviaLP60-00q.zip contains data files for the FlaviaLP60 implementation of the Free Logic Array, described in Flavia: the Free Logic Array and Chapter 12 of The XXICC Anthology rev 0.0q. FlaviaLP60 is for the ValentF(x) LOGI-Pi FPGA board, rev R1.2.
…Data files for the FlaviaP60 implementation of the Free Logic Array, described in Flavia: the Free Logic Array and Chapter 12 of The XXICC Anthology rev 0.0q. FlaviaP60 is for the Gadget Factory Papilio One 500K FPGA board. To reduce chances of confusion…
Data files for the FlaviaP40 implementation of the Free Logic Array, described in Flavia: the Free Logic Array and Chapter 12 of The XXICC Anthology rev 0.0q. FlaviaP32 is for the Gadget Factory Papilio One 250K FPGA board. To reduce chances of confusion…
This document describes how to install and run XXICC on your computer, either by compiling XXICC source code or installing binaries.
This is revision 0.0q, which adds the -rpio2 option for Raspberry Pi 2 and makes minor changes to Section 6.
For more information…
This document contains the source code for XXICC revision 0.0q in PDF for the convenience of users and developers who want to look at GalaxC source code without installing the XXICC Object Editor (XOE). .gal files are ASCII, but may contain control characters…
Source code and makefiles for XXICC code release 0.0q. You should be able to edit make, .h, and .c files using any text editor. .gal files may contain control characters that confuse your text editor, so you may need to use the XXICC Object Editor (XOE…
This book is a collection of miscellaneous XXICC topics. It supplements "Programming in the GalaxC Language".
For more information on XXICC, see the 'blog post XXICC (21st Century Co-design) release 0.0q and XXICC's home page: xxicc.…
Summary of enhancements and bug fixes for XXICC revision 0.0q.
For more information on XXICC and GalaxC, see the ’blog post XXICC (21st Century Co-design) release 0.0q and XXICC’s home page: xxicc.org.
FlaviaLP56-00p.zip contains data files for the FlaviaLP56 implementation of the Free Logic Array, described in Flavia: the Free Logic Array and Chapter 12 of The XXICC Anthology rev 0.0n. FlaviaLP56 is for the ValentF(x) LOGI-Pi FPGA board, rev R1.2.
…FlaviaLB56-00p.zip contains data files for the FlaviaLB56 implementation of the Free Logic Array, described in Flavia: the Free Logic Array and Chapter 12 of The XXICC Anthology rev 0.0n. FlaviaLB56 is for the ValentF(x) LOGI-Bone FPGA board, rev R1.0…
Data files for the FlaviaPD59 implementation of the Free Logic Array, described in Flavia: the Free Logic Array and Raspberry Pi 2 meets Papilio DUO. FlaviaPD59 is for the Gadget Factory Papilio DUO. To reduce chances of confusion, I recommend that you…
This document describes how to install and run XXICC on your computer, either by compiling XXICC source code or installing binaries. install00p.zip contains two files: install00p.pdf is the readable document and install.xoe is its source code which you…
This document is a udev rules file for the FTDI FT2232D, FT2232H, FT232H, and Gadget Factory Papilio DUO (which uses an FT2232H with a custom product ID).
For instructions on how to use 85-ftdi.rules, see Installing and Running XXICC rev 0.0q step 9.
If…
This document contains the source code for XXICC revision 0.0p in PDF for the convenience of users and developers who want to look at GalaxC source code without installing the XXICC Object Editor (XOE). .gal files are ASCII, but may contain control characters…
Source code and makefiles for XXICC code release 0.0p. You should be able to edit make, .h, and .c files using any text editor. .gal files may contain control characters that confuse your text editor, so you may need to use the XXICC Object Editor (XOE…
Summary of enhancements and bug fixes for XXICC revision 0.0p.
For more information on XXICC and GalaxC, see the ’blog post XXICC (21st Century Co-design) release 0.0p and XXICC’s home page: xxicc.org.
0.0p adds another Xilinx Spartan-6 Flavia implementation…
Summary of enhancements and bug fixes for XXICC revision 0.0n.
For more information on XXICC and GalaxC, see the 'blog post XXICC (21st Century Co-design) release 0.0n and XXICC's home page: xxicc.org.
0.0n adds two Xilinx Spartan-6 Flavia implementations…
These are the .xoe files for "Programming in the GalaxC Language", "The XXICC Anthology", install.pdf, compile.pdf, and TamingWB.pdf. It also includes the .gal files for collecting the individual .xoe chapter files into a book with…
Data files for the FlaviaLB56 implementation of the Free Logic Array, described in Flavia: the Free Logic Array and Chapter 12 of The XXICC Anthology rev 0.0n. FlaviaLB56 is for the ValentF(x) LOGI-Bone FPGA board. To reduce chances of confusion, I recommend…
Data files for the FlaviaLP56 implementation of the Free Logic Array, described in Flavia: the Free Logic Array and Chapter 12 of The XXICC Anthology rev 0.0n. FlaviaLP56 is for the ValentF(x) LOGI-Pi FPGA board. To reduce chances of confusion, I recommend…
Data files for the FlaviaP48 implementation of the Free Logic Array, described in Flavia: the Free Logic Array and Chapter 12 of The XXICC Anthology rev 0.0n. FlaviaP48 is for the Gadget Factory Papilio One 500K FPGA board. To reduce chances of confusion…
Data files for the FlaviaP32 implementation of the Free Logic Array, described in Flavia: the Free Logic Array and Chapter 12 of The XXICC Anthology rev 0.0n. FlaviaP32 is for the Gadget Factory Papilio One 250K FPGA board. To reduce chances of confusion…
These are compiled and linked XXICC executable binaries built as described in Installing and Running XXICC rev 0.0n, for users who do not want to build XXICC executables from source code. Includes executables for GNU/Linux on x86 PCs, Raspberry Pi, and…