FPGA
  • Technologies
  • More
FPGA
Polls Not-as-expensive FPGA Boards
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: johnbeetem
  • Date Created: 27 Aug 2017 8:57 PM Date Created
  • Last Updated Last Updated: 11 Oct 2021 2:57 PM
  • Views 7543 views
  • Likes 0 likes
  • Comments 35 comments
Related
Recommended

Not-as-expensive FPGA Boards

I haven't done a poll in a while so I thought it would be fun and instructive to do one about less-expensive FPGA boards.  One of the challenges of getting into FPGA design is that the boards are usually a lot more expensive than a Raspberry Pi or a microcontroller board from ST, NXP, or TI.  This may prevent people from giving FPGAs a try, which in turn makes the boards more expensive since they're manufactured in smaller quantities.

 

Still, if you look around there are some nice boards under US$100 and even under US$50.  I highly recommend Joel Williams' list of Cheap FPGA Development Boards.

 

Here are some boards available for US$50 or less that seem particularly interesting.  I've used the Papilio One and iCEstick myself.

 

  • Gadget Factory Papilio One 250K: This is one of my favorite boards and IMO a very good value at US$38.  It has a Xilinx Spartan-3E 250K, 48 I/Os on headers, and a JTAG programmer.  It's currently out of stock, but you get its "big brother" with a 500K part for US$65.

  • Generic Cyclone II board: Two years ago Michael Kellett wrote a nice 'blog about a US$15 Altera Cyclone II board available from Chinese distributor AliExpress.  It's an impressive board, except that it doesn't come with a programmer.  Michael was able to get a bundle with a programmer for just under US$50.

  • Lattice iCEstick:  At US$22 from some vendors, this is the least expensive FPGA board I know of that includes a programmer.  It has a Lattice iCE40 1K LUT FPGA, which is a small FPGA -- maybe a fifth the capacity of Papilio One 250K.   On the other hand, iCE40 is the only FPGA that has a fully open-source tool chain.

 

  • Numato Labs Mimas: At US$35, Numato's Mimas is the cheapest Spartan 6 LX9 board I've seen with a programmer.  It has a lots of I/O on headers, along with some LEDs and push-buttons.  Numato is based in India, so I don't know what shipping is like.  Numato also has Mimas V2 for US$50, which adds 64MB DDR SDRAM, VGA connector, and 3-digit 7-segment display but much less general-purpose I/O than Mimas.  And they also have the US$30 Elbert V2 with a 50K Xilinx Spartan 3A and I/O similar to Mimas V2.

 

  • Scarab Hardware miniSpartan3 is a small Xilinx Spartan 3A board with a 50K or 200K part for $30 or $40, including an on-board programmer.  I've never dealt with Scarab personally.  The miniSpartan3 is a nice size to incorporate into other projects and has lots of general-purpose I/O.

 

So which one do you like best?  Or is there another not-as-expensive FPGA board you prefer?  If you have experience with any of these boards or vendors, please comment.

  • icestick
  • papilio
  • xilinx
  • cyclone
  • fpgafeatured
  • fpga
  • lattice
  • altera
  • spartan
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • michaelkellett
    michaelkellett over 9 years ago in reply to michaelkellett +8
    Having said all that I've just ordered this: MAXimator PROMO with Expander shield and Kamami USB-Blaster - Kamami because I'm planning to use an Altera MAX10 (because I can get a lot of welly in a 144…
  • michaelkellett
    michaelkellett over 9 years ago +7
    Lattice ICE40HX8k-B-EVN, £34 from Mouser, Farnell don't stock it 8k FPGA with on board USB programmer and very little else except lots of uncluttered breakout pins. At the other end of the scale the Xilinx…
  • Jan Cumps
    Jan Cumps over 9 years ago +6
    other: Xess XuLA2 with beefy Spartan 6 XC6SLX25 FPGA all budget goes to a serious IC with as much pins broken out as possible and enough flash to persist the designs. No buttons, LEDs, displays, etc. The…
Parents
  • rsjsouza
    rsjsouza over 8 years ago

    The blog post with the generic Altera board points to a re-used Aliexpress link (points to a keypad product).

     

    The board, however, seems to be available for purchase from a brand called RioRand.

     

    With their USB Blaster, the total comes below US$50.00.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • johnbeetem
    johnbeetem over 8 years ago in reply to rsjsouza

    rsjsouza  wrote:

     

    The blog post with the generic Altera board points to a re-used Aliexpress link (points to a keypad product).

     

    The board, however, seems to be available for purchase from a brand called RioRand.

     

    With their USB Blaster, the total comes below US$50.00.

    Thanks.  Someone told me it's also available at DealExtreme (DX).  I don't know if that's a reliable vendor.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 8 years ago in reply to johnbeetem

    Here's another Altera dev board with blaster and some other stuff at a good price.

     

    MAXimator PROMO with Expander shield and Kamami USB-Blaster - Kamami

     

    I've got one of these and I'll do blog about it soon.

     

    It's based on the MAX10 FPGA which is  a good choice for DIY or low cost manufacturing processes since it comes in 144 pin TQFP and is available in single 3.3V supply versions.

     

    MK

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • rsjsouza
    rsjsouza over 8 years ago in reply to johnbeetem

    johnbeetem  wrote:

     

    rsjsouza   wrote:

     

    The blog post with the generic Altera board points to a re-used Aliexpress link (points to a keypad product).

     

    The board, however, seems to be available for purchase from a brand called RioRand.

     

    With their USB Blaster, the total comes below US$50.00.

    Thanks.  Someone told me it's also available at DealExtreme (DX).  I don't know if that's a reliable vendor.

    I haven't purchased anything from DealExtreme, but I know this is sold through Amazon.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • rsjsouza
    rsjsouza over 8 years ago in reply to michaelkellett

    michaelkellett  wrote:

     

    Here's another Altera dev board with blaster and some other stuff at a good price.

     

    MAXimator PROMO with Expander shield and Kamami USB-Blaster - Kamami

     

    I've got one of these and I'll do blog about it soon.

     

    It's based on the MAX10 FPGA which is  a good choice for DIY or low cost manufacturing processes since it comes in 144 pin TQFP and is available in single 3.3V supply versions.

     

    MK

    MK, that looks an excellent value.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • rsjsouza
    rsjsouza over 8 years ago in reply to michaelkellett

    michaelkellett  wrote:

     

    Here's another Altera dev board with blaster and some other stuff at a good price.

     

    MAXimator PROMO with Expander shield and Kamami USB-Blaster - Kamami

     

    I've got one of these and I'll do blog about it soon.

     

    It's based on the MAX10 FPGA which is  a good choice for DIY or low cost manufacturing processes since it comes in 144 pin TQFP and is available in single 3.3V supply versions.

     

    MK

    MK, that looks an excellent value.