FPGA
  • Technologies
  • More
FPGA
Polls Not-as-expensive FPGA Boards
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: johnbeetem
  • Date Created: 27 Aug 2017 8:57 PM Date Created
  • Last Updated Last Updated: 11 Oct 2021 2:57 PM
  • Views 7582 views
  • Likes 0 likes
  • Comments 35 comments
Related
Recommended

Not-as-expensive FPGA Boards

I haven't done a poll in a while so I thought it would be fun and instructive to do one about less-expensive FPGA boards.  One of the challenges of getting into FPGA design is that the boards are usually a lot more expensive than a Raspberry Pi or a microcontroller board from ST, NXP, or TI.  This may prevent people from giving FPGAs a try, which in turn makes the boards more expensive since they're manufactured in smaller quantities.

 

Still, if you look around there are some nice boards under US$100 and even under US$50.  I highly recommend Joel Williams' list of Cheap FPGA Development Boards.

 

Here are some boards available for US$50 or less that seem particularly interesting.  I've used the Papilio One and iCEstick myself.

 

  • Gadget Factory Papilio One 250K: This is one of my favorite boards and IMO a very good value at US$38.  It has a Xilinx Spartan-3E 250K, 48 I/Os on headers, and a JTAG programmer.  It's currently out of stock, but you get its "big brother" with a 500K part for US$65.

  • Generic Cyclone II board: Two years ago Michael Kellett wrote a nice 'blog about a US$15 Altera Cyclone II board available from Chinese distributor AliExpress.  It's an impressive board, except that it doesn't come with a programmer.  Michael was able to get a bundle with a programmer for just under US$50.

  • Lattice iCEstick:  At US$22 from some vendors, this is the least expensive FPGA board I know of that includes a programmer.  It has a Lattice iCE40 1K LUT FPGA, which is a small FPGA -- maybe a fifth the capacity of Papilio One 250K.   On the other hand, iCE40 is the only FPGA that has a fully open-source tool chain.

 

  • Numato Labs Mimas: At US$35, Numato's Mimas is the cheapest Spartan 6 LX9 board I've seen with a programmer.  It has a lots of I/O on headers, along with some LEDs and push-buttons.  Numato is based in India, so I don't know what shipping is like.  Numato also has Mimas V2 for US$50, which adds 64MB DDR SDRAM, VGA connector, and 3-digit 7-segment display but much less general-purpose I/O than Mimas.  And they also have the US$30 Elbert V2 with a 50K Xilinx Spartan 3A and I/O similar to Mimas V2.

 

  • Scarab Hardware miniSpartan3 is a small Xilinx Spartan 3A board with a 50K or 200K part for $30 or $40, including an on-board programmer.  I've never dealt with Scarab personally.  The miniSpartan3 is a nice size to incorporate into other projects and has lots of general-purpose I/O.

 

So which one do you like best?  Or is there another not-as-expensive FPGA board you prefer?  If you have experience with any of these boards or vendors, please comment.

  • icestick
  • papilio
  • xilinx
  • cyclone
  • fpgafeatured
  • fpga
  • lattice
  • altera
  • spartan
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • michaelkellett
    michaelkellett over 9 years ago in reply to michaelkellett +8
    Having said all that I've just ordered this: MAXimator PROMO with Expander shield and Kamami USB-Blaster - Kamami because I'm planning to use an Altera MAX10 (because I can get a lot of welly in a 144…
  • michaelkellett
    michaelkellett over 9 years ago +7
    Lattice ICE40HX8k-B-EVN, £34 from Mouser, Farnell don't stock it 8k FPGA with on board USB programmer and very little else except lots of uncluttered breakout pins. At the other end of the scale the Xilinx…
  • Jan Cumps
    Jan Cumps over 9 years ago +6
    other: Xess XuLA2 with beefy Spartan 6 XC6SLX25 FPGA all budget goes to a serious IC with as much pins broken out as possible and enough flash to persist the designs. No buttons, LEDs, displays, etc. The…
Parents
  • DAB
    DAB over 9 years ago

    Hi John,

     

    I would really like to see you do a sort of usability chart of the various software used to program the FPGA devices.

    I think most of us understand the basics, but are hesitant to jump in because of our perceived fear  of learning and using the development tools effectively.

     

    Key issues for me are the basic circuit development process, ease of implementation and testing/debug support.

     

    The best hardware in the world cannot compensate for a tedious development tool.

    Sometimes a lessor capability is more desirable because the tool set provided makes the implementation easy.

     

    Just a thought,

    DAB

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to DAB

    DAB wrote:

     

    ....

    I think most of us understand the basics,

    ....

    Don, I'm going to challenge that statement. I'm making the bold claim here that the toolchain is not the part that makes the learning curve steep.

    I think that it's the prerequisite to understand digital design knowledge - and as a second topic: understanding timing and delays.

    It's an uncommon skill for someone that didn't get a formal training (unlike programming - it's easier for hobbyists to pick that up because you can walk the steps of a program almost one by one).

    AND, OR, NOT gates and the likes are usually still graspable. Flip-flops can be learned in a good day.

    But then, understanding the more complex circuits based on these are often a challenge, let alone building a reasonable design based on these blocks.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • johnbeetem
    johnbeetem over 9 years ago in reply to Jan Cumps

    DAB wrote:

    I think most of us understand the basics...

     

    Jan Cumps wrote:

    Don, I'm going to challenge that statement. I'm making the bold claim here that the toolchain is not the part that makes the learning curve steep.

    I think that it's the prerequisite to understand digital design knowledge - and as a second topic: understanding timing and delays.

    It's an uncommon skill for someone that didn't get a formal training (unlike programming - it's easier for hobbyists to pick that up because you can walk the steps of a program almost one by one).

    AND, OR, NOT gates and the likes are usually still graspable. Flip-flops can be learned in a good day.

    But then, understanding the more complex circuits based on these are often a challenge, let alone building a reasonable design based on these blocks.

    "Logic!  Why don't they teach logic in these schools?" complains the Old Professor in The Lion, the Witch, and the Wardrobe.  I read somewhere that Lewis Carroll wrote his famous book Symbolic Logic because he discovered his undergraduates didn't understand the basics of logic, something they should have learned when they were 11 years old.

     

    I'm largely self-taught, and owe it to my mother who bought me a copy of Wff 'n Proof, now known as "the grandfather of educational games".  It was probably suggested to her by a well-meaning sales clerk and she probably bought it out of ignorance.  As a game it was a wash-out because there was nobody to play it with, but I devoured the instruction/text book and learned the basics of symbolic logic.  I found Lewis Carroll's book at the public library, along with various vintage logic and computer design books.  My first logic circuits were relay logic for my electric trains (done before reading any logic books) followed by discrete resistor-transistor logic copied from the GE Transistor Handbook, another great resource from the library.  You cannot imagine my delight when 7400-series logic came out and I could buy little insect-like packages that meant I didn't have to wire up transistors any more.  Geek heaven!

     

    Today it's much easier and at the same time much harder.  It's much easier because you can pick up something like a Lattice iCEstick for the cost of a restaurant dinner, but harder because of the complexity of installing and learning how to use tools.  It's much more intuitive to wire up a few transistors and resistors, just like it's easier to toggle in a small PDP-11 machine language program through the front panel switches than to learn to use the assembler and linker.  You're very limited in what you can practically do, but it's an easy start.

     

    I think the main challenge is to get people started.  When learning any new topic there's a spark of interest, which comes from seeing or reading about something cool.  If you can quickly make progress that spark grows into a flame, and then a blaze.  If it's hard to get started, the spark goes out, usually permanently.  The window varies a lot between individuals, and depends highly on what an individual thinks is "fun".

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • johnbeetem
    johnbeetem over 9 years ago in reply to Jan Cumps

    DAB wrote:

    I think most of us understand the basics...

     

    Jan Cumps wrote:

    Don, I'm going to challenge that statement. I'm making the bold claim here that the toolchain is not the part that makes the learning curve steep.

    I think that it's the prerequisite to understand digital design knowledge - and as a second topic: understanding timing and delays.

    It's an uncommon skill for someone that didn't get a formal training (unlike programming - it's easier for hobbyists to pick that up because you can walk the steps of a program almost one by one).

    AND, OR, NOT gates and the likes are usually still graspable. Flip-flops can be learned in a good day.

    But then, understanding the more complex circuits based on these are often a challenge, let alone building a reasonable design based on these blocks.

    "Logic!  Why don't they teach logic in these schools?" complains the Old Professor in The Lion, the Witch, and the Wardrobe.  I read somewhere that Lewis Carroll wrote his famous book Symbolic Logic because he discovered his undergraduates didn't understand the basics of logic, something they should have learned when they were 11 years old.

     

    I'm largely self-taught, and owe it to my mother who bought me a copy of Wff 'n Proof, now known as "the grandfather of educational games".  It was probably suggested to her by a well-meaning sales clerk and she probably bought it out of ignorance.  As a game it was a wash-out because there was nobody to play it with, but I devoured the instruction/text book and learned the basics of symbolic logic.  I found Lewis Carroll's book at the public library, along with various vintage logic and computer design books.  My first logic circuits were relay logic for my electric trains (done before reading any logic books) followed by discrete resistor-transistor logic copied from the GE Transistor Handbook, another great resource from the library.  You cannot imagine my delight when 7400-series logic came out and I could buy little insect-like packages that meant I didn't have to wire up transistors any more.  Geek heaven!

     

    Today it's much easier and at the same time much harder.  It's much easier because you can pick up something like a Lattice iCEstick for the cost of a restaurant dinner, but harder because of the complexity of installing and learning how to use tools.  It's much more intuitive to wire up a few transistors and resistors, just like it's easier to toggle in a small PDP-11 machine language program through the front panel switches than to learn to use the assembler and linker.  You're very limited in what you can practically do, but it's an easy start.

     

    I think the main challenge is to get people started.  When learning any new topic there's a spark of interest, which comes from seeing or reading about something cool.  If you can quickly make progress that spark grows into a flame, and then a blaze.  If it's hard to get started, the spark goes out, usually permanently.  The window varies a lot between individuals, and depends highly on what an individual thinks is "fun".

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • johnbeetem
    johnbeetem over 9 years ago in reply to johnbeetem

    johnbeetem wrote:

     

     

    I think the main challenge is to get people started. When learning any new topic there's a spark of interest, which comes from seeing or reading about something cool. If you can quickly make progress that spark grows into a flame, and then a blaze. If it's hard to get started, the spark goes out, usually permanently. The window varies a lot between individuals, and depends highly on what an individual thinks is "fun".

    I once saw a terrific juggler who was performing for children, including my daughters.  He said something very profound regarding education in general and juggling in particular.  He said: "Kids, if you want to learn to juggle, don't start with eggs.  Start with silk handkerchiefs because then you're juggling in slow motion."

     

    This is true of learning so many things: start with a simplified version to master the fundamentals, and then add complexity gradually as your knowledge and skills deepen.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 9 years ago in reply to johnbeetem

    Hi John,

     

    I agree.

     

    When I began programming the PDP-11, it was in machine language.

    When I learned electronics, it was tube design followed by and introduction into transistors.

     

    After that, learning integrated circuits, microprocessors, bit slice devices, higher level languages, operating systems and the rest were on the job training.

     

    What helped me was that early hands on working with actual bits and bytes coupled with logic mathematics and circuit design.

     

    Starting from the bottom up, you get used to working with the details, focusing on each wire connection, output loads, timing issues and all of the coordination needed between the hardware and the software.  Which is why I majored in Computer Engineering and not Computer Science.  The power of the computer was dependent upon knowing how to get the software to interact with the real world.

     

    As you said, getting started and persisting with your learning is key.

     

    Pick a FPGA device family, learn the tools, study a lot, play a lot, and learn how to exploit the devices.

     

    If you become proficient, you achieve a level of capability needed to fully exploit the technology.

     

    But it takes time and effort.  There are no free lunches involved with FPGA devices.  If you do not take the time to learn how to use them, then you will regret it.

     

    DAB

    • Cancel
    • Vote Up +4 Vote Down