FPGA
  • Technologies
  • More
FPGA
Polls Not-as-expensive FPGA Boards
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: johnbeetem
  • Date Created: 27 Aug 2017 8:57 PM Date Created
  • Last Updated Last Updated: 11 Oct 2021 2:57 PM
  • Views 7557 views
  • Likes 0 likes
  • Comments 35 comments
Related
Recommended

Not-as-expensive FPGA Boards

I haven't done a poll in a while so I thought it would be fun and instructive to do one about less-expensive FPGA boards.  One of the challenges of getting into FPGA design is that the boards are usually a lot more expensive than a Raspberry Pi or a microcontroller board from ST, NXP, or TI.  This may prevent people from giving FPGAs a try, which in turn makes the boards more expensive since they're manufactured in smaller quantities.

 

Still, if you look around there are some nice boards under US$100 and even under US$50.  I highly recommend Joel Williams' list of Cheap FPGA Development Boards.

 

Here are some boards available for US$50 or less that seem particularly interesting.  I've used the Papilio One and iCEstick myself.

 

  • Gadget Factory Papilio One 250K: This is one of my favorite boards and IMO a very good value at US$38.  It has a Xilinx Spartan-3E 250K, 48 I/Os on headers, and a JTAG programmer.  It's currently out of stock, but you get its "big brother" with a 500K part for US$65.

  • Generic Cyclone II board: Two years ago Michael Kellett wrote a nice 'blog about a US$15 Altera Cyclone II board available from Chinese distributor AliExpress.  It's an impressive board, except that it doesn't come with a programmer.  Michael was able to get a bundle with a programmer for just under US$50.

  • Lattice iCEstick:  At US$22 from some vendors, this is the least expensive FPGA board I know of that includes a programmer.  It has a Lattice iCE40 1K LUT FPGA, which is a small FPGA -- maybe a fifth the capacity of Papilio One 250K.   On the other hand, iCE40 is the only FPGA that has a fully open-source tool chain.

 

  • Numato Labs Mimas: At US$35, Numato's Mimas is the cheapest Spartan 6 LX9 board I've seen with a programmer.  It has a lots of I/O on headers, along with some LEDs and push-buttons.  Numato is based in India, so I don't know what shipping is like.  Numato also has Mimas V2 for US$50, which adds 64MB DDR SDRAM, VGA connector, and 3-digit 7-segment display but much less general-purpose I/O than Mimas.  And they also have the US$30 Elbert V2 with a 50K Xilinx Spartan 3A and I/O similar to Mimas V2.

 

  • Scarab Hardware miniSpartan3 is a small Xilinx Spartan 3A board with a 50K or 200K part for $30 or $40, including an on-board programmer.  I've never dealt with Scarab personally.  The miniSpartan3 is a nice size to incorporate into other projects and has lots of general-purpose I/O.

 

So which one do you like best?  Or is there another not-as-expensive FPGA board you prefer?  If you have experience with any of these boards or vendors, please comment.

  • icestick
  • papilio
  • xilinx
  • cyclone
  • fpgafeatured
  • fpga
  • lattice
  • altera
  • spartan
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • michaelkellett
    michaelkellett over 9 years ago in reply to michaelkellett +8
    Having said all that I've just ordered this: MAXimator PROMO with Expander shield and Kamami USB-Blaster - Kamami because I'm planning to use an Altera MAX10 (because I can get a lot of welly in a 144…
  • michaelkellett
    michaelkellett over 9 years ago +7
    Lattice ICE40HX8k-B-EVN, £34 from Mouser, Farnell don't stock it 8k FPGA with on board USB programmer and very little else except lots of uncluttered breakout pins. At the other end of the scale the Xilinx…
  • Jan Cumps
    Jan Cumps over 9 years ago +6
    other: Xess XuLA2 with beefy Spartan 6 XC6SLX25 FPGA all budget goes to a serious IC with as much pins broken out as possible and enough flash to persist the designs. No buttons, LEDs, displays, etc. The…
Parents
  • aventuri
    aventuri over 9 years ago

    today i've got a very light envelope with the boards inside; it took very few days..

     

    here a picture with my (fuzzy) phone..

     

    upduino  iCE40 FPGA board from Gnarly Grey

    boy, how small they are!!

     

    now it's time to test the blinking led demo.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 9 years ago in reply to aventuri

    How did you order 2 - I couldn't find anywhere to set the quantity yo buy.

     

    I've just ordered one at £7.99 (oddly a worse exchange rate than Paypal offered if I paid in $ but maybe that's for extra post.)

     

    I can't understand why Lattice don't get these parts into Digikey and Mouser, and even more I don't understand why Farnell are stocking XIlinx Ultra FPGAs at nearly £1000 per chip but don't stock the cheap Lattice and Altera parts that they might actually shift in numbers.

     

    Thanks for taking the plunge Andrea - keep us posted.

     

    MK

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • aventuri
    aventuri over 9 years ago in reply to michaelkellett

    yeah, there's no Q field.i made two payments separately, BUT i wrote in the notes that he could send me the devices in the same shipping..

     

    PS i'm told that the shipping is just 1$ if the envelope is less then 1/4 inch thick, otherwise it's 13$.. so can understand why the delivery is a bit of "a shot in the dark.."

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • aventuri
    aventuri over 9 years ago in reply to michaelkellett

    here some better pics; the flash is marked 25Q03213 E40 a Micron 32Mbit part..

     

    i need to solder the rails, actually..

     

    Upduino iCE40 UP5 front side

     

    Upduono back side with SPI flash

     

    PS maybe it's time to get out of this thread and move on a dedicate one..

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • aventuri
    aventuri over 9 years ago in reply to michaelkellett

    hello,

    after some trials, i've been able to write into the FPGA SRAM for a live test of a bitstream (created with IceCube2), here the "digital kitten video"! :-)

     

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

     

    i took some time for a couple of reasons:

    • as  i'm using a SBC with Allwinner A10, i was unable to find a library like wiringPi and i wrote GPIO with a direct access to registers via MMAP. it's really bare metal HW access, more performant!
    • the "clever" wiring of the board SPI interface can permit both to write a design bitstream into the SPI FLASH EEPROM and the load of the bitstream into the FPGA SAM (for a quick test, volatile).

    the two modes do need anyway to have the host application to write on one way (FLASH_MISO) for the first task, and on the other way for the second one (FLASH_MOSI). i took my time to wrap my head around the wiring (because the doc is not that clear on this topic..).

    i plan to release my simple app as soon as i've checked i can write the SPI FLASH too..

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 9 years ago in reply to aventuri

    My board turned up today, pretty quick considering where it came from.

     

    Initial reaction is that the design is not that good - no ground planes, decoupling caps too few and too far from the FPGA.

     

    I'll get some power on it some time in the next few days and see what it will actually do.

     

    MK

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • michaelkellett
    michaelkellett over 9 years ago in reply to aventuri

    My board turned up today, pretty quick considering where it came from.

     

    Initial reaction is that the design is not that good - no ground planes, decoupling caps too few and too far from the FPGA.

     

    I'll get some power on it some time in the next few days and see what it will actually do.

     

    MK

    • Cancel
    • Vote Up +3 Vote Down