A little more than a month ago a friend told me about a cheap wifi module. So I searched for this piece of wifi magic and founded the ESP8266 Wifi module. And it is really cheap. Depending on where you get it and the version we can say is between $5 and $8 for one module. Told myself I can spare $8 for this Wifi promise land so I ordered two for a little more than $8.
Yesterday I got them, right away I got very exited!! On yes, new toy!
First I realized that I ordered the ESP8266 ESP-03 model. Seems to be one of the favorites (from the forums) because it has several exposed digital IOs. But .... (there is always a but) it has no pin headers, so I said, no problem I solder a few and get done with it. Pin space separation is not the same as my pin headers. I then move to plan B (or C, hard to keep track when you are exited to get this working). Anyhow, the idea was to place it on a perf board and solder small wires to the position of some pin headers so I can wire this up.
I did manage to hook up some wires then the moment came. I got the usb to serial, connected to the device, opened the terminal window and.... and..... nothing! Nothing at all.
As of now I do not know if I damaged the device or the soldering is not good enough or even if I am totally wiring it incorrectly. For that I air my frustration here while I manage to get a lease from sleeping time to continue working on this.
It may be nothing, but this board has the antenna upside down. Comparing it to the other, and to others in the web. It might be nothing.
What is my future plan:
I got two of this, in the new un-touched one I will be more carefull.
1. Only wire the needed pins to avoid overheating the thing.
2. Hook everything through a level shifter to make sure I am on the safe side of the 3.3V
3. Pray
4. See what happens
Also there is one of the other versions in the way so I will try with other versions. I am sure this will be sorted out, and I will be able to use this for the Christmas decorations. But if someone is using one of these modules, or just have any comment, please do.
I will update with progress about this for others to benefit, there are not that many youtube videos about this device. However it seems to be working for a lot of folks.
I don't easily give up. Hope tonight I have the time to make this work.

Top Comments
-
camuyano
-
Cancel
-
Vote Up
0
Vote Down
-
-
Sign in to reply
-
More
-
Cancel
Comment-
camuyano
-
Cancel
-
Vote Up
0
Vote Down
-
-
Sign in to reply
-
More
-
Cancel
Children