Internet of Things
  • Technologies
  • More
Internet of Things
Blog Fail of the week with ESP8266 Cheap Wifi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Internet of Things to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: camuyano
  • Date Created: 17 Oct 2014 11:24 PM Date Created
  • Views 4176 views
  • Likes 4 likes
  • Comments 24 comments
  • uart_to_wifi_convert_module
  • hobbyist
  • esp8266
Related
Recommended

Fail of the week with ESP8266 Cheap Wifi

camuyano
camuyano
17 Oct 2014

A little more than a month ago a friend told me about a cheap wifi module. So I searched for this piece of wifi magic and founded the ESP8266 Wifi module. And it is really cheap. Depending on where you get it and the version we can say is between $5 and $8 for one module. Told myself I can spare $8 for this Wifi promise land so I ordered two for a little more than $8.

Yesterday I got them, right away I got very exited!! On yes, new toy!

First I realized that I ordered the ESP8266 ESP-03 model. Seems to be one of the favorites (from the forums) because it has several exposed digital IOs. But .... (there is always a but) it has no pin headers, so I said, no problem I solder a few and get done with it. Pin space separation is not the same as my pin headers. I then move to plan B (or C, hard to keep track when you are exited to get this working). Anyhow, the idea was to place it on a perf board and solder small wires to the position of some pin headers so I can wire this up.

I did manage to hook up some wires then the moment came. I got the usb to serial, connected to the device, opened the terminal window and.... and..... nothing! Nothing at all.

As of now I do not know if I damaged the device or the soldering is not good enough or even if I am totally wiring it incorrectly. For that I air my frustration here while I manage to get a lease from sleeping time to continue working on this.

It may be nothing, but this board has the antenna upside down. Comparing it to the other, and to others in the web. It might be nothing.

image

What is my future plan:

I got two of this, in the new un-touched one I will be more carefull.

1. Only wire the needed pins to avoid overheating the thing.

2. Hook everything through a level shifter to make sure I am on the safe side of the 3.3V

3. Pray

4. See what happens

 

Also there is one of the other versions in the way so I will try with other versions. I am sure this will be sorted out, and I will be able to use this for the Christmas decorations. But if someone is using one of these modules, or just have any comment, please do.

I will update with progress about this for others to benefit, there are not that many youtube videos about this device. However it seems to be working for a lot of folks.

 

I don't easily give up. Hope tonight I have the time to make this work.

  • Sign in to reply

Top Comments

  • hansaya
    hansaya over 11 years ago +2
    YAY!, got it working after countless hours of playing with this. Connect these lines CONNECT GPIO15 TO GROUND CONNECT CH_PD TO HIGH test this with serial terminal with 9600bud This should get the device…
  • jw0752
    jw0752 over 11 years ago +1
    Hi Javier, This type of problem happens to me frequently. The good part is that I usually end up learning more from my experience than I would have if the thing worked right the first time. I look forward…
  • e14 Contributor
    e14 Contributor over 11 years ago +1
    Hi Guys I'm very confused about this ESP03 chip. After watching countless hours of videos and reading, what do i actually have to connect to get this to work? I understand that I can only use 3.3volts…
Parents
  • hansaya
    hansaya over 11 years ago

    YAY!, got it working after countless hours of playing with this.

     

    Connect these lines

    CONNECT GPIO15 TO GROUND

    CONNECT CH_PD TO HIGH

    test this with serial terminal with 9600bud

     

    This should get the device going but then you need to change the firmware because the one came with mine did not reply to my AT commands

    CONNECT GPIO 0 TO GROUND

    with the the pins above. Then go with normal procedures to change the firmware. (115200bud)

    Cloud updating your Wi07C ESP8266 now! | Electrodragon Blog

     

    After the firmware update, you still need to keep the GPIO15 at ground to work.

     

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • camuyano
    camuyano over 11 years ago in reply to hansaya

    Congrats, so good to read about your success. As soon as I can I will try to mimic your achievement.

     

    Excellent work and thanks for sharing, post about what would you be doing with it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • hansaya
    hansaya over 11 years ago in reply to camuyano

    I'm trying to get a example firmware compiled, but not having much luck with it.

    I'm going to use the modules to make a home security system. Since its so cheap and small, if i can code to get GPIO pins working, then i could use stand alone modules to interface with sensors and outputs.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • camuyano
    camuyano over 11 years ago in reply to hansaya

    I compiled the AT sample from the sdk with some guy toolchain on linux. But failed to run it on the device. Also the other example I wasn't able to even compile it.
    If I am not mistaken this was the link I used https://github.com/esp8266/esp8266-wiki/wiki/Toolchain

    This module most definitely work as a great stand alone wifi sensor for a security system. I have only been able to download firmware to the module from windows, there is a script to download from python but I had no luck with it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • camuyano
    camuyano over 11 years ago in reply to hansaya

    I compiled the AT sample from the sdk with some guy toolchain on linux. But failed to run it on the device. Also the other example I wasn't able to even compile it.
    If I am not mistaken this was the link I used https://github.com/esp8266/esp8266-wiki/wiki/Toolchain

    This module most definitely work as a great stand alone wifi sensor for a security system. I have only been able to download firmware to the module from windows, there is a script to download from python but I had no luck with it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • hansaya
    hansaya over 11 years ago in reply to camuyano

    I had the same experience, only simple one works not the blinky. let me know if you had any luck with it. Look at this guy's example; I'm trying to figure out how to compile his example and seems like, good place to start

    wifi | FreeIO

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • hansaya
    hansaya over 11 years ago in reply to camuyano

    I had the same experience, only simple one works not the blinky. let me know if you had any luck with it. Look at this guy's example; I'm trying to figure out how to compile his example and seems like, good place to start

    wifi | FreeIO