Internet of Things
  • Technologies
  • More
Internet of Things
Blog Set up Elecrow TTN LoRaWAN gateway on Raspberry Pi - Pt. 1: build and test
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Internet of Things to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 28 Dec 2023 9:20 PM Date Created
  • Views 8046 views
  • Likes 8 likes
  • Comments 37 comments
  • raspberry
  • the things network
  • lorawan
  • ttn
  • gateway
  • iot
Related
Recommended

Set up Elecrow TTN LoRaWAN gateway on Raspberry Pi - Pt. 1: build and test

Jan Cumps
Jan Cumps
28 Dec 2023
Set up Elecrow TTN LoRaWAN gateway on Raspberry Pi - Pt. 1: build and test

I installed the software for the Elecrow LoRaWAN gateway (see  Low-Cost LoRaWAN Gateways! ), and enabled the gateway on The Things Network (TTN). I used Raspberry OS bullseye 32-bit lite on a Raspberry Pi  A+. I tested this on a B+ with the same OS too.

epic

Instructions from Elecrow: https://www.elecrow.com/wiki/index.php?title=LR1302_LoRaWAN_Gateway_Module

Preparation

sudo apt-get update

sudo apt install -y git

cd ~

run sudo raspi-config to enable

  • i2c,
  • SPI and
  • Serial Port. For Serial Port, do not allow console (question 1: no), but allow enabling of the port (question 2: yes).

Build the software


The following section is different than the vendor's instructions:

clone https://github.com/Elecrow-RD/LR1302_loraWAN.git

cd LR1302_loraWAN

cd LR1302_HAL

cd sx1302_hal

back to the existing instruction

make

Create new TTN Gateway

If you don't have an account yet, create one. Select the suggested settings for your location. Once logged in, navigate to the console. Select Gateways

image

Register your new Gateway. Accept the suggested frequency and setup. I used https://descartes.co.uk/CreateEUIKey.html to generate an ID

image

Then download the json file that's created for you. It holds some of the settings you 'll need to update in the gateway's config file later.

Configure the packet_forwarder

The following section is different than the vendor's instructions:

cd packet_forwarder

nano global_conf.json.sx1250.EU868

I had to change this line extra, not in instructions:
"gps_tty_path": "/dev/ttyS0",

back to the existing instruction

change the EUI in the config file, and check the TTN server URL. Save

The following section is different than the vendor's instructions:

chmod +x reset_lgw.sh

Test

back to the existing instruction

./lora_pkt_fwd -c global_conf.json.sx1250.EU868

You will get a log of what's happening:

image

The TTN console confirms it found you:

image

And after some time, you will appear on the maps: https://ttnmapper.org/heatmap/

image

I've tested with an Arduino MKR 1310, and all worked fine:

Proper install of all software (covered fully in the next blog)

There's more than this. To install all software in a location of your choice, check the instructions on git: https://github.com/Elecrow-RD/LR1302_loraWAN/blob/master/LR1302_HAL/sx1302_hal/readme.md

first edit target.cfg, and set your user name and location where to install (must exist)

Then 

make install

make install_conf

Full install post:  Set up Elecrow TTN LoRaWAN gateway on Raspberry Pi - Pt. 2: full install and run as service 

Enjoy

  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 1 year ago in reply to DaniLecx +1
    In the github issue you are referring to, there is a replacement reset script attached ( here ). If you overwrite sx1302_hal/bin/reset_lgw.sh with those contents, it should work with a sysfs-less linux…
  • Jan Cumps
    Jan Cumps over 1 year ago in reply to Jan Cumps +1
    the USE_LIBGPIOD setting in docker does the same : (see start file ) if [[ ${USE_LIBGPIOD} -eq 0 ]]; then cp /app/reset.sh.legacy ${RESET_FILE} else cp /app/reset.sh.gpiod ${RESET_FILE} fi /app…
Parents
  • DaniLecx
    DaniLecx over 1 year ago

    I get this error on my Raspberry Pi 4 64bit, looks like the issue is that GPIO sysfs is deprecated and superseded by libgpiod.

    github.com/.../120

    image

    After this I tried using basicstation-docker, it's better but now it gives me another error:

    image

    After adding this parameter in docker compose, it solved my issue :)

    USE_LIBGPIOD: 1

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 1 year ago in reply to DaniLecx

    In the github issue you are referring to, there is a replacement reset script attached (here). If you overwrite sx1302_hal/bin/reset_lgw.sh with those contents, it should work with a sysfs-less linux. As long as gpiod is installed.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps over 1 year ago in reply to DaniLecx

    In the github issue you are referring to, there is a replacement reset script attached (here). If you overwrite sx1302_hal/bin/reset_lgw.sh with those contents, it should work with a sysfs-less linux. As long as gpiod is installed.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Jan Cumps
    Jan Cumps over 1 year ago in reply to Jan Cumps

    the USE_LIBGPIOD setting in docker does the same : (see start file)

            if [[ ${USE_LIBGPIOD} -eq 0 ]]; then
                cp /app/reset.sh.legacy ${RESET_FILE}
            else
                cp /app/reset.sh.gpiod ${RESET_FILE}
            fi
    

    /app/reset.sh.legacy uses the old school sysfs approach

    /app/reset.sh.gpiod uses gpiod

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DaniLecx
    DaniLecx over 1 year ago in reply to Jan Cumps

    Yes you are right ! I had tried using reset_lgw.sh.gpiod but it told me gpiod wasn't installed so I gave up ( a bit fast indeed ).

    Using docker compose with basicstation was a bit more familiar and simple for me, that's a good alternative even though both approaches work :)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 1 year ago in reply to DaniLecx

    After installing, I had to do a few extra steps, to

    • run as a service and
    • avoid that the log filled the disk space

    I don't know if that could be an issue with docker. If yes, it's worth checking the follow-up blogs. They deal with that.