Internet of Things
  • Technologies
  • More
Internet of Things
Forum GPRS module HTTP GET/POST
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Internet of Things to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 523 subscribers
  • Views 29487 views
  • Users 0 members are here
  • internet
  • post
  • sim800l
  • gsm
  • gprs
  • iot
  • get
  • arduino
  • module
Related

GPRS module HTTP GET/POST

e14 Contributor
e14 Contributor over 10 years ago

Hello Everyone,

I've been working on a LoNet mini GSM module (SIM800L), interfacing it with Arduino.

I've inserted the SIM mobile card with Internet connection available.

Through serial monitor I'm communicating with it with no problems, but when it comes to make a GET or a POST request to a webserver page it returns Network Error (601).

Here it is:

 

AT+SAPBR=3,1,"CONTYPE","GPRS"

OK

 

AT+HTTPINIT

OK

 

AT+HTTPPARA="CID",1

OK

 

AT+HTTPPARA="URL","http://<Public_Ip_Address>:8080/folder/savedata.php"

OK

 

AT+HTTPACTION=0

OK

+HTTPACTION: 0,601,0      //601: Network Error

 

AT+HTTPREAD=1,100000

OK

 

And no response of the "echo" of the php page...

Do you have any suggestion?

Thanks in advance.

Attachments:
image
image
  • Sign in to reply
  • Cancel
  • BigG
    BigG over 10 years ago

    Usually after this command AT+SAPBR=3,1,"CONTYPE","GPRS" you  enter your "APN", "USR" & "PWD" details also using SAPBR=3,1 etc. These details must match the SIM card / mobile phone provider.

     

    Then it is recommended to check that your device has now received an IP address. Sometimes this is not straight away. Use AT+SAPBR=2,1 to query and this will return your IP address which you should check for confirmation.

     

    Once you have IP address you can enter AT+HTTPINIT, AT+HTTPPARA="CID",1 etc.

     

    Now to use GET you have to include a "?" after the URL to provide your php script with a key=value pairing.

     

    Thus in your case it is something like, AT+HTTPPARA="URL","http://<Public_Ip_Address>:8080/folder/savedata.php?A=1001" where A is the key and 1001 is the value.

     

    Now send the AT+HTTPACTION=0 and you should get a +HTTPACTION: 0,200,1000 response where 200 is the OK and 1000 is the payload size. AT+HTTPREAD will allow you to read the response if it is required.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to BigG

    Hi BigG, thanks to your response, it is very useful to me...

    What I still don't understand is:

     

    why do I have to set APN (access point name), USR, PSW, if I don't connect to the Internet using an Access Point?

    I want to connect to the Internet using GPRS directly, without passing through a Lan or through a Router which I have to connet to.

    Thanks again.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to BigG

    HiBigG,

    I got what you wanted to say. We talk about APN,USER,PSW of the Provider of the GPRS sim card.

    I've searched these pieces of information on the Internet and I've found: APN= "tre.it", USER=""; PSW=""

    then I wrote the following commands, but, as you can see, I cannot get a valid IP address to start the connection:

     

    RDY

    +CFUN: 1

    +CPIN: READY

     

    Call Ready

     

    SMS Ready

     

    AT

    OK

     

    AT+CGATT? 

    +CGATT: 1

    OK

     

    AT+CGATT=1

    OK

     

    AT+SAPBR=3,1,"CONTYPE","GPRS"

    OK

     

    AT+SAPBR=3,1,"APN","tre.it" 

    OK

     

    AT+SAPBR=3,1,"USER","" 

    OK

     

    AT+SAPBR=3,1,"PWD","" 

    OK

     

    AT+SAPBR=2,1 

    +SAPBR: 1,3,"0.0.0.0"

    OK

     

    ... What am I getting wrong? Thanks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • BigG
    BigG over 10 years ago

    Hello, no you are not getting anything wrong as far as I can tell. Assuming you have credit on SIM card, are using the right settings and that you have reasonable cellular signal strength etc, then what is happening is that you are waiting for the tre.it AP to assign you an IP address. As noted in my original post, this does not always happen straight away. You could wait awhile (minutes) on some occasions and other times you can get one straight away. You just keep checking every few seconds using AT+SAPBR=2,1

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • arun@819
    arun@819 over 9 years ago in reply to BigG

    HI BigG

     

    hello i am  also working in sim 800 and whenever i try to update to the http server i am facing these kind of errors mainly

     

    +HTTPACTION: 0,603,0 (Dns error)

    +HTTPACTION: 0,601,0 (network error)

    +HTTPACTION: 0,604,0 (stack Busy)

     

    i am not getting any idea how to solve it  tried whatever u were telling to  Alessandro Argentieri but i was not able to solve it is there any way to get to know what the problem is by using any other  at commands .

     

    1)how to overcome the stack busy error ?

    2)  i got network error (+HTTPACTION: 0,601,0 ) but when i call it picks my call? at that moment.

     

    please help me to sought the error

     

    Thanks in advance

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • BigG
    BigG over 9 years ago

    Arun, if I recall from past experience this could have something to do with your server script rather than with device hardware/code. Are you trying to get a large amount of data in return via a server response. If it is stack related you may need to use a chunked data response. Sometime you need to buffer at server side before responding. Did you try a "hello world" test etc. to make sure a basic http request works.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • arun@819
    arun@819 over 9 years ago

    HI BigG

     

    I am able to uplod data to the server but sometimes i get these type of errors which i mentioned earlier.Please look at the issues also.

    I am trying to post the data to the server and my buff size will be around  150KB and with some delay i am posting one more data which will be around 30KB

     

    and some times i get this error +HTTPACTION 604 (stack error ) and after that i get one more error is +HTTPACTION 603(dns error) .

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • BigG
    BigG over 9 years ago

    Need to see your device and server code as well as know what microcontroller and server type is being used to rule in / rule out probable causes.

     

    Did you search stackoverflow, as a quick search revealed this link gsm - error +HTTPACTION:0,601,0 - Stack Overflow