Internet of Things
  • Technologies
  • More
Internet of Things
Forum GPRS module HTTP GET/POST
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Internet of Things to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 523 subscribers
  • Views 29488 views
  • Users 0 members are here
  • internet
  • post
  • sim800l
  • gsm
  • gprs
  • iot
  • get
  • arduino
  • module
Related

GPRS module HTTP GET/POST

e14 Contributor
e14 Contributor over 10 years ago

Hello Everyone,

I've been working on a LoNet mini GSM module (SIM800L), interfacing it with Arduino.

I've inserted the SIM mobile card with Internet connection available.

Through serial monitor I'm communicating with it with no problems, but when it comes to make a GET or a POST request to a webserver page it returns Network Error (601).

Here it is:

 

AT+SAPBR=3,1,"CONTYPE","GPRS"

OK

 

AT+HTTPINIT

OK

 

AT+HTTPPARA="CID",1

OK

 

AT+HTTPPARA="URL","http://<Public_Ip_Address>:8080/folder/savedata.php"

OK

 

AT+HTTPACTION=0

OK

+HTTPACTION: 0,601,0      //601: Network Error

 

AT+HTTPREAD=1,100000

OK

 

And no response of the "echo" of the php page...

Do you have any suggestion?

Thanks in advance.

Attachments:
image
image
  • Sign in to reply
  • Cancel
Parents
  • BigG
    BigG over 10 years ago

    Usually after this command AT+SAPBR=3,1,"CONTYPE","GPRS" you  enter your "APN", "USR" & "PWD" details also using SAPBR=3,1 etc. These details must match the SIM card / mobile phone provider.

     

    Then it is recommended to check that your device has now received an IP address. Sometimes this is not straight away. Use AT+SAPBR=2,1 to query and this will return your IP address which you should check for confirmation.

     

    Once you have IP address you can enter AT+HTTPINIT, AT+HTTPPARA="CID",1 etc.

     

    Now to use GET you have to include a "?" after the URL to provide your php script with a key=value pairing.

     

    Thus in your case it is something like, AT+HTTPPARA="URL","http://<Public_Ip_Address>:8080/folder/savedata.php?A=1001" where A is the key and 1001 is the value.

     

    Now send the AT+HTTPACTION=0 and you should get a +HTTPACTION: 0,200,1000 response where 200 is the OK and 1000 is the payload size. AT+HTTPREAD will allow you to read the response if it is required.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • BigG
    BigG over 10 years ago

    Usually after this command AT+SAPBR=3,1,"CONTYPE","GPRS" you  enter your "APN", "USR" & "PWD" details also using SAPBR=3,1 etc. These details must match the SIM card / mobile phone provider.

     

    Then it is recommended to check that your device has now received an IP address. Sometimes this is not straight away. Use AT+SAPBR=2,1 to query and this will return your IP address which you should check for confirmation.

     

    Once you have IP address you can enter AT+HTTPINIT, AT+HTTPPARA="CID",1 etc.

     

    Now to use GET you have to include a "?" after the URL to provide your php script with a key=value pairing.

     

    Thus in your case it is something like, AT+HTTPPARA="URL","http://<Public_Ip_Address>:8080/folder/savedata.php?A=1001" where A is the key and 1001 is the value.

     

    Now send the AT+HTTPACTION=0 and you should get a +HTTPACTION: 0,200,1000 response where 200 is the OK and 1000 is the payload size. AT+HTTPREAD will allow you to read the response if it is required.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to BigG

    Hi BigG, thanks to your response, it is very useful to me...

    What I still don't understand is:

     

    why do I have to set APN (access point name), USR, PSW, if I don't connect to the Internet using an Access Point?

    I want to connect to the Internet using GPRS directly, without passing through a Lan or through a Router which I have to connet to.

    Thanks again.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to BigG

    HiBigG,

    I got what you wanted to say. We talk about APN,USER,PSW of the Provider of the GPRS sim card.

    I've searched these pieces of information on the Internet and I've found: APN= "tre.it", USER=""; PSW=""

    then I wrote the following commands, but, as you can see, I cannot get a valid IP address to start the connection:

     

    RDY

    +CFUN: 1

    +CPIN: READY

     

    Call Ready

     

    SMS Ready

     

    AT

    OK

     

    AT+CGATT? 

    +CGATT: 1

    OK

     

    AT+CGATT=1

    OK

     

    AT+SAPBR=3,1,"CONTYPE","GPRS"

    OK

     

    AT+SAPBR=3,1,"APN","tre.it" 

    OK

     

    AT+SAPBR=3,1,"USER","" 

    OK

     

    AT+SAPBR=3,1,"PWD","" 

    OK

     

    AT+SAPBR=2,1 

    +SAPBR: 1,3,"0.0.0.0"

    OK

     

    ... What am I getting wrong? Thanks.